Tool change description
This section lists and describes the changes for each version of this tool.
Version | Change descriptions |
|---|---|
1.0 | New tool. |
1.1 | Added Settings and Help menus. Moved link about version changes to the message console, when it is applicable. Added icon to indicate online/offline status. Removed Summary dialog; summary is shown in the console. |
1.2.0 | Added Retry button. Changed Apply button to Update . Added Close button. Tool can be launched from the Windows Start menu. Updated versioning to support patch releases. Updated for the MTB flow. Added toolbar commands to show/hide items, as well as collapse and expand the trees. |
1.30 | Added indications for newer versions of BSPs and libraries. For BSPs and libraries that are not selected, the displayed version was changed from Latest #.X release to the actual most recent X.Y.Z release. |
1.40 | Updated the handling on . mtbx files. |
2.0 | Entire GUI updated to support ModusToolbox™ version 3.0. |
2.10 | Added Rename BSP feature. Added Create from MPN feature. Changed Offline mode to Local Content mode. Removed online status icon. |
2.20 | Back-end changes and bug fixes. Updated the Properties tab to include descriptions. |
2.21 | Added Information Levels to Settings menu. |
2.30 | Added Manifest DB option to Settings menu. |
2.40 | Updated the Settings menu to add a link to the Settings tool and remove all of the items for general settings. |
2.50 | Back-end changes and bug fixes. |