PSOC™ 4, PMG
| Library | Details | Docs |
|---|---|---|
| mtb-hal-cat2 | The Hardware Abstraction Layer package provides a set of APIs to initialize, configure, and use the resources using the defined Hardware Abstraction Layer. | API reference |
| mtb-pdl-cat2 | The Peripheral Driver Library (PDL) integrates device header files, startup code, and low-level peripheral drivers into a single package. | API reference |
| recipe-make-cat2 | This repo provides the build recipe make files and scripts for building and programming PSOC™ 4 and PMG applications. | Release notes |