Skip to main content

Launch the Project Creator

You can launch the Project Creator in various ways based on your operating system and how you work.

As a stand-alone GUI tool

Launch the Project Creator as a stand-alone GUI tool by running its executable for your operating system (for example, select it using the Windows Start menu or the macOS Finder). By default, it is installed here:

[install_dir]/ModusToolbox/tools_[version]/project-creator

GUI command-line options

The Project Creator GUI provides several useful command-line options that you can use when launching the GUI. The following table shows each option and its corresponding purpose:

OptionDescription
--closeCloses the GUI once the project creation is complete.
--ide [IDE Name]Sets the value of the Target IDE field on the Application page. The [IDE Name] can be one of the following: eclipse, vscode, ewarm, uvision, none.
--ide-readonlyCauses the Target IDE field in the project-creator to be read-only.
--machine-interfaceOutputs project creation status in a JSON format to the standard output.
--verbose[0-3]When launching from the executable, you can add this option to specify more or less messaging in the message console. The default level is 1.

From the Dashboard

Starting with the ModusToolbox™ 3.1 tools package, there is a Dashboard tool that allows you to launch the Project Creator for a given IDE. Refer to the Dashboard user guide for more details.

VS Code and Eclipse

VS Code and Eclipse have tools to launch the Project Creator tool. Refer to the applicable user guide for more details:

As a command-line tool

To run the Project Creator as a command-line tool, navigate to the install location and run the project-creator-cli executable from a command-line prompt. By default, it is installed here:

[install_dir]/ModusToolbox/tools_[version]/project-creator

For more information about command-line options, run the project-creator-cli executable using the -h option. Refer to the CLI description section later in this document for more details and an example.