CLI description
You can also use the project-creator-cli executable to create applications from a command-line prompt or from within batch files or shell scripts. The exit code for the CLI is zero if the operation is successful, or non-zero if the operation encounters an error. For Windows, use the modus-shell bash installed in the ModusToolbox™ "tools" directory. For macOS and Linux, use the appropriate bash for your system.
The project-creator-cli executable is located in the same directory as the GUI version of the tool ([install_dir]/ModusToolbox/tools_[version]/project-creator/). To see all the options available, run the tool with the -h option:
$ project-creator-cli -h
The following example shows running the tool with the basic options to specify a BSP and application:
$ project-creator-cli \
--board-id KIT_PSC3M5_EVK \
--app-id mtb-example-ce240510-hello-world