Install and configure software
The ModusToolbox™ Setup program is located on our website here:
https://softwaretools.infineon.com/tools/com.ifx.tb.tool.modustoolboxsetup
The Setup program is used to install base packages and additional packages on Windows, Linux, and macOS. Select the latest tools package and any other packages you want, such as the Eclipse IDE for ModusToolbox™. The Setup program will also select dependency package, such as Programming tools. Refer to the
ModusToolbox™ software installation guide
for specific instructions.
GUI set-up instructions
In general, the GUI-based tools included as part of the ModusToolbox™ tools package work out of the box without any changes required. The same is true of packages installed through the Setup program in addition to the tools package. Simply launch the executable for the applicable GUI tool. On Windows, most tools are on the
Start
menu.
CLI set-up instructions
Before using the CLI tools, ensure that the environment is set up correctly. To check your installation, open the appropriate command-line terminal for your operating system.
Note: For Windows, the tools package provides a command-line utility called "modus-shell." You can run this by typing "modus-shell" in the Windows search box.
Type
which make
. For most environments, it should return
/usr/bin/make
.
Type
which git
. For most environments, it should return
/usr/bin/git
.
If these commands return the appropriate paths, then you can begin using the CLI. Otherwise, install and configure the GNU make and Git packages as appropriate for your environment.