Sensing
Example | Description |
|---|---|
CAPSENSE Buttons and Slider | This code example features a 5-segment CAPSENSE™ slider and two CAPSENSE™ buttons. Button 0 turns the LED on, Button 1 turns the LED off and the slider controls the brightness of the LED. The code example also demonstrates monitoring CAPSENSE™ data using CAPSENSE™ Tuner GUI tool. For more details, see the README on GitHub . |
CAPSENSE Buttons and Slider FreeRTOS | This code example features a 5-segment linear slider and two CAPSENSE™ buttons. Button 0 turns the LED on, Button 1 turns the LED off and the slider controls the brightness of the LED. The code example also demonstrates interfacing the CAPSENSE™ Tuner using the I2C interface. For more details, see the README on GitHub . |
CAPSENSE Custom Scan | This code example demonstrates CAPSENSE™ custom scanning through callback functions from CAPSENSE™ Middleware that allows altering the sensor parameters during runtime or synchronizing the CAPSENSE™ scan with non-CAPSENSE™ operations. For more details, see the README on GitHub . |
Motion Sensor over I2C FreeRTOS | This example demonstrates how to interface PSOC™ 6 MCU with a BMI160/BMI270 motion Sensor over an I2C interface within a FreeRTOS task using the BMI160/BMI270 motion sensor library. This example reads the raw motion data and estimates the orientation of the board. For more details, see the README on GitHub . |