Bluetooth®
Example | Description |
|---|---|
Battery Server | This code example demonstrates the implementation of a simple Bluetooth® battery service. The battery service exposes the battery level of the device and supports enabling battery level notifications. For more details, see the README on GitHub . |
Bluetooth LE CAPSENSE Buttons and Slider | This code example features a 5-segment CAPSENSE™ slider and two CAPSENSE™ buttons with Bluetooth® Low Energy custom service. Button 0 turns the LED on, Button 1 turns the LED off and the slider controls the brightness of the LED. The LED status is notified to the client via Bluetooth® Low Energy GATT profile. For more details, see the README on GitHub . |
Bluetooth LE CTS Client | This code example demonstrates the implementation of a simple AIROC™ Bluetooth® LE GAP peripheral - GATT client with Current time service (CTS) using PSOC™ 6 MCU, AIROC™ CYW20829, and ModusToolbox™ Software Environment. For more details, see the README on GitHub . |
Bluetooth LE CTS Server | This code example demonstrates the implementation of a simple AIROC™ Bluetooth® LE GAP central - GATT server with Current time service (CTS) using PSOC™ 6 MCU, AIROC™ CYW20829, and ModusToolbox™ software environment. For more details, see the README on GitHub . |
Bluetooth LE Environmental Sensing Service | This code example demonstrates the implementation of a simple Bluetooth® LE environmental sensing profile. It shows how to send environmental parameters like temperature by sending simulated temperature values over the Bluetooth® LE connection using AIROC™ CYW20829 Wi-Fi & Bluetooth® combo SoCs For more details, see the README on GitHub . |
Bluetooth LE Findme | This code example demonstrates the implementation of a simple Bluetooth® Immediate Alert Service (IAS)-based Find Me Profile (FMP) using the Infineon PSOC™ 6 MCU with AIROC™ Bluetooth® LE, AIROC™ CYW20829, and AIROC™ Wi-Fi & Bluetooth® combo SoC devices. For more details, see the README on GitHub . |
Bluetooth LE Findme | This code example demonstrates the implementation of a simple Bluetooth® Immediate Alert Service (IAS)-based Find Me Profile (FMP) using the Infineon Wi-Fi & Bluetooth® combo SoC devices. For more details, see the README on GitHub . |
Bluetooth LE Hello Sensor | This code example demonstrates the implementation of Bluetooth® LE custom service with Bluetooth® security using AIROC™ CYW20829, PSOC™ 6 , and ModusToolbox™ software environment. For more details, see the README on GitHub . |
Bluetooth LE Long Range Central | This code example demonstrates the use of LE Long Range PHY as a central (GATT Client) application with Infineon AIROC™ CYW55xxx Bluetooth® devices and ModusToolbox™ software environment. |
Bluetooth LE Multi Beacon | This code example demonstrates the implementation of a beacon which advertises Eddystone and iBeacon UUID data. For more details, see the README on GitHub . |
Bluetooth LE Peripheral Privacy | This code example demonstrates the privacy features available to users in Bluetooth® Low Energy 5.0 and above using ModusToolbox™ software. For more details, see the README on GitHub . |
Headset Speaker | This app demonstrates the use of a Bluetooth® Headset via the audio libraries. This app also supports the AAC codec for some Bluetooth® devices. |
Hello-Client | This code example demonstrates the implementation of Bluetooth® LE multi role applications using AIROC™ CYW955513EVK_01, and ModusToolbox™ software. |
Hello-Sensor | This code example demonstrates the implementation of Bluetooth® LE custom service with Bluetooth® security using AIROC™ CYW955513EVK_01 and ModusToolbox™ software environment. |
Watch | This app demonstrates the use of a Bluetooth® A2DP Source via the audio libraries. This app also supports the HFP AG, AVRCP, GATT, AMS, ANCS profiles. |
Wi-Fi Onboarding Using Bluetooth LE | This code example demonstrates Wi-Fi Onboarding using Bluetooth® Low Energy. For more details, see the README on GitHub . |