Motor Control
Example | Description |
|---|---|
MOTOR DEMO | This example is the out-of-the-box (OOB) demo project for the Infineon's Motor Drive card. For more details, see the README on GitHub . |
PMSM FOC SL with 1-shunt | This code example demonstrates the implementation of single shunt PMSM sensorless field-oriented control (FOC) using the Infineon's in PSoC™ Control C3 MCU devices. For more details, see the README on GitHub . |
PMSM FOC SL with 3-shunt | This code example demonstrates the implementation of PMSM sensorless field-oriented control (FOC) using the Infineon's in PSoC™ Control C3 MCU devices. For more details, see the README on GitHub . |