| Bluetooth LE Battery Client | This code example demonstrates the implementation of the Bluetooth® LE Battery Service client using the Infineon® AIROC™ CYW20829 Bluetooth® chip and PSoC™ 6 MCU with AIROC™ Bluetooth® LE with ModusToolbox™ software environment.
For more details, see the README on GitHub. |
| Bluetooth LE Battery Server | This code example demonstrates the implementation of a simple Bluetooth® LE Battery Service. The Battery Service exposes the Battery Level of the device and supports over-the-air (OTA) update over Bluetooth® Low Energy connection.
For more details, see the README on GitHub. |
| Bluetooth LE CAPSENSE Buttons and Slider | This code example features a 5-segment CAPSENSE™ slider and two CAPSENSE™ buttons with Bluetooth® Low Energy custom service. Button 0 turns the LED on, Button 1 turns the LED off and the slider controls the brightness of the LED. The LED status is notified to the client via Bluetooth® Low Energy GATT profile.
For more details, see the README on GitHub. |
| Bluetooth LE CTS Client | This code example demonstrates the implementation of a simple AIROC™ Bluetooth® LE GAP peripheral - GATT client with Current time service (CTS) using PSoC™ 6 MCU, AIROC™ CYW20829, and ModusToolbox™ Software Environment.
For more details, see the README on GitHub. |
| Bluetooth LE CTS Server | This code example demonstrates the implementation of a simple AIROC™ Bluetooth® LE GAP central - GATT server with Current time service (CTS) using PSoC™ 6 MCU, AIROC™ CYW20829, and ModusToolbox™ software environment.
For more details, see the README on GitHub. |
| Bluetooth LE Environmental Sensing Service | This code example demonstrates the implementation of a simple Bluetooth® LE environmental sensing profile. It shows how to send environmental parameters like temperature by sending simulated temperature values over the Bluetooth® LE connection using AIROC™ CYW20829 Wi-Fi & Bluetooth® combo SoCs
For more details, see the README on GitHub. |
| Bluetooth LE Findme | This code example demonstrates the implementation of a simple Bluetooth® Immediate Alert Service (IAS)-based Find Me Profile (FMP) using the Infineon PSoC™ 6 MCU with AIROC™ Bluetooth® LE, AIROC™ CYW20829, and AIROC™ Wi-Fi & Bluetooth® combo SoC devices.
For more details, see the README on GitHub. |
| Bluetooth LE Hello Sensor | This code example demonstrates the implementation of Bluetooth® LE custom service with Bluetooth® security using AIROC™ CYW20829, PSoC™ 6 , and ModusToolbox™ software environment.
For more details, see the README on GitHub. |
| Bluetooth LE Multi Beacon | This code example demonstrates the implementation of a beacon which advertises Eddystone and iBeacon UUID data.
For more details, see the README on GitHub. |
| Bluetooth LE Multi-peripheral | This code example demonstrates the implementation of multi-peripheral functionality using PSoC™ 6 MCU with Bluetooth® Low Energy, AIROC™ CYW20829, and ModusToolbox™ software environment.
For more details, see the README on GitHub. |
| Bluetooth LE Peripheral Privacy | This code example demonstrates the privacy features available to users in Bluetooth® Low Energy 5.0 and above using ModusToolbox™ software.
For more details, see the README on GitHub. |
| Bluetooth LE SensorHub | This code example features a Bluetooth® LE custom GATT Server with multiple sensors. The motion sensor and thermistor are interfaced with PSoC™ 6 MCU. The sensor reading is sent to the GATT Client over GATT notification. This project uses the sensors and middleware library; it is developed in the ModusToolbox™ software environment.
For more details, see the README on GitHub. |
| Bluetooth LE UI demo | This code example features a Bluetooth® LE custom GATT service with UI experience for an E-INK display along with sensors and RGB LED. The sensor readings are sent to the GATT Client over GATT indication. This RGB LED is controlled over a GATT Client application; it is developed in the ModusToolbox™ software environment.
For more details, see the README on GitHub. |
| Wi-Fi Onboarding Using Bluetooth LE | This code example demonstrates Wi-Fi Onboarding using Bluetooth® Low Energy.
For more details, see the README on GitHub. |