Troubleshooting
Problem
Errors are observed while performing the --device-list command with MiniProg4 probe connected:
Error = The HID read has timed out. Cannot open the 'MiniProg4 CMSIS-DAP HID-<serial-number> device.
Root cause
KitProg2 firmware is installed on MiniProg4.
Solution
Update KitProg-based device from Bootloader mode:
-
Switch the KitProg3-based device to Bootloader mode.
- Unplug device while pressing the Mode Select button.
- Plug in device back.
- Release the Mode Select button.
-
Perform firmware update using the
--update-kp3 command.
Problem
The supported KitProg3-based device is connected and can be seen in the system, but it cannot be detected by the fw-loader tool.
Root cause
The device is currently accessed by another process (such as PSOC™ Programmer, etc.), or the fw-loader tool version is not up to date with the KitProg3 Firmware on the connected device.
Solution
Close any other applications that might use the connected KitProg3-based device and retry the operation. If the issue persists, make sure to use the latest version of the fw-loader tool, or downgrade the KitProg3 FW to the older supported version via firmware update from Bootloader mode (see steps above).