PSOC™ Control quick start guide
This topic provides a quick start reference for PSOC™ Control devices. See also the video here: Getting started using PSOC™ Control using ModusToolbox™ software
-
Install ModusToolbox™ Setup; see the ModusToolbox™ software installation guide for more details.
-
Run the Setup program and install:
- Arm® GNU Toolchain (GCC)
- base tools package
- IDE (optional, Eclipse or VS Code)
- Edge Protect Security Suite
- Programming tools package
- Industrial MCU Pack
-
Run the ModusToolbox™ Dashboard and create project for desired IDE or command line for PSOC™ Control kit. See the Dashboard user guide for more details.
-
Open the project in the desired IDE or command line, write code, and build.
-
To use J-Link (optional):
-
Install J-Link and note install location
-
Edit bsp.mk file to add
BSP_PROGRAM_INTERFACE=JLink -
If you install J-Link in a non-default location or have multiple versions, also add
MTB_JLINK_DIR=[path to J-Link], for example:- Windows: C:/Program Files/SEGGER/JLink_V852
- macOS: /Applications/SEGGER/JLink_V852
- Linux: /opt/SEGGER/JLink_V852
-
Save the bsp.mk file
-
-
Attach kit
-
Program and debug as applicable to the desired IDE