GUI Description
The BSP Assistant GUI contains various menus and fields used to create and modify BSPs.

Menus
File
-
New - Provides options to create a new BSP:
- From Sample Board
- From Contained MPNs
-
Open - Opens an existing BSP; see Opening existing BSP .
-
Export as ZIP file… - This opens a standard save file selection dialog for the host operating system, and if a file name is selected, a ZIP file containing the BSP as it is at that moment will be created at that location.
-
Open in System Explorer - This opens your computer’s file explorer tool to the folder that contains the BSP.
-
Exit - Closes the BSP Assistant.
Edit
- Undo [action]/Redo <action - Reverts/redoes the previous action made in the BSP Assistant tool, such as change devices, run configurators, or add libraries.
Settings
-
ModusToolbox™ Settings :
This opens the Settings tool, an editor that allows you to configure a wide range of settings for your environment, such as proxy settings, content modes, and manifest DB settings. See the Settings tool user guide for more details on specific features.
View
- List Changed Files - This opens a dialog to display a list of changed files; see Viewing changed files .
Help
-
View Help - Opens this document.
-
About - Opens the About box for version information, with links to open Infineon.com and the current session log file.
BSP location
The "BSP location" field is not editable, and contains the location of the currently-loaded BSP.
BSP Sections
These are various sections to edit and view the current BSP's information: see Editing the BSP for more details.
Messages
The text area at the bottom of the window displays progress and error messages from the system.
Save and Close buttons
The BSP Assistant provides Save and Close buttons, described as follows:
-
Save - This button becomes active when you make a change, such as device information, libraries, defines, etc. See Making changes section.
-
Close - This button closes the BSP Assistant. If you have any unsaved changes, a dialog displays asking if you want to save the changes.