Getting started
There are two basic steps to get started using local content:
- Create a local database (full or partial).
- Update your settings.
You can also share local content storage with other users.
Create full database
To create a local copy of the entire database, run this command:
$HOME/ModusToolbox/tools_3.4/lcs-manager-cli/lcs-manager-cli –-add-all
This creates a copy of the entire database from the remote manifest. It may take a long time depending on how many repos are in the manifest.
Create partial database
To create a local copy of a partial database, specify a particular BSPs using this command:
$HOME/ModusToolbox/tools_3.4/lcs-manager-cli/lcs-manager-cli --add-bsp <BSP Name>
Where [BSP Name] is a valid name of a BSP from the remote manifest. The specified BSP will be added to a file named watchlist.json in the lcs directory, and the BSP and all dependencies will be downloaded into local content storage.
In some cases when you use the --add-bsp command, the tool may not download all the necessary dependencies, resulting in situations where you cannot create the desired application. This can happen if a dependency is referenced by a .mtb file and not in the manifest. To solve this problem, we recommend running lcs-manager-cli with the --add-all option to download the full database.
Examples of valid BSP names include CYW943907AEVAL1F, TARGET_PMG1-CY7112, and CY8CKIT-062S2-43012. See GitHub manifest file for an example of a BSP manifest.
Update settings to use local content
Beginning with the 3.5.0 tools package, there is a ModusToolbox™ Settings tool to configure a wide range of settings for your environment, including LCS settings. You can run the settings tool as a GUI or from the command line. See the Settings tool user guide for more details on specific features.
GUI option
Launch the Settings tool GUI as applicable for your operating system. You can launch it from various tools like Project Creator and Library Manager. Once open, select Operating Mode > Local Content Mode to set the LCS mode for all tools.
If your LCS directory is located in a non-default location, use the Local Content Storage Location option to specify the location of the **.**modustoolbox/lcs directory.
Command-line option
Run the Settings tool CLI (mtb-settings-cli) in a terminal (modus-shell on Windows) using the following command:
cd [path to mtb-settings]
./mtb-settings-cli --set operating_mode=local
If your LCS directory is located in a non-default location, also use this command to specify the location of the **.**modustoolbox/lcs directory:
./mtb-settings-cli --lcs_path="[path to LCS dir]"
Share LCS
As mentioned, local content is stored in your home directory in the **.**modustoolbox/lcs folder. If you want to share LCS with other users, you can copy it from your computer to a thumb drive or network server.
When other users want to use the local content, they can paste it into the same location on their computer (*[user-home]/**.*modustoolbox/lcs) and the various ModusToolbox™ tools on the other computer will find it when they switch to use local content.
If another user copies the local storage to an alternate location, they will need to update the settings as described in Update settings to use local content section.
Local content can be shared over a network, but shouldn't be modified while it is shared.