Getting Started Guide

About this document​

Scope and purpose​

DRIVECORE is a scalable software bundle portfolio that streamlines and accelerates software development. It simplifies processes, reduces migration efforts, and minimizes commercial complexities. Drive Core offers a seamless user experience throughout the R&D journey for Infineon’s automotive microcontrollers: AURIX™, TRAVEO™, and PSOC™.

This document is created in a collaboration between Infineon and the partners of the specific bundle, to support you in the installation and set-up phase of the software, show code examples, and provide answers to common issues in this phase.

Intended audience​

Engineers who integrate with the iSOFT toolchain and the TC4D7 development board.

Introduction​

Bundle overview​

Drive Core is a scalable software bundle portfolio for AURIX™, TRAVEO™, and PSOC™ that facilitates a rapid start into Automotive software development.

Developed through close collaboration between Infineon and CP AUTOSAR toolchain providers, AURIX™ Drive Core AUTOSAR [Infineon, iSOFT, TASKING] is designed to reduce development complexity, costs, and time-to-market, while enhancing overall development productivity.

This comprehensive bundle empowers developers to quickly and efficiently tackle sophisticated design challenges.

The bundle includes:

  • Infineon’s MCAL drivers for reliable hardware abstraction

  • iSOFT’s ORIENTAIS Toolchain, featuring

    • SWC Builder for streamlined Application Software (ASW) design

    • BSW Configurator for efficient Basic Software (BSW) customization

  • A pre-integrated real-time operating system for out-of-the-box performance

  • A demo project to quickly demonstrate the communication flow from ASW to BSW

  • TASKING’s latest certified TC4x Tool Chain SmartCode

Software components​

Table 1.Software components

Tool

Version

Description

SmartCode Eclipse IDE

v10.3r1

Used for compiling TC4D7 projects

Universal Debug Engine

2024.02

Used for downloading and debugging

ORIENTAIS_Configurator

v2.2

Used for configuring BSW

ORIENTAIS_SWC_Builder

v2.2

Used for configuring SWC

EB tresos

V29.7.5

Used for configuring MCAL

AURIX_TC4x_MC-ISAR

v2.10.0

The installation package of MCAL includes the system boot file, the source code of MCAL and the documentation of MCAL

BUSMASTER

v3.2.2.25

Used for sending and receiving TC4D7 messages

Workflow​

Integrated workflow of the Demo project:

  1. Create the SWC project in the SWC Configuration Tool, import the BSW service encapsulation file generated in step 3 (optional), create the application SWC Type, SWC instance, Port connection, and the mapping from the SWC instance to the ECU. Import the DBC file, perform SignalMapping, as well as ECU partitioning and partition mapping. Perform ECU extraction to obtain the ECU extract file

  2. Create the MCAL project in the MCAL Configuration Tool, complete the configuration of the MCAL module, generate the SchM file, MemMap file and MCAL configuration file (.c/.h format) of the MCAL module, and export the MCAL configuration (.arxml format)

  3. Create the BSW project in the BSW Configuration Tool. Import the ECU extract file generated in step 1 and the MCAL configuration generated in step 2 (.arxml format) into the BSW project to complete the configuration of the BSW module and generate the service encapsulation file of the module (optional). Update the bswmd file of the BSW module (Update Bswmd), synchronize Rte/Os (Synchronized Rte/iRte-Os), and generate configuration files

  4. Create a compilation project in the SmartCode Eclipse IDE, integrate the MCAL configuration file generated in step 2, the BSW module configuration file generated in step 3, and various Source Code files into the compilation project for compilation

Figure 1. Workflow


The compilation project can be organized according to the following file structure:

Figure 2. Project directory structure diagram


The following table is a description of the project directory structure:

Table 2.Project directory structure table

Level 1 Path

Level 2 Path

Level 3 Path

Level 4 Path

Description

01_OrientaisProject

Stores the BSW module configuration project

02_TaskingProject

src

App

Stores Application code for users to utilize

BSW

BswCode

Stores the source code of the BSW modules

BswConfig

Stores the configuration of the BSW modules

Intergration

Stores additional source code for integration

LinkFile

Stores linker files

MCAL

MCALCode

Stores the source code of the MCAL modules

MCALConfig

Stores the configuration of the MCAL modules

SSw

Cfg

Stores the configuration for the startup code

Ssc_VM_Disable

Stores the non-virtualized startup code

03_SwcProject

Stores the configuration project for the SWC Application

04_McalProject

Stores the MCAL configuration project

Files in bundle​

Table 3. Files

File name

Short description

ORIENTAIS_Configurator_User_Installation_Manual.pdf

The installation guidance for the BSW configuration tool

ORIENTAIS_SWC_Builder_User_Installation_Manual.pdf

The installation guidance for the SWC configuration tool

ORIENTAIS_SWC_Builder_2.0_Feature_Manual.pdf

Guidance on the Use of SWC configuration tools

ORIENTAIS_Configurator_V2.2_User_Manual.pdf

Guidance on the Use of BSW configuration tools

Installation​

ORIENTAIS AUTOSAR toolchain setup​

License keys

After the installation is complete, when you open the tool for the first time, a pop-up window will appear. Enter the license in the pop-up window.

Figure 3. Login Window


Attention:

This license code supports the use of both ORIENTAIS Configurator and ORIENTAIS SWC Builder tools, but is only for one person to use online at a time, with a validity period of 90 days. If there are any verification issues, please delete C:\ProgramData\BitAnswer and try to re-authorize.

Installation

ORIENTAIS_Configurator installation excute file location:

..\iSOFT\Tool_Package\ ORIENTAIS Configurator V2.2_installer\ORIENTAIS_Configurator_V2.2.exe

ORIENTAIS_SWC_Builder installation excute file location:

..\iSOFT\Tool_Package\ ORIENTAIS SWC Builder V2.2_installer\ ORIENTAIS_SWC_Builder _V2.2.exe

For the installation of the iSOFT toolchain, please refer to the following documentation:

  1. BSW Configuration Tool: ORIENTAIS_Configurator_User_Installation_Manual.pdf

  2. SWC Configuration Tool: ORIENTAIS_SWC_Builder_User_Installation_Manual.pdf

Location:

..\iSOFT\Tool_User_Manual\ ORIENTAIS_Configurator_User_Installation_Manual.pdf

..\iSOFT\Tool_User_Manual\ ORIENTAIS_SWC_Builder_User_Installation_Manual.pdf

Install the remaining software on your own or consult their respective installation guides.

During installation, please note:

  1. When installing the Tasking client, enter the correct license and connect to the remote or locally deployed Tasking License Manager Server (TLM Server)

  2. When installing EB tresos 29.7.5, a valid license is required

  3. When installing AURIX_TC4x_MC-ISAR_2.10.0, a valid license is required

Setup and configuration

For the setup of the iSOFT toolchain, please refer to the following documentation:

  1. ORIENTAIS_SWC_Builder_2.0_User_Manual_Software_Design.pdf

  2. ORIENTAIS_SWC_Builder_2.0_User_Manual_Overview.pdf

  3. ORIENTAIS_SWC_Builder_2.0_User_Manual_Feature.pdf

  4. ORIENTAIS_Configurator_V2.2_User_Manual.pdf

Location:


..\iSOFT\Tool_User_Manual\ORIENTAIS_SWC_Builder_2.0_User_Manual_Software_Design.pdf

..\iSOFT\Tool_User_Manual\ORIENTAIS_SWC_Builder_2.0_User_Manual_Overview.pdf

..\iSOFT\Tool_User_Manual\ ORIENTAIS_SWC_Builder_2.0_User_Manual_Feature.pdf

..\iSOFT\Tool_User_Manual\ORIENTAIS_Configurator_V2.2_User_Manual.pdf

HW setup​

Board description

Overview

Please use the hardware development board with version KIT_A3G_TC4D7_Lite v2.1 and chip partnumber SAK-TC4D7XP-20MF500MC AB.

Setup

  1. Power Connection


    The TC4D7 board requires an external DC supply, which can be fed either through the barrel jack X3 (+7V ~ +14V) or the USB-C connector (+5V). LEDs LED3 and LED4 indicate the presence of the +3.3V and +5.0V rails. For this project the board is powered via USB-C

  2. Debugger Connection


    The TC4D7 board must be connected to an external debugger via Infineon’s 10-pin Device Access Port (DAP). This project uses the Universal Access Device 2pro for flashing and debugging

  3. CAN Connection


    The TC4D7 board needs to be connected to an external CAN bus debugger through Infineon’s high-speed CAN transceiver TLE9371VSJ. In this project, BUSMUST (external CAN debugger hardware) and BUSMASTER (the corresponding software for the external CAN debugger) are used for debugging CAN-bus-related protocol stacks

    CAN requires the configuration of three pins: CAN_TX (P01.3, ALT5), CAN_RX (P01.4, GPIO), and CAN_STB (P03.5, GPIO, this pin must be driven low)

Image

Figure 4. Board image


Demo​

Introduction​

This Demo is integrated based on the AURIX™ TC4D7 development board, including CAN communication protocol stack, CAN network management protocol stack, CAN diagnostic communication protocol stack, storage protocol stack and OS protocol stack.

Figure 5. Demo Workflow


Setup​

The overall deployment flow is as follows:

  1. Configure MCAL, generate the MCAL configuration files, and export the MCAL configuration

  2. Configure SWC and export the ECU extract file

  3. Configure BSW, import the MCAL configuration (arxml format) and the ECU extract file into the BSW configuration tool, and generate the BSW configuration files

Configure MCAL

Infineon MACL installation execute file location:

Location: ../Infineon/ AURIX_TC4x_MC-ISAR_2.10.0/ AURIX_TC4x_MC-ISAR_2.10.0.exe

EB tresos installation execute file location:

Location: ../Infineon/EB_Tresos_29.7.5/ CommandDownload2025-02-10/ setup.exe

EB tresos client license installation execute file location:

Location:../Infineon/EB_Tresos_29.7.5/EBFlexNetClientPackage(1.5.1)/EB_Client_License_Administrator_1_5_1_Setup.exe

EB tresos client license installation manual location:

Location: ../Infineon/EB_Tresos_29.7.5/EBFlexNetClientPackage(1.5.1)/ LicensingUserGuide.pdf

For usage of EB tresos, refer to this MCAL installation folder:

Location: ../Infineon/ AURIX_TC4x_MC-ISAR_2.10.0/Docs/User_Manuals

The license key for the tool is given in your Infineon Developer Center (lDC) portal

https://softwaretools.infineon.com/my/software

(Ensure to login to IDC using registered credentials).

Please import the existing MCAL configuration project (04_McalProject) into EB tresos according to the following steps:

Figure 6. Importing MCAL configuration project into EB tresos diagram


Please refer to the TC4D7 user manual, development board manual, and chip manual provided by Infineon to complete the MCAL configuration, verification, and generation of the MCAL configuration file. The detailed configuration process will not be explained here.

For usage of the MCAL configuration tool, please consult the EB tresos manual.

After completing the MCAL configuration, export it in ARXML format. The export flow is illustrated below:

Figure 7. EB tresos export MCAL configuration diagram


Configure SWC

For usage of SWC Builder, refer to:

  1. ORIENTAIS_SWC_Builder_2.0_User_Manual_Software_Design.pdf

  2. ORIENTAIS_SWC_Builder_2.0_User_Manual_Overview.pdf

  3. ORIENTAIS_SWC_Builder_2.0_User_Manual_Feature.pdf

Location: ..


..\iSOFT\Tool_User_Manual\ ORIENTAIS_SWC_Builder_2.0_User_Manual_Software_Design.pdf

..\iSOFT\Tool_User_Manual\ORIENTAIS_SWC_Builder_2.0_User_Manual_Overview.pdf

..\iSOFT\Tool_User_Manual\ ORIENTAIS_SWC_Builder_2.0_User_Manual_Feature.pdf

The license key for the tool is given in your Infineon Developer Center (lDC) portal

https://softwaretools.infineon.com/my/software

(Ensure to login to IDC using registered credentials).

Please import the existing SWC configuration project (03_SwcProject) into ORIENTAIS_SWC_Builder according to the following steps:

Figure 8. Importing SWC configuration project into SWC tool diagram


The SWC is used to configure the Service Encapsulation Interface. Please configure it according to specific requirements. For usage of the SWC configuration tool, refer to the

ORIENTAIS_SWC_Builder_2.0_Feature_Manual.pdf

(It is located in the installation directory usermanual of the SWC configuration tool).

  1. Import the DBC file into the SWC configuration tool

  2. Complete the SWC configuration

  3. Perform ECU extraction

  4. Import the resulting extraction file (in ARXML format) into the BSW configuration tool;

Importing the DBC file into the SWC configuration tool is shown in the diagram below:

Figure 9. Importing DBC file into SWC tool diagram


Below is the description of the imported CAN communication matrix:

Table 4. CAN communication protocol stack transmit message description table

Message Name

ID

Description

ECU_0x100

0x100

Periodic message, cycle time:100 ms

ECU_0x101

0x101

Mixed message, normal period 1000 ms, after event trigger send 3 consecutive frames with 50 ms interval

ECU_0x102

0x102

Event message, after trigger send 4 consecutive frames with 50 ms interval

ECU_0x103

0x103

Event message

ECU_0x104

0x104

Event message

ECU_0x200

0x200

Event message

Table 5. CAN communication protocol stack receive message description table

Message Name

ID

Description

TESTER_0x110

0x110

Periodic message, cycle time:100 ms

TESTER_0x111

0x111

Periodic message, cycle time:100 ms

TESTER_0x112

0x112

Periodic message, cycle time:100 ms

TESTER_0x113

0x113

Periodic message, cycle time:100 ms

TESTER_0x114

0x114

Periodic message, cycle time:100 ms

TESTER_0x201

0x201

Normal message

Before performing the extraction export, need to configure either inter-ECU or intra-ECU communication (Sender-Receiver communication) so that the CAN communication matrix imported from the DBC file can be extracted correctly.

This project implements a 1:N communication mechanism using the multi-instance approach, creating one sender and three receivers. The procedure is as follows:

  1. Create one System and one ECU Composition, then add the ECU Composition to the Root Composition, as shown in the diagram below:

    Figure 10.

    Inter-ECU communication configuration diagram 1


  2. A SWC’s externally visible behavior is defined by its Ports and Port Interfaces. A Port is a concrete communication endpoint of the SWC; each Port is bound to exactly one Port Interface through which data items are exchanged or services are invoked. For this project two Port Interfaces are created:

    1. one for the Sender

    2. one for the Receiver

      Figure 11.

      Inter-ECU communication configuration diagram 2


  3. Create two application components Sender and Receiver:

    1. The Sender instantiates one Provide-type Port Prototype (bound to the Provide Port Interface)

    2. The Receiver instantiates one Receive-type Port Prototype (bound to the Receive Port Interface)

      Figure 12.

      Inter-ECU communication configuration diagram 3


  4. Each of the two application SWCs creates one cyclic Runnable, as shown below:

    Figure 13.

    Inter-ECU communication configuration diagram 4


  5. Create one Access-Point Trigger for each runnable:

    1. Sender runnable - select Write Data

    2. Receiver runnable - select Read Data

      Figure 14.

      Inter-ECU communication configuration diagram 5


  6. For the ECU Composition created in Step 1, create four Port prototypes:

    1. three R-Ports (Receiver)

    2. one P-Port (Provider)


      Note:

      Each new Port prototype is bound to the corresponding Port Prototype created in Step 3, the three R-Ports all use the same Receive-type Port Prototype, as shown in the diagram below:


      Figure 15.

      Inter-ECU communication configuration diagram 6


  7. Create four delegation ports and bind each one to the corresponding Port prototype created in Step 6. For every delegation port, add an Inter Port connection that links the delegation port to the application component’s port, as shown in the diagram below:

    Figure 16.

    Inter-ECU communication configuration diagram 7


  8. Map the application components to the ECU, as shown in the diagram below:

    Figure 17.

    Inter-ECU communication configuration diagram 8


  9. Signal mapping links the Sender-Receiver communication data to message signals, in this project, to the signals carried on the CAN frames, as shown in the diagram below:

    Figure 18.

    Inter-ECU communication configuration diagram 9


After the Sender-Receiver communication configuration above is complete, perform the ECU extraction, as shown in the diagram below:

Figure 19. SWC configuration tool exporting extraction file diagram


Configure BSW

For usage of BSW Configurator, refer to ORIENTAIS_Configurator_V2.2_User_Manual.pdf


Location:


..\iSOFT\Tool_User_Manual\ORIENTAIS_Configurator_V2.2_User_Manual.pdf

The license key for the tool is given in your Infineon Developer Center (lDC) portal

https://softwaretools.infineon.com/my/software

(Ensure to login to IDC using registered credentials).

Please import the existing BSW configuration project (01_OrientaisProject) into ORIENTAIS_Configurator according to the following steps:

Figure 20. Importing BSW configuration project into BSW configuration tool diagram


This project configures 18 messages in total: twelve for CAN communication (periodic, event and mixed), one for CAN network management, three for CAN diagnostic communication and two for E2E communication. A total of 10 Tasks are configured.

For detailed BSW configuration, please refer to

Configuration

. For instructions on using the BSW configuration files, please refer to

ORIENTAIS_Configurator_V2.2_User_Manual.pdf

(It is located in the installation directory usermanual of the BSW configuration tool).

After finishing the MCAL configuration, import the MCAL configuration file (ARXML) exported by

Configure MCAL

into the BSW configuration tool. This step is required because BSW modules depend on the MCAL settings, the import flow is as follows:

Figure 21. BSW configuration tool importing MCAL configuration diagram


After SWC configuration is complete, import the ECU extract file (ARXML) exported by

Configure SWC

into the BSW configuration tool, this import is necessary because SWC configuration essentially links user interfaces with BSW interfaces, the import flow is as follows:

Figure 22. BSW configuration tool importing extract file diagram


After MCAL and SWC configuration are complete, configure the BSW modules according to

Configuration

, then generate the configuration by following the steps below:

  1. Configure the initialization configuration of each module inside EcuM

    Figure 23.

    EcuM configuration diagram 1


    Figure 24.

    EcuM configuration diagram 2


  2. Update the Bswmd files of all BSW modules, re-synchronise Rte/iRte-OS, open the OS module and save it, so that every BSW MainFunction is dispatched by the correct Task

  3. Validate all BSW modules and resolve every error. Choose to validate all modules at once or one module at a time. Refer to the diagram below, the left half diagram shows the simultaneous validation of all modules, the right half diagram shows the validation of a single module

    Figure 25.

    BSW configuration tool validation diagram


  4. Generate configuration files for all BSW modules, choose to generate all modules at once or one module at a time. The left half of the diagram shows the generate all modules, the right half of the diagram shows the generate single module

    Figure 26.

    BSW configuration tool generation diagram


  5. Only on the first generation, add the CAN interrupt-service functions to the corresponding ISR entry points in the generated Os_UserInf.c, this ensures the correct routine is invoked when the interrupt occurs. In all subsequent generations the previously added code will be preserved and not overwritten, as illustrated below

    ISR(ISR_CAN0_INT4_Handler)

    {

    /* please insert your code here ... */

    /** DO NOT CHANGE THIS COMMENT!

    * <USERBLOCK CAN0_INT4>

    */

    /* custom code.... */

    Can_17_McmCan_IsrReceiveHandler(0,1);

    /** DO NOT CHANGE THIS COMMENT!

    * </USERBLOCK>

    */

    }

    ISR(ISR_CAN0_INT5_Handler)

    {

    /* please insert your code here ... */

    /** DO NOT CHANGE THIS COMMENT!

    * <USERBLOCK CAN0_INT5>

    */

    /* custom code.... */

    Can_17_McmCan_IsrTransmitHandler(0,1);

    /** DO NOT CHANGE THIS COMMENT!

    * </USERBLOCK>

    */

    }

    ISR(ISR_CAN0_INT6_Handler)

    {

    /* please insert your code here ... */

    /** DO NOT CHANGE THIS COMMENT!

    * <USERBLOCK CAN0_INT6>

    */

    /* custom code.... */

    Can_17_McmCan_IsrBusOffHandler(0,1);

    /** DO NOT CHANGE THIS COMMENT!

    * </USERBLOCK>

    */

    }

    ISR(ISR_CAN0_INT7_Handler)

    {

    /* please insert your code here ... */

    /** DO NOT CHANGE THIS COMMENT!

    * <USERBLOCK CAN0_INT7>

    */

    /* custom code.... */

    Can_17_McmCan_IsrRxFIFOHandler(0,1);

    /** DO NOT CHANGE THIS COMMENT!

    * </USERBLOCK>

    */

    }
  6. After every generation, place MemAcc_MainFunction() and Mem_17_Nvm_MainFunction() immediately after Fee_MainFunction() in the generated Rte.c to ensure the memory stack MainFunctions are dispatched in the correct order, as shown below

    TASK(iSoft_Auto_OsTask_10ms_BSW)

    {

    EventMaskType eventMask;/* PRQA S 1532 */ /*VL_QAC_OneFunRef */

    while (1)

    {

    WaitEvent(iSoft_Auto_OsEvent_10ms_BSW);

    GetEvent(iSoft_Auto_OsTask_10ms_BSW,&eventMask);

    ClearEvent(eventMask);

    /* Position:0 */

    if ((eventMask & iSoft_Auto_OsEvent_10ms_BSW) != 0)

    {

    Fee_MainFunction();

    MemAcc_MainFunction();

    Mem_17_Nvm_MainFunction();

    }

    }

    }
  7. Modify Cpu0_Main.c, place EcuM_Init() inside core0_main() and use it to perform ECU initialization, as shown below

    #include "EcuM.h"

    void core0_main (void)

    {

    EcuM_Init();

    for(;;)

    {

    }

    }
  8. Place Mcu_Init() in EcuM_Callout_Stubs.c and initialize the clocks(Initialization clock options, lock the PLL, and switch the clock source), as shown below

    void EcuM_AL_DriverInitOne(void)

    /* PRQA S 6070 -- */

    {

    const EcuM_GenBSWPbCfgType * pbCfg =EcuM_ConfigPtr->modulePBCfg;

    /* PRQA S 0317 ++ */ /* VL_QAC_0317 */

    /** DO NOT CHANGE THIS COMMENT!

    * <USERBLOCK EcuM_AL_DriverInitOne MCU one>

    */

    /* custom code.... */

    /** DO NOT CHANGE THIS COMMENT!

    * </USERBLOCK>

    */

    Mcu_Init(pbCfg->mcu00PbCfg);

    /** DO NOT CHANGE THIS COMMENT!

    * <USERBLOCK EcuM_AL_DriverInitOne MCU two>

    */

    /* custom code.... */

    (void)Mcu_InitClock(0);

    while(MCU_PLL_UNLOCKED ==Mcu_GetPllStatus())

    {

    }

    (void)Mcu_DistributePllClock();

    /** DO NOT CHANGE THIS COMMENT!

    * </USERBLOCK>

    */

    Can_17_McmCan_Init(pbCfg->can01PbCfg);

    Port_Init(pbCfg->port02PbCfg);

    /* PRQA S 0317 -- */

    /** DO NOT CHANGE THIS COMMENT!

    * <USERBLOCK EcuM_AL_DriverInitOne Other>

    */

    /* custom code.... */

    Mem_17_Nvm_Init(NULL_PTR);

    extern const MemAcc_ConfigType MemAcc_Config;

    MemAcc_Init(&MemAcc_Config);

    /** DO NOT CHANGE THIS COMMENT!

    * </USERBLOCK>

    */

    }
  9. The iSOFT-supplied link file

    Lcf_Tasking_Tricore_Tc.lsl

    includes the BSW link file

    Bsw_Link.lsl

    and the OS link

    file Os_Link.lsl

    , both auto-generated when BSW configuration is generated

Configuration​

CAN Communication Stack

Overview of the CAN Communication Protocol Stack

The CAN communication protocol stack involves the following software modules: CAN, CanIf, PduR, Com, and ECUC. The main function of each module is listed in the table below:

Table 6.CAN communication protocol stack module description table

Module Name

Function

Can

Configures the CAN controller, baud rate, and transmit/receive mailboxes

CanIf

CanIf handles PDU transfer between upper layers and the CAN driver, offering a uniform interface to manage different CAN hardware

PduR

PDU Router provides I-PDU-based routing among communication interface (CanIf), transport protocol (CanTp), diagnostic communication manager (Dcm), and communication manager (Com)

Com

COM offers I-PDU and signal management

Ecuc

ECUC supplies PDU definitions so all modules can reference them and be cross-linked by the configuration tool

Configuration of the CAN Communication Protocol Stack

Configure one CAN controller (Node 1, base address 0xf4710500) with a baud rate of 500 kbps (default); set up two receive mailboxes (one standard frame, one extended frame) and one transmit mailbox (standard frame).

When the extraction file is imported, the CAN communication protocol stack automatically sets up the routing; the only additional work is to configure CanIf, since it is tied to the CAN driver. The extra CanIf settings required are listed below:

Table 7.CanIf module configuration table

Parameter Name

Value

CanIfCtrlCanCtrlRef

Select the CAN Controller configured in the CAN module

CanIfCtrlDrvNameRef

Select the CAN module name (Can_17_McmCan)

CanIfPublicCtrlDrvVersion

Select the CAN module AUTOSAR version (AUTOSAR440)

CanIfPublicCddHeaderFile

Select the CAN module header file name (Can_17_McmCan.h)

CAN Network Manage Protocol Stack

Overview of the CAN Network Manage Protocol Stack

Table 8. CAN network management protocol stack module description table

Module Name

Function

Can

Configures the CAN controller, baud rate, and message buffers

CanIf

CanIf routes PDUs between upper layers and the CAN driver, offering a uniform interface to manage different CAN hardware

NM

The Nm module acts as an adaptation layer between ComM and CanNm and coordinates synchronized shutdown across bus channels

ComM

ComM collects and arbitrates communication requests, driving one state machine per channel to control all on-board busses

CanSM

Interacts with the hardware-abstraction and system-service layers to define bus-specific state management and flow control for each CAN bus

CanNM

Decides ECU state transitions (when to enter sleep, remain fully operational, etc.)

Ecuc

ECUC provides PDU definitions so all modules can be cross-linked by the configuration tool

Configuration of the CAN Network Manage Protocol Stack

CAN network-management transmit message ID is 0x410.

Key configuration parameters for the CAN network management stack are listed below:

Table 9.CanNM module configuration table

Parameter Name

Value

CanNmComControlEnabled

True

CanNmMainFunctionPeriod

0.005

CanNmActiveWakeupBitEnabled

True

CanNmImmediateNmTransmissions

0

CanNmMsgCycleOffset

0.01

CanNmMsgCycleTime :

0.2

CanNmNodeDetectionEnabled

True

CanNmNodeId

0

CanNmNodeIdEnabled

True

CanNmPduCbvPosition

CANNM_PDU_BYTE_1

CanNmPduNidPosition

CANNM_PDU_BYTE_0

CanNmRepeatMessageTime

1.0

CanNmTimeoutTime

3.0

CanNmWaitBusSleepTime

4.0

CanNmComMNetworkHandleRef

Reference the CAN channel configured in the ComM module.

Table 10. CanSM module configuration table

Parameter Name

Value

CanSMMainFunctionTimePeriod

0.002

CanSMModeRequestRepetitionMax

10

CanSMModeRequestRepetitionTime

0.01

CanSMBorCounterL1ToL2

20

CanSMBorTimeL1

0.01

CanSMBorTimeL2

0.1

CanSMBorTimeTxEnsured

1.0

CanSMComMNetworkHandleRef

Reference the CAN channel configured in the ComM module

CanSMControllerId

Reference the CAN controller ID defined in the CanIf module

Table 11.ComM module configuration table

Parameter Name

Value

ComMDirectUserMapping

True

ComMEcuGroupClassification

3

ComMResetAfterForcingNoComm

True

ComMDcmEnabled

True

Table 12. Nm module configuration table

Parameter Name

Value

NmNumberOfChannels

1

NmComControlEnabled

True

NmPduRxIndicationEnabled

True

NmStateChangeIndEnabled

True

NmComMChannelRef

Reference the CAN channel configured by ComM

NmStandardBusType

NM_BUSNM_CANNM

CAN Diagnostic Protocol Stack

Overview of the CAN Diagnostic Protocol Stack

Table 13.CAN diagnostic protocol stack module description table

Module Name

Function

Can

Configures the CAN controller, baud rate, and message buffers

CanIf

CanIf routes PDUs between upper layers and the CAN driver, giving them a single interface to manage any CAN hardware

PduR

PDU Router routes I-PDUs among the communication interface (CanIf), transport protocol (CanTp), diagnostic communication manager (Dcm), and communication manager (Com)

CanTp

CanTp implements the ISO 15765-2 transport layer send/receive service on CAN

Dcm

Parses diagnostic requests and executes positive/negative responses according ISO 15765-3 and ISO 14229-1

Dem

Implements storage and management of diagnostic faults, and provides APIs for other modules to read DTCs along with their associated freeze-frame and extended data

Configuration of the CAN Diagnostic Protocol Stack

CAN IDs for the CAN diagnostic protocol stack are listed below:

Table 14. CAN IDs table of CAN diagnostic protocol stack

CANID Type

CANID

Physical Request CAN ID

0x703

Functional Request CAN ID

0x7DF

Physical Response CAN ID

0x70A

Diagnostic services configured in the project are listed below:

Table 15. CAN diagnostic protocol stack diagnostic services table

Service ID

Diagnostic Services Name

Sub-functions

Diagnostic Session

NRCApplies

Security Level

Default(01)

Extended(03)

Phy

Func

Phy

Func

Level 1

0x10

DiagnosticSessionControl

0x01 DefaultSession

√

√

√

√

12

13

22

7E

0x02 ProgrammingSession

×

×

√

√

0x03 ExtendedDiagnosticSession

√

√

√

√

0x11

EcuReset

0x01 HardReset

×

×

√

×

12

13

22

7F

0x27

SecurityAccess

0x01 Security Level1 (Request Seed)

0x02 Security Level1 (Send Key)

×

×

√

×

12

13

22

24

31

35

36

37

7F

0x28

CommunicationControl

0x00 EnableRxAndTx

×

×

√

√

12

13

22

31

7F

0x01 EnableRxAndDisableTx

×

×

√

√

0x02 DisableRxAndEnableTx

×

×

√

√

0x03 DisableRxAndTx

×

×

√

√

0x3E

TesterPresent

0x00 ZeroSubFunction

√

√

√

√

12

13

0x85

ControlDTCSetting

0x01 ON

×

×

√

√

12

13

22

31

0x02 OFF

×

×

√

√

0x22

ReadDataByIdentifier

N/A

√

√

√

√

13

22

31

0x2E

WriteDataByIdentifier

N/A

×

×

√

×

13

31

22

7F

√

0x14

ClearDiagnosticInformation

FFFFFF - Clear All DTCs

×

×

√

×

13

22

31

7F

0x19

ReadDTCInformation

0x01 ReportNumberOfDTCByStatusMask

×

×

√

×

12

13

31

7F

0x02 ReportDTCByStatusMask

×

×

√

×

0x04 ReportDTCSnapshotRecordByDTCNumber

×

×

√

×

0x06 ReportDTCExtendedDataRecordByDTCNumber

×

×

√

×

0x0A ReportSupportedDTC

×

×

√

×

0x2F

InputOutputControlByIdentifier

N/A

×

×

√

×

13

22

31

33

7F

√

0x31

RoutineControl

0x01 StartRoutine

×

×

√

×

12

13

22

24

31

33

√

0x02 StopRoutine

×

×

√

×

0x03 RequestRoutineResults

×

×

√

×

Configuration information of the security access algorithm is as follows:

Mask = 0x5555AAAAu

The key algorithm (calculating the key based on the seed) is as follows, where 'seed' refers to the input seed.

Key = Seed & Mask

Note:

The maximum number of failed attempts is 3; once this limit is reached, a 10-second delay is triggered. Consecutive invalid seed requests do not increment the error count. If the seed remains unchanged, the error count will reset to zero after the delay period expires.

Table 16. I/O DID table

DIDs(HEX)

Name

InputOutputControlParameter

ControlOption

ControlStatus

Size(Byte)

1111

00

×

√

1

01

×

√

1

02

×

√

1

03

√

√

1

Note:

  1. InputOutputControlParameter: This parameter is used in the request message of &2F service to describe how the server shall control its inputs or outputs

  2. ControlOption: This parameter is used in the request message of $2F service to describe the detailed control state of request

  3. ControlState: This parameter is used in the response message of $2F service to describe the detailed control results

Table 17. DID table

DIDs(HEX)

Name

InputOutputControlParameter

ControlOption

ControlStatus

Size(Byte)

F183

Sw number

√

300

F184

√

√

9

1111

√

√

√

1

F198

√

6

F298

√

1

F286

√

100

F170

Used for DID–NVM interaction validation

√

√

10

Table 18. Routine DID table

DIDs

Name

RoutineControlType

RoutineControlOption

RoutineStatus

in Size

out size

Safety level requirements

0x1234

01

√

√

1

1

LevWel1

02

√

√

1

1

03

√

0

1

0x0203

CheckProgPreCondition

01

√

0

1

Level1

Note:

  1. RoutineControlType: 01: startRoutine, 02: stopRoutine, 03: requestRoutineResults

  2. RoutineControlOption: This parameter is used in the request message of $31 service to describe the detailed control state of request

  3. RoutineStatus: This parameter is used in the response message of $31 service to describe the detailed control results

Table 19.DTC table

DTC Number

DTC Description

DTC-Set Condition

Faults-Recover Condition

W/Lamp

Possible Fault Causes

Corrective Actio

0xC00001

The test code causes SWC to report faults

SWC directly reports faults

SWC reports non-fault

No

SWC directly reports faults

0xC00002

The test code causes SWC to report faults

SWC directly reports faults

SWC reports non-fault

No

SWC directly reports faults

0xC00003

The test code causes SWC to report faults

SWC directly reports faults

SWC reports non-fault

Yes

SWC directly reports faults

0xC00004

The test code causes SWC to report faults

SWC directly reports faults

SWC reports non-fault

Yes

SWC directly reports faults

0xC00005

CAN Bus off

CAN Bus off

CAN not in busoff state

No

1: CAN connect line failure

2: controller failure

1: check connect line

2: change RM controller

Table 20 DTC Attribute table

DTC Number

EventId

Debounce Algorithm

WIR Information

Debounce Threshold

Aging Threshold

DTC priority

0xC00001

1

counter

10

5

1

Tip:

The Tester through seed DTC Status 0x01 read only the currently DTC, through seed DTC Status 0x08 read only the history DTC. All the ECU should obey it.


Memory Protocol Stack

Overview of the Memory Protocol Stack

Table 20. Memory protocol stack module description table

Module Name

Function

Mem

Offers upper layers a unified, hardware-independent read/write/erase interface

MemAcc

Exposes address-based parameters, letting upper modules access diverse memory devices

Fee

Provides a virtual linear address space and a common allocation scheme

MemIf

Bridges NvM to Fee

NvM

Stores and manages non-volatile data

Configuration of the Memory Protocol Stack

The memory stack is configured with the following NvM blocks:

Table 21. Memory protocol stack function of NvMBlock description table

NvMBlock Name

Function

NvMBlock_ConfigID

NVM management

NvMBlock_DID_0xF170

Stores DID 0xF170 data

NvMBlock_FalseAccessCount

Records unsuccessful 0x27 unlock attempts

NvMBlock_Primary_0

Stores event data

NvMBlock_Primary_1

Stores event data

NvMBlock_Primary_2

Stores event data

NvMBlock_Primary_3

Stores event data

NvMBlock_Primary_4

Stores event data

NvMBlock_AdminData

Stores DEM management data

NvMBlock_EventStatusData

Stores UDS status

Os protocol Stack

Overview of the Os protocol Stack

AUTOSAR OS is responsible for task and interrupt management, implementing modules such as Task, ISR, Counter, Alarm, ScheduleTable, Event, and Resource.

Configuration of the Os protocol Stack

Most of the OS stack configuration is completed automatically by synchronizing Rte/iRte-Os; only the compiler environment, system clock frequency and Oslsrs (interrupt service routines) must be set manually.

The following OS configuration items have been completed:

Table 22. OS basic information configuration

Name

Value

Cores Number

1

Compiler

tasking_cctc

Table 23.Systemlsrs configuration table

Name

Parameter

Value

OsTimerSourceCore_0

STM_Frequency[MHz]

100

OsTimerSourceCore_0

TickTime[s]

0.001

OsTimerSourceCore_0

Stack Size[4bytes]

512

Table 24. Oslsrs configuration table

Name

Gategory

Stack Size[4Bytes]

Priority

Nested Enable

Core

CAN0_INT4

GATEGORY_2

512

4

False

0

CAN0_INT5

GATEGORY_2

512

5

False

0

CAN0_INT6

GATEGORY_2

512

6

False

0

CAN0_INT7

GATEGORY_2

512

7

False

0

Table 25. OsTask configuration table

Name

Priority

Stack Size[4Bytes]

Preemptive Poilcy

OsTaskAutostart

Core

iSoft_Auto_OsTask_1ms

25

256

FULL

False

0

iSoft_Auto_OsTask_10ms

25

256

FULL

False

0

iSoft_Auto_OsTask_19ms

25

256

FULL

False

0

iSoft_Auto_OsTask_Shared_0

63

256

FULL

False

0

iSoft_Auto_OsTask_2ms_BSW

25

256

FULL

False

0

iSoft_Auto_OsTask_5ms_BSW

25

256

FULL

False

0

iSoft_Auto_OsTask_10ms_BSW

25

256

FULL

False

0

iSoft_Auto_OsTask_20ms_BSW

25

256

FULL

False

0

iSoft_Auto_OsTask_SchM_0

63

256

FULL

False

0

iSoft_Auto_DEFAULT_OsTask_Init

63

1024

NON

False

0

Running the demo or build​

Build and download

TASKING_SmartCode_v10.3r1 installation excute file location:


..\Tasking\ TASKING_SmartCode_v10.3r1.zip

For the installation of the TASKING Smartcode, please refer to the following documentation:

..\Tasking\TASKING SmartCode Installation guide.pdf

For the usage of of the TASKING Smartcode, please refer to the following documentation:

..\Tasking\smartcode_ctc_user_guide.pdf


..\Tasking\smartcode_getting_started.pdf

The license key for the tool is given in your Infineon Developer Center (lDC) portal

https://softwaretools.infineon.com/my/software

(Ensure to login to IDC using registered credentials).

Please import the existing compilation project (02_TaskingProject) into SmartCode Eclipse IDE according to the following steps:

Figure 27. Importing compilation project into SmartCode Eclipse IDE diagram


  1. Import the code and configurtion file of MCAL, the code and configuration file of BSW, and the system-related files into the 02_TaskingProject build project, organizing them according to Figure

  2. Configure include paths and build parameters;

  3. Compile, first Clean project, then Build project, as shown below:

    Figure 28.

    Tasking project compilation diagram


    After successful compilation, the.elf file is generated in the Debug director:

    Figure 29.

    Compiled .elf file location diagram


  4. Use UDE 2024 to download the compiled .elf file into TC4D7

For usage of UDE, please refer to the official website of PLS:

https://www.pls-mc.com/support/downloads/

Note:

Users can choose other compatible devices for flashing and debugging.

Once the Universal Access Device 2pro has successfully connected the host to the ECU, downloading can proceed, as shown below:

Figure 30. UDE download diagram


Run and Verify

Verify of CAN Communication Stack

After successful download and execution, use a CAN bus debugger to receive the messages sent by theTC4D7, the following messages can be received:

Figure 31. CAN communication stack CAN bus message monitor diagram


Verify of CAN Diagnostic Stack

After successful download and execution, Send a diagnostic request message (CAN ID is 0x703) to TC4D7, and TC4D7 will return a diagnostic request response message (CAN ID is 0x70A).

Figure 32. CAN diagnostic stack CAN bus message monitor diagram


Development resources​

TASKING SmartCode Eclipse IDE​

TASKING® Smart­Code is an inno­v­a­tive develop­ment solu­tion for the Infineon® AURIX™ TC4x micro­con­troller family. Smart­Code offers reliable code optimization, advanced multicore support and fully supports all architectures and microprocessor cores integrated in the TC4x.

Universal Debug Engine​

The Universal Debug Engine (UDE) is a professional debugging framework designed for multi-core SoCs (System-on-Chips) and microcontrollers. It provides a comprehensive set of tools for debugging, tracing, and testing embedded systems, offering support for both high-level languages (C/C++) and assembly-level debugging.

iSOFT ORIENTAIS_Configurator​

iSOFT’s AUTOSAR solution provides a standardized,localized basic software platform for automotive electronics, supporting the development of high-performance and high-safety automotive ECUs. ORIENTAIS_Configurator is used for configuring BSW.

iSOFT ORIENTAIS_SWC_Builder​

iSOFT’s AUTOSAR solution provides a standardized, localized basic software platform for automotive electronics, supporting the development of high-performance and high-safety automotive ECUs. ORIENTAIS_Configurator is used for configuring SWC.

Infineon AURIX_TC4x_MC-ISAR​

Microcontroller – Infineon Software Architecture (MC-ISAR) is the AUTOSAR-compliant low-level driver for Infineon microcontrollers, also called MCAL (Microcontroller Abstraction Layer). It is the bottom layer in the AUTOSAR software architecture, interfacing directly with the hardware. It abstracts the hardware by allowing higher software layers to interface with microcontroller peripherals without having to know the peripheral’s architecture and registers.

BUSMASTER​

BUSMASTER is an Open Source Software tool to Simulate, Analyze and Test data bus systems such as CAN, LIN.

Support​

Troubleshooting​

Module not loaded

Description

When opening an existing BSW project with the BSW configuration tool, the project cannot read the chip or module normally.

Solution

First, right-click the project button, and then click Reset Cache to reload the project.

Figure 33. Reload the project diagram


Open BSW project

Description

The BSW Configuration Tool cannot load projects with the same name simultaneously.

Solution

First, remove the project names with the same name from the workspace of the BSW configuration tool, and then open the remaining projects with the same name.

Ecu extraction

Description

The DBC file is imported into the SWC Configuration tool for direct extraction. After successful extraction, the extracted file is imported into the BSW configuration project, and the CAN protocol stack route is not automatically generated.

Solution

The signals contained in the DBC communication matrix imported by the SWC configuration tool must be used by the system to be successfully extracted. So after importing the DBC file with the SWC configuration tool, configure the communication between application components so that the signal can be used by the system.

Contact support​

MyCases

In the event of any problems, issues, or questions, please do not hesitate to reach out to your designated Infineon contact or Field Application Engineer (FAE) for assistance. Alternatively, you can also submit a request through our ticketing system

https://mycases.infineon.com/

. For more information on how to use the myCases portal, please refer to this

document

.

Partners

By contacting support, you agree that your request and contact details are shared between

iSOFT

,

TASKING

, and Infineon.