| Example | Description |
|---|---|
| Battery Server | This code example demonstrates the implementation of a simple Bluetooth® battery service. The battery service exposes the battery level of the device and supports enabling battery level notifications. For more details, see the README on GitHub. |
| Bluetooth LE Beacon | TThis code example demonstrates the implementation of Bluetooth® LE extended advertisements and the use of the beacon library. For more details, see the README on GitHub. |
| Bluetooth LE Findme | This code example demonstrates the implementation of a simple Bluetooth® Immediate Alert Service (IAS)-based Find Me Profile (FMP) using the Infineon Wi-Fi & Bluetooth® combo SoC devices. For more details, see the README on GitHub. |
| Bluetooth LE GATT Throughput Client | This code example demonstrates the maximum Bluetooth® LE throughput (using GATT layer notification and GATT write command) that can be achieved with Infineon CYW55913 Wi-Fi and Bluetooth® LE connected MCU. For more details, see the README on GitHub. |
| Bluetooth LE Privacy | This code example demonstrates the privacy features available to users in Bluetooth® Low Energy 5.0 and above. For more details, see the README on GitHub. |
| Bluetooth LE Wi-Fi onboarding | This example uses the Infineon Wi-Fi onboarding custom service via Bluetooth® LE for provisioning a new device to a Wi-Fi Access point. For more details, see the README on GitHub. |
| Over-the-air firmware update using Bluetooth LE | This code example showcases how to perform an over-the-air (OTA) update using the Bluetooth® LE in CYW955913EVK-01 Evaluation Kit. For more details, see the README on GitHub. |
Bluetooth®
Last updated on