Example

Description

Bluetooth LE CAPSENSE Buttons and Slider

This code example features a 5-segment CAPSENSE™ slider and two CAPSENSE™ buttons with Bluetooth® Low Energy custom service. Button 0 turns the LED on, Button 1 turns the LED off and the slider controls the brightness of the LED. The LED status is notified to the client via Bluetooth® Low Energy GATT profile. For more details, see the README on GitHub .

Bluetooth LE CTS Client

This code example demonstrates the implementation of a simple AIROC™ Bluetooth® LE GAP peripheral - GATT client with Current time service (CTS) using PSOC™ 6 MCU, AIROC™ CYW20829, and ModusToolbox™ Software Environment. For more details, see the README on GitHub .

Bluetooth LE CTS Server

This code example demonstrates the implementation of a simple AIROC™ Bluetooth® LE GAP central - GATT server with Current time service (CTS) using PSOC™ 6 MCU, AIROC™ CYW20829, and ModusToolbox™ software environment. For more details, see the README on GitHub.

Bluetooth LE Environmental Sensing Service

This code example demonstrates the implementation of a simple Bluetooth® LE environmental sensing profile. It shows how to send environmental parameters like temperature by sending simulated temperature values over the Bluetooth® LE connection using AIROC™ CYW20829 Wi-Fi & Bluetooth® combo SoCs For more details, see the README on GitHub.

Bluetooth LE Hello Sensor

This code example demonstrates the implementation of Bluetooth® LE custom service with Bluetooth® security using AIROC™ CYW20829, PSOC™ 6 , and ModusToolbox™ software environment. For more details, see the README on GitHub .

Bluetooth LE Multi Beacon

This code example demonstrates the implementation of a beacon which advertises Eddystone and iBeacon UUID data. For more details, see the README on GitHub.

Bluetooth LE Peripheral Privacy

This code example demonstrates the privacy features available to users in Bluetooth® Low Energy 5.0 and above using ModusToolbox™ software. For more details, see the README on GitHub.

Wi-Fi Onboarding Using Bluetooth LE

This code example demonstrates Wi-Fi Onboarding using Bluetooth® Low Energy. For more details, see the README on GitHub .