Running a simulation
When a schematic has been set up, it can be simulated. This automatically creates the required netlist, saves the simulation results, and displays them for analysis in the Waveform Viewer.
About this task
Simulating a schematic lets you view the currents and voltages at specified points of interest over time. The simulation is controlled using the toolbar at the bottom of the Simulation Environment view
Note that rerunning a simulation overwrites any previous results from simulating the same schematic. If you want to be able to access the results of an earlier simulation, you must first make a copy of them in the file system. The results are stored in a subfolder of the project folder with the name
sim-
schematicName
-Default
. If you make a copy of that folder, you can later open the
.csdf
file in it using the
command in Waveform Viewer.
Before you begin
The schematic must be completed, as described in Working with schematics . It must be displayed in the frontmost tab.
The simulation must be set up, as described in Setting up a simulation .
Procedure
Results
The simulation is run with the specified settings. Diagnostic output is written to the tabs of the Output view. The Waveform Viewer is opened, displaying the simulation results.
What to do next
You can review the simulation results in the Waveform Viewer, as described in Evaluating simulations . If the Waveform Viewer does not open automatically, you can open it manually by clicking
.
You can review the log messages generated during the simulation by clicking
.
You can access the files generated by the simulation by clicking
.