This section lists and describes the changes for each version of this tool.

Version

Change descriptions

1.0

New tool.

1.1

Redesigned the GUI to provide a better flow.

Added Settings and Help menus.

Added icon to indicate online/offline status.

Added Import BSP button.

1.2.0

Tool can be launched from Windows Start menu.

Updated versioning to support patch releases.

Updated to select and create multiple applications at one time.

Updated to provide information about new library management flow.

1.30

Updated versioning to allow for additional minor changes.

Updated the import process to check if the BSP/application includes a makefile.

Added Target IDE option to the GUI.

Added colors to the messages; red for error, yellow for warning, green for success.

1.40

Added categories for Template Applications.

Updated handling of .mtbx files.

2.0.0

Added Expand All/Collapse All buttons.

Changed "Custom" to "Import" in the tree.

Changed

Import

button to

Browse

.

2.10.0

Updated to include new GUI command-line options.

Added

Create from MPN

feature.

Added ability to rename BSP.

Changed various button names.

Changed offline content to Local Content Storage.

Removed online indicator.

2.20

Back-end changes and bug fixes.

2.21

Added Information Levels to

Settings

menu.

2.30

Added Manifest DB option to

Settings

menu.

2.40

Updated the

Settings

menu to add a link to the Settings tool and remove all of the items for general settings.

2.50

Added connected kits feature to tool.

Back-end changes and bug fixes.