Tools targets
Note: There are various targets to launch tools and configurators that are not part of the make system, but they can be used in the application directory. The following table lists a few of the common targets as a convenience. Refer to the applicable user guide for details for the given configurator or tool.
Target | Description |
|---|---|
bsp-assistant | Launches the BSP Assistant with the active BSP for the application. |
bt-configurator | Launches the Bluetooth® Configurator GUI for the application's cybt file. |
capsense-configurator | Launches the CAPSENSE™ Configurator GUI for the target's cycapsense file. |
capsense-tuner | Launches the CAPSENSE™ Tuner GUI for the target's cycapsense file. |
device-configurator | Launches the Device Configurator on the application's *. modus file. |
library-manager | Launches the Library Manager for the application to add/remove libraries and to upgrade/downgrade existing libraries. |
lin-configurator | Launches the LIN Configurator GUI for the target's mtblin file. |
qspi-configurator | Launches the QSPI Configurator GUI for the target's cyqspi file. |
seglcd-configurator | Launches the Segment LCD Configurator GUI for the target's cyseglcd file. |
smartio-configurator | Launches the Smart I/O Configurator GUI for the target's modus file. |
usbdev-configurator | Launches the USB Configurator GUI for the target's cyusbdev file. |