Advanced tab [all gen]
The
Advanced
tab provides advanced configuration parameters. In
SMARTSENSE
mode, most of the advanced parameters are tuned automatically. Select Manual tuning to control and configure the CAPSENSE™ middleware parameters.
The parameters in the Advanced tab are systematically arranged in the following subtabs.
General subtab [various gen]
1
– Contains the parameters common for all widgets irrespective of the sensing method used for the widgets.
CSD Settings subtab [various gen]
– Contains the parameters common for widgets that use the CSD sensing method. This subtab is relevant only if at least one widget uses the CSD sensing method.
CSX Settings subtab [various gen]
– Contains the parameters common for widgets that use the CSX sensing method. This subtab is relevant only if at least one widget uses the CSX sensing method.
ISX Settings subtab [5th gen LP]
– Contains the parameters common for widgets that use the ISX sensing method. This subtab is relevant only if at least one widget uses the ISX sensing method.
WBX Settings subtab [5th gen LP]
– Contains the parameters common for widgets that use the WBX sensing method. This subtab is relevant only if at least one widget uses the WBX sensing method.
Widget Details subtab [various gen]
– Contains the parameters specific to widgets and/or sensors.
Note: Hover over the parameter value to display its description.
Hover over the parameter value to display its description.