Refer to the instructions in the

ModusToolbox™ software installation guide

for how to download and install ModusToolbox™ software. The Dashboard provides links to various sources of documentation and training materials. It also contains starting points such as: creating a new application, creating/editing a BSP, and installing or launching the ModusToolbox™ Setup program. For more details, refer to the

ModusToolbox™ Dashboard user guide.

After installation, you can launch the Dashboard to create a new application for the IDE of your choice, such as Eclipse, VS Code, IAR, or µVision. You can also access documentation and training material. The following example shows a new application for Eclipse.

  • The Learn panel provides several useful links to ModusToolbox™ community support, video tutorials, training materials, and documentation.

  • The Create panel provides access to the Project Creator and BSP Assistant tools, as well as user guides for each IDE and tool.

  • The Install panel provides a link to install and use the ModusToolbox™ Setup program.

To create a new application, select the IDE of your choosing from the drop-down menu under the Create tab. Then, click the icon or link to begin the process.