Getting Started Guide

About this document​

Scope and purpose​

DRIVECORE is a scalable software bundle portfolio that streamlines and accelerates software development. It simplifies processes, reduces migration efforts, and minimizes commercial complexities. Drive Core offers a seamless user experience throughout the R&D journey for Infineon’s automotive microcontrollers: AURIX™, TRAVEO™, and PSOC™.

This document is created in a collaboration between Infineon and the partners of the specific bundle, to support you in the installation and set-up phase of the software, show code examples, and provide answers to common issues in this phase.

Intended audience​

Engineers who integrate with the iSOFT toolchain and the TC4D7 development board.

Introduction​

DRIVECORE​

DRIVECORE is a scalable software bundle portfolio for AURIX™, TRAVEO™ and PSOC™ that facilitates a rapid start into Automotive software development.

PSOC™ DRIVECORE Smart End Point [Infineon, Elektrobit, IAR]​

The PSOC™ DRIVECORE Smart End Point [Infineon, Elektrobit, IAR] is a software Bundle suite designed to simplify and accelerate the development of edge controllers and small peripheral ECUs in automotive subsystems. With a focus on cost efficiency, re-usability, and extensibility, it empowers developers to bring reliable, scalable solutions to market faster. Tailored for applications such as smart sensors, interior lighting, and motor controls, it is ideal for small, safety-relevant ECUs where performance and resource optimization are critical.

The bundle combines proven software and tools from Infineon, Elektrobit, and IAR, enabling rapid development on Elektrobit’s EB tresos AutoCore Light—a lightweight, high-performance, ASIL-B ready, and CSMS-certified platform. It supports LIN signal-based communication, a UDS service handler (ISO 14229-1), and offers a streamlined integration and configuration work flow. Paired with Infineon’s PSOC™ 4 HV microcontroller, the bundle minimizes memory and processing overhead and ensures resource-optimized, deterministic, reliable operation in safety-relevant automotive subsystems.

Software & Tool components​

Software components

Table 1. Software components table

Packages

Version

Description

EB tresos 9 AutoCore OS

6.1.400

Stand-alone AUTOSAR compliant real-time, single-core Operating System. The OS is hardware and compiler dependent

EB tresos 9 - AutoCore Light Base Package

9.4.0

This product features hardware-independent communication stacks for LIN protocols, supports signal-based communication, and includes basic diagnostic interfaces for identification and coding. It also provides interfaces for MCAL driver integration and includes a robust watchdog stack for system reliability

EB tresos 9 - AutoCore OEM Extension Startup Package Application for Essentials

9.4.0

EB creates a generic EB tresos Studio project configuration that runs on the selected μC with customer defined compiler and compiler settings, integrating one set of project specific ECU and Diagnostic extracts

EB tresos 9 - Board Support Package MCAL

9.4.0

Integration of 3rd party MCAL modules into EB tresos Studio, for the requested μC, with pre-defined compiler and compiler settings

EB tresos 9 - Board Support Package Platform

9.4.0

Porting of the basic set of hardware-dependent packages (e.g. compiler abstraction, memory abstraction, μC

initialization, ..)

Micro HAL

0.1.0 Code drop

PSOC™ 4 HV family Micro Hardware Abstraction Layer (HAL) that abstracts the hardware-specific details of the microcontroller.

Auto PDL

1.10.1

PSOC™ 4 HV family Auto Peripheral Driver Library (PDL) is a collection of low-level drivers and APIs that enable developers to interact with the hardware peripherals of the PSoC™ 4 HV family microcontrollers.

Tools Components

Table 2. Tools components table

Tool chain

Version

Description

EB tresos Studio version

33.0.0

Tool for configuration and generation of basic software components in accordance with AUTOSAR

IAR Embedded Workbench for Arm, Functional Safety

8.50.10

IAR Embedded Workbench is a complete development toolchain with an optimized compiler, debugger, and analysis tools, streamlining embedded software development.

Prerequisites

  • KIT_PSoC4-HVMS-128K_LITE

  • MCU: CY8C4147LWE-HVS135X

  • Windows 10 64-bit host computer

Workflow​

Introduction

This configuration workflow introduces the end-to-end workflow for generating ECU software using EB tresos Studio.

  1. Provide Your Input Files

    • EB tresos Studio supports several standard file formats relevant for managing ECU configuration projects

      • EB tresos Studio supports AUTOSAR XML files containing:

        • System Description

        • LDF (Lin Description Format)

        • DBC

  2. Import and Configure

    • Once inputs are loaded, EB tresos Studio guides you through:

      • Importing definitions into the configuration environment

      • Transforming them into AUTOSAR-compliant components

      • Configuring software modules using graphical editors

      • Validating configurations to ensure completeness and correctness

  3. Generate Output Artifacts

    • After validation, EB tresos Studio produces all required build assets:

      • Code Generation for the configured AUTOSAR stack

Figure 1. Configuration Workflow

A computer screen shot of a computer screen AI-generated content may be incorrect.

Files in bundles

Table 3. Files in bundles table

File name

Short description

Document List


├──ACL-9.4.0_CY8C4147LWE_42036-B1109400_EvalKit.zip


│ ├──ACL-9.4.0_CY8C4147LWE_42036-B1109400_EvalKit


│ │ ├── 1.1_EB_tresos_installation_guide.pdf


│ │ ├── Documentation_Doc.uip


│ │ ├── Documentation_EBtresosStudio.uip


│ │ ├── EBtresosStudio_EBtresosStudio.uip


│ │ ├── EBtresosStudio_Wibui.uip


│ │ ├── setup.exe


Installation file “setup.exe” to start installing the EB tresos and user documentations

Installation​

Installation of EB tresos Studio​

For introductory guidance on EB tresos Studio workflows, refer to the following resources:

  • Tutorials available under the Tutorials tab on the

    Working with EB tresos Studio – Elektrobit

    webpage

  • The Getting Started materials on the same webpage

  • The

    Workflows view

    chapter in the EB tresos Studio User Guide, available at: $TRESOS_BASE/doc/2.-0_EB_tresos_Studio/2.1_Studio_documentation_users_guide.pdf

  • Install EB tresos Studio license

  • Install the workspace: the AutoCore OEM Extension Startup Package Application workspace is delivered as an uip package and is installed with the EB tresos Studio installer

  • The license key for the tool is given in your Infineon Developer Center (IDC) portal

    https://softwaretools.infineon.com/my/software

    (Ensure to log in to IDC using registered credentials)

Installation of IAR Embedded Workbench​

  1. Download the IAR Embedded Workbench installer from

    IAR Embedded Workbench for Arm Functional Safety, version 8.50.10

  2. Install IAR Embedded Workbench for Arm Functional Safety version 8.50.10. Installation instructions and license activation instructions are provided in

    Installation and Licensing Quick Reference

    /



    Note:

    Make sure to specify an installation directory without any spaces, for example C:\iar\EWARMFS850


    The license key for the tool is given in your Infineon Developer Center (IDC) portal

    https://softwaretools.infineon.com/my/software

    (Ensure to login to IDC using registered credentials)

  3. Copy the device support patch

    IAR_EWARM_Patch_PSoC4HV.zip

    from the PSOC™ DRIVECORE Smart End Point [Infineon, Elektrobit, IAR] V1.0 software delivery and unzip it on top of the IAR Embedded Workbench installation (for example C:\iar\EWARMFS850)

  4. Configure the compiler path by opening/EB/tresos/templates/Application_Lin_ACL/util/launch_cfg.bat, and change the value of TOOLPATH_COMPILER to the installation location of your compiler (for example C:\iar\EWARMFS850)

HW setup​


Complete Setup

Figure 3. Test bench setup


Note:
Note: A 12V supply (VBAT) is typically required for a PSOC-based LIN slave node to perform a remote wake-up.


LIN Connections to the board

Lin Channel and Lin Ports Pins Configuration as given below:

Table 4. LIN Connections to the board table

Lin channel

LIN0-CH1

Port Pin

Pin function

P2.0

LIN0 Receive Input

P2.1

LIN0 Transmit Output

P2.2

LIN0 Channel Enable

Demo​

Introduction​

The AutoCore OEM Extension Startup Package Application LIN provides a ready-to-use foundation for integrating EB tresos AutoCore Light 9 on a dedicated target platform.

It simplifies initial setup by preconfiguring essential LIN communication components, project structure, and platform-specific settings.

This demo accelerates development and reduces integration effort, enabling teams to focus on application functionality and customization.

LIN Slave Configuration​

AutoCore Light OEM Extension Startup Package Application LIN supports LIN communication for Application messages for Transmission and Reception and Diagnostics Services using Uds and BlPduR.

Table 5.LIN Slave Configuration

ID

PID

Type

Length

Direction

Description

Application

0x00

0x80

LIN

1 Byte

Rx

Pdu_CounterIn_0R_128R

contains byte 0 for CounterIn_

0R_128R signal

Application_Lin_ACL

0x01

0xC1

LIN

1 Byte

Tx

Pdu_CounterOut_1T_193T

contains byte 0 for CounterOut_1T_193T signal

Application_Lin_ACL

0x3C

--

LIN

8 Bytes

Rx

UDS physical request

Application_Lin_ACL

0x3D

--

LIN

8 Bytes

Tx

UDS physical response

Application_Lin_ACL

Baudrate is 19200 bits per second for LIN communication

Building and running the demo Application​

Importing the project

You must import the project into your EB tresos Studio workspace (for example C:/EB/tresos).

Step 1 : Navigate to the

tresos

installation and run

tresos_gui.exe

Figure 4. Step 1


Step 2: A pop-up asking to create the workspace directory, click

Yes

. A new workspace folder will then be automatically created inside the Tresos directory.

Figure 5. Step 2


Step 3: Tresos will open click on

Start

.

Figure 6. Step 3


Step 4: In the

File

menu, click

Import

.

Figure 7. Step 4


Step 5: In the

Import

window, click

Existing Projects into Workspace

, and then click

Next

.

Figure 8. Step 5


Step 6: Click

Select root directory

and browse to templates/<Application_Lin_ACL> and then click

Select Folder

.

Figure 9. Step 6


Step 7: In the

Import Projects

window, click

Copy projects into workspace

to copy the project into the default workspace and then Click

Finish

.

Figure 10. Step 7


In the

Project Explorer

view, you can:

► Open the project by double-clicking on the project name.\

Figure 11. Step 7a


► Open the configuration by clicking.

Figure 12. Step 7b


Building the project

Step 1: Ensure EB tresos Studio is not running.


Step 2: Navigate to your workspace directory

Step 3: In the Application_Lin_ACL/util directory, double-click launch.bat. The first startup of launch.bat takes some time.

Figure 13. Step 3


Step 4: In the command line window, execute this command: make generate

Figure 14. Step 4


Step 5: Execute this command: make or for compiling in parallel: make -j -O.

Figure 15. Step 5


The resulting binary file is in the Application_Lin_ACL/output/bin directory.

Executing batch files for the project

Batch files are available to execute automatically some project steps. The files are in the templates folder.

Figure 16. Batch files


Please follow the same sequence when running the batch files

  • __Start_Tresos.bat:

    Starts EB tresos Studio and automatically imports the projects if not previously imported than close the tresos

  • Application_Lin_ACL_RunSysRestoreWizard.bat:

    Performs a complete system update based on the supplementary files, it uses Execute multiple tasks Unattended Wizards

  • Application_Lin_ACL_Generate.bat:

    Generates tresos application

  • Application_Lin_ACL_Build.bat:

    Compiles the project using the build environment

  • Application_Lin_ACL_Clean.bat:

    Cleans the project using the build environment

Debugging the project

  1. Rename the executable file in C:\EB\tresos\workspace\Application_Lin_ACL\output\bin named CORTEXM0_CY8C4147LWE_Application_Lin_ACL.elf to CORTEXM0_CY8C4147LWE_Application_Lin_ACL.out

  2. Start IAR Embedded Workbench version 8.50.10

  3. Select

    Project>Create New Project

    and choose

    Externally built Executable:

    Figure 17.

    Create new project


  4. Select the name and location for your IAR Embedded Workbench project

  5. Add the executable file CORTEXM0_CY8C4147HV_basicTemplate.out to the project using

    Project>Add Files

  6. Open the Project Options and select the correct device:

    Figure 18.

    Select the device


  7. In the debugger options select CMSIS-DAP as the Debugger driver

    Figure 19.

    Selecting the Debugger driver


  8. Connect the board to your PC using the USB-cable provided:

    Figure 20.

    Connecting the board


  9. To start the debugger, select the project in the workspace window and click the

    Download and Debug

    button in the toolbar:



    The project can be reused whenever you rebuild your executable file. The debugger will notice if the executable file has been rebuilt and ask you if you want to reload it.

  10. Start LIN Simulator tool (PLIN View Pro/CANalyzer) to verify the LIN communication on the target. Configure PLIN View Pro as Master and send frame with ID 0x00 to wake up the target. Once the wakeup frame is received, target will start sending the frame with ID 0x01 with 1 second interval incrementing the data. Please note that the wake-up frame should be sent continuously within 4 second interval else the target will go in sleep state.

Development resources​

The SW-C composition consists of the following components:


► SWC_CyclicCounter

Only runnable from above Software components are utilized for C API implementation. Rte is integrated with BSW_SCHEDULER_ONLY mode for scheduling the BSW module main functions.

Support​

Contact support​

MyCases

In the event of any problems, issues, or questions, please do not hesitate to reach out to your designated Infineon contact or Field Application Engineer (FAE) for assistance. Alternatively, you can also submit a request through our ticketing system

https://mycases.infineon.com/

. For more information on how to use the myCases portal, please refer to this

document

.

Partners

By contacting support, you agree that your request and contact details are shared between

iSOFT

,

TASKING

, and Infineon.