About this document
Scope and purpose
The Release Notes contain an overview of the current and previous versions of InfineonSpice including changes, improvements and bug-fixes.
Intended audience
The intended audience for this document are users of InfineonSpice who want to be informed about the feature sets and changes for different versions of the software.
Product information
InfineonSpice is a full-fledged analog circuit simulator. It is a standalone, Windows-based software for comprehensive circuit design and visualization.
With its focus on ease of use and intuitiveness, it displays a welcome page when it starts, with tips to get started and quick access to the most important parts of the documentation.
A comprehensive list of basic and Infineon components such as product models are provided directly in the tool, ready for use in your designs. It is easy to import additional components from other sources that can be integrated in simulations with full support for the capabilities and performance of InfineonSpice.
Setting up and evaluating simulations is supported by easily accessible and transparent help and output features. Simulations are managed in self-contained projects, which makes it convenient to collaborate on and share designs. In addition, Infineon provides a constantly growing number of virtual reference designs for many applications via the tool.
You can use it both if you have never worked with InfineonSpice and if you are an experienced user. It assumes that you are familiar with designing and testing analog circuits and simulating them with SPICE. If you require more information about either topic, please consult appropriate documentation.
Description of releases
Here the features and changes are listed for each version - starting with the latest.
Version 2025.03
The list below contains the features, enhancements and Bug Fixes which are new in this product release.
Features
- Plots can be moved to another group of plots that share the same axis
- S-parameter file support is enabled via Additional Netlist Commands (no GUI flow)
- PWL sources include a file subtype that allows sourcing characteristics from a given file
- A new "Ask the Community" link is available under the Help menu
- Support of AC Analysis setup
- Resistor models support the "T_ABS" parameter
- Files with extensions “.spi,” “.tit,” and “.cir” are interpreted as libraries
- A Lossless Transmission Line component has been added to Basic Components
Enhancements
- The Download Manager's content-loading performance has been significantly improved
- The user interface visually indicates when the "Snap-to-Grid" feature is disabled
- The size of plots in the Waveform Viewer has been adjusted for better usability
- Input validation prevents improper entries for additional model libraries in Simulation Setup
- The file size of SVG schematic exports has been significantly reduced
- Renaming is now possible for opened files in the Design Environment
- Buttons in the Simulation Environment are disabled when the corresponding action is unavailable
- Anti-aliasing has been introduced for Waveform Viewer plots to improve visual clarity
- Newly introduced parameters in the Simulation Environment receive a unique name automatically
- The "Stop Simulation" button has been replaced with a more prominent option
- Drag-and-drop functionality initiates a copy when objects are moved to another project, where applicable
- The robustness of the TITAN simulation engine has been improved for high-power applications
- Exporting to network drives is supported
- Upon import, a new project name is proposed based on the imported file’s name
- Minor user interface enhancements have been implemented
Bug Fixes
- Crash occurring when removing a project while its Waveform Viewer remains open
- Issue in the Waveform Viewer where horizontal scrolling with the mouse wheel was not possible
- Incorrect syntax highlighting in library files
- Text cut-off issue in the Symbol Generation Options dialog
- Crash that occasionally appeared when moving devices within a schematic
- Incorrect node permutations for Voltage-Controlled Switches
- Issue with the "Zoom All" feature for logarithmic axis presentations in the Waveform Viewer
Version 2025.01
The list below contains the features which are new in this product release.
Features
- Workspace
- Creation, export and import of projects
- Easy import and usage of own libraries and models
- Offer download of missing Infineon Components
- Schematic Editor
- Direct access to Infineon product models
- Download of Infineon Components
- Building circuits with Infineon Components and Basic elements
- Downloadable Reference Designs (example schematics)
- Simulation Setup
- Simulation Profiles
- Analysis (Transient/OP/DC)
- Export and import of parameter lists
- Plot settings
- Additional Netlist commands
- Waveform Viewer
- Waveform comparison
- Waveform export
- Waveform calculator
- Netlister
- Deterministic netlisting
Known limitations
This chapter makes the reader aware of product limitations as well as circumstances where unexpected behavior may occur.
- The Plot Setup for AC analysis is still under development (e.g., function naming might be unintuitive)
- A Symbol library does not exist
- Not all Infineon Components are yet visible
- Some compatibilities issues of models used in other simulators
- A multidimensional Sweep is not available yet
- Digital primitives are not available for placement in the schematic yet
Sources
Sources of some used free and open source software:
- https://softwaretools.infineon.com/tools/com.ifx.tb.tool.fossinfineonspiceeigen
- https://softwaretools.infineon.com/tools/com.ifx.tb.tool.fossinfineonspicelibquadmath
- https://softwaretools.infineon.com/tools/com.ifx.tb.tool.fossinfineonspiceqt5
- https://softwaretools.infineon.com/tools/com.ifx.tb.tool.fossinfineonspicesuitesparse
Disclaimer
Trademarks
All referenced product or service names and trademarks are the property of their respective owners.
Important notice
The information given in this document shall in no event be regarded as a guarantee of conditions or characteristics (“Beschaffenheitsgarantie”).
With respect to any examples, hints or any typical values stated herein and/or any information regarding the application of the product, Infineon Technologies hereby disclaims any and all warranties and liabilities of any kind, including without limitation warranties of non-infringement of intellectual property rights of any third party.
In addition, any information given in this document is subject to customer’s compliance with its obligations stated in this document and any applicable legal requirements, norms and standards concerning customer’s products and any use of the product of Infineon Technologies in customer’s applications.
The data contained in this document is exclusively intended for technically trained staff. It is the responsibility of customer’s technical departments to evaluate the suitability of the product for the intended application and the completeness of the product information given in this document with respect to such application.
Warnings
Due to technical requirements products may contain dangerous substances. For information on the types in question please contact your nearest Infineon Technologies office.
Except as otherwise explicitly approved by Infineon Technologies in a written document signed by authorized representatives of Infineon Technologies, Infineon Technologies’ products may not be used in any applications where a failure of the product or any consequences of the use thereof can reasonably be expected to result in personal injury.
Imprint
edition2025-06-30
Published by
Infineon Technologies AG
81726 Munich, Germany
© 2025 Infineon Technologies AG
All Rights Reserved.
Do you have a question about any aspect of this document?
Email: erratum@infineon.com
Document reference
deo1706861927848