USB Configurator Guide¶
About this document
Version
2.40
Scope and purpose
The USB Configurator main use is to create device descriptor configuration and generate code with the descriptor tables as part of the device firmware.
Intended audience
This document helps application developers understand how to use the USB Configurator as part of creating a ModusToolbox™ application.
Document conventions
Convention |
Explanation |
---|---|
Bold |
Emphasizes heading levels, column headings, menus and sub-menus |
Italics |
Denotes file names and paths. |
Courier New |
Denotes APIs, functions, interrupt handlers, events, data types, error handlers, file/folder names, directories, command line inputs, code snippets |
File > New |
Indicates that a cascading sub-menu opens when you select a menu item |
Abbreviations and definitions
The following define the abbreviations and terms used in this document:
API – application programming interface
BOS – binary device object store
CDC – communication device class
Configurator – A GUI-based tool used to configure a resource.
Descriptor – A defined-format data structure used by USB devices to report their attributes to a USB host or in other words a piece of stored data that indicates how other data is stored.
Endpoint – A uniquely addressable portion of a USB device that is the source or sink of information in a communication flow between the host and device.
HID – human interface device
USB – universal serial bus device
Reference documents
Refer to the following documents for more information as needed:
1. Overview¶
The Universal serial bus (USB) Configurator is a stand-alone tool included with the ModusToolbox™ software to configure USB device descriptors. See the Supported descriptors section for a list of supported USB descriptors. After configuring and saving a USB device descriptor, the USB Configurator generates configuration files that store USB device descriptors and other information (see Code generation) used by the USB device middleware configuration and operation.
1.1 Supported middleware¶
Name |
Link |
---|---|
USB device middleware library |
2. Launch the USB Configurator¶
There are several ways to launch the USB Configurator, and those ways depend on how you use the various tools in ModusToolbox™.
2.1 make command¶
As described in the ModusToolbox™ user guide “Build System” chapter, you can run numerous make commands in the application directory, such as launching the USB Configurator. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:
make config_usbdev
or
make open CY_OPEN_TYPE=usbdev-configurator
If the application has an existing USB configuration (.*cyusbdev) file, this command opens the USB Configurator GUI for the specific application in which you are working.
If there is no *. cyusbdev file, then this command launches the USB Configurator with default configuration. You must open an existing *. cyusbdev file or create a new one for the application in which you want to configure the USB Configurator.
2.2 Eclipse IDE¶
If there is a *.cyusbdev file in the application folder, you can launch the USB Configurator GUI directly from the
Eclipse IDE using any of the following methods:
Double-click on the *.cyusbdev file in the application.
Right-click on the top-level application folder, and select ModusToolbox™ > USB Configurator.
Click on the USB Configurator link in the Quick Panel, under Configurators.
Refer to the Eclipse IDE for ModusToolbox™ user guide for more details.
If there is no *.cyusbdev file in the application folder, the options from the menu and Quick Panel read USB Configurator (new configuration). Select either option, and the USB Configurator opens with default configuration (*.cyusbdev) that will be saved to the design.cyusbdev file in the application folder. Refer to the USB device middleware library for more details about this code.
2.3 Executable (GUI)¶
If you don’t have an application or if you just want to see what the configurator looks like, you can launch the USB Configurator GUI by running its executable as appropriate for your operating system (for example, double-click it or select it using the Windows Start menu). By default, it is installed here:
<install_dir>/ModusToolbox/tools_<version>/usbdev-configurator-<version>
On Windows, launch the tool from the Start menu. For other operating systems, navigate to the install location and run the executable. When opened this way, the USB Configurator opens with an untitled configuration file (*.cyusbdev). Save it as a new file and provide a file name, or open another existing *.cyusbdev file.
2.4 Executable (CLI)¶
You can run the usbdev-configurator executable from the command line. There is also a usbdev-configurator-cli executable, which re-generates the source code based on the latest configuration settings from a command-line prompt or from within batch files or shell scripts. The exit code for the usbdev-configurator-cli executable is zero if the operation is successful, or non-zero if the operation encounters an error. To use the usbdev-configurator-cli executable, you must provide at least the –config argument with a path to the configuration file.
For more information about the command-line options, run the usbdev-configurator or usbdev-configurator-cli executable using the -h option.
3. Quick start¶
This section provides a simple workflow for how to use the USB Configurator.
Configure the device descriptors hierarchy in the Device Descriptor Tree pane.
Configure device descriptor parameters in the Parameters pane.
The Parameters pane contains a subpane for HID descriptor (HID Report pane).
Save the configuration. See Code generation.
Use the generated structures as input parameters for functions in your application.
4. Code generation¶
The USB Configurator generates header (.h) and source (.c) files that contain relevant firmware used by the USB Device middleware configuration and operation. The firmware contains arrays to store USB Device descriptors, structures that help the middleware to access descriptors, middleware and classes configuration structures, and a set of defines. The generated files cycfg_usbdev.h and cycfg_usbdev.c are located in the GeneratedSource folder next to the *. cyusbdev file.
Refer to the USB device middleware library for more information about this code.
5. GUI description¶
The USB Configurator GUI contains menus, toolbars, panes, and a subpane used to configure device descriptors.
6. Toolbars¶
6.1 Descriptor toolbar¶
Provides the basic buttons from the Menus to create, open, edit, and save files.
Also, the descriptor toolbar provides buttons to configure the descriptors hierarchy:
Add new descriptor – Click this button to create a new descriptor.
Delete selected descriptor – Removes the selected descriptor.
Import descriptor – Select a descriptor from the pull-down menu to transfer it into the configuration.
Expand all tree items – Clicking this button displays all the items in the Device Descriptors Tree.
Collapse all tree items – Clicking this button leaves only the Device Descriptors Tree visible.
Move up – Shifts up the selected descriptor.
Move down – Shifts down the selected descriptor.
6.2 HID Report toolbar¶
The HID Report toolbar provides the buttons to configure an HID descriptor report.
Add HID report item – Creates a new HID report item.
Delete HID report item – Removes the selected HID report item.
Load HID report – Opens an HID report file into the current HID Descriptor.
Import HID report – Transfers an HID report item into the configuration for the current HID Descriptor.
Move up HID report item – Shifts up an IDHIFDHID report item.
Move down HID report item – Shifts down an IDHIFDHID report item.
6.3 Array editor toolbar¶
The Array editor toolbar provides the buttons to edit array elements.
Add new element – Creates a new element.
Delete element – Removes the selected element.
Move up element – Shifts up an element.
Move down element – Shifts down an element.
7. Panes¶
The USB Configurator contains two panes that display information about descriptors and their parameters:
7.1 Device Descriptors Tree pane¶
This pane shows the descriptors hierarchy.
All the descriptors have their own hierarchy that can be created when their parent is selected. However, the Device Descriptors Tree is the root descriptor.
To add specific descriptors, for example, CDC Interface descriptor or HID descriptor, add a special parent descriptor:
Add CDC interface descriptor for CDC descriptor
Add HID alternate settings for HID descriptor.
7.2 Parameters pane¶
This pane shows configuration information for the selected descriptor.
Note
The Parameters pane has different controls to edit different parameters (text box, combo box, or multi-line text box). Most parameters have a text box as the editing control.
Vendor-defined items – Some string parameters or HID report items, such as iSerialNumber, have a combo box with a list of predefined items. The “Empty” value is selected by default. To specify a value that is not on the list, select “Vendor-defined.” The combo box will change to a text box to type an appropriate value. To return to the combo box, erase the value and leave the control.
String pool – Parameters such as iChannelNames in AC Processing Unit of Audio Interface descriptor 1.0 support a string pool and require a multi-line text box. To insert several strings, use an end-line separator.
Read-only parameters – There are two types of read-only parameters: predefined bDescriptorType or auto-calculated bConfigurationValue.
Array parameters – Parameters such as bSubordinateInterface in union with Communication Alternate Settings is an array. Use “;” to separate elements. Also, you can open the Array editor dialog to set the parameters using the [ … ] button.
Hexadecimal/Decimal – When a value starts with “0x,” it is parsed as a hexadecimal value. Otherwise, it is parsed as a decimal.
Map and bit fields – Some parameters, such as bmAttributes, are read-only by themselves. However, you can insert them using the related bit fields below them in the parameters list. The bit fields size is 0B. Their name starts with the name of a field whole part, plus the bits for which they are responsible. For example, bmAttributes(1-0): Transfer Type.
8. Notice List¶
The Notice List combines notices (errors, warnings, tasks, and notes) from many places in the configuration into a centralized list. If a notice shows a location, double-click the entry to show the error or warning. Also, you can read an error message in a tooltip.
When you try to save the configuration with errors, a message shows the problem to fix.
9. Supported descriptors¶
All supported descriptors are described by USB Implementers Forum, Inc. You can find more details at http://www.usb.org.
The supported descriptors:
Device, Configuration, IAD (Interface association descriptor), Interface, Endpoint descriptors
Device descriptor (Billboard), Device Qualifier descriptor
Audio Interface descriptor 1.0 and 2.0
CDC Interface descriptor
HID descriptor and HID Report descriptor
BOS descriptors (USB 2.0 Extension descriptors, Container ID, Billboard Capability descriptor, and Billboard Alternate Mode Capability descriptor)
MS OS String descriptor
Note
The Interface Descriptor is represented by the two items to build a tree structure: Interface Descriptor with an empty parameters pane and Alternate Settings with all Interface Descriptor parameters.
Class-Specific AS Encoder/Decoder Descriptors from USB Audio v2.0 are not supported.
10. Known issues, limitations, and workarounds¶
The USB Configurator supports import from the HID Descriptor tool. Current version 2.40 contains an error related to strings. Per spec HID1.11, string items have such values:
String Index 0111 10 nn
String Minimum 1000 10 nn
String Maximum 1001 10 nn
However, the HID Descriptor tool generates:
String Index 0110 10 nn
String Minimum 0111 10 nn
String Maximum 1000 10 nn
Before importing, fix these items manually in the file generated with the HID descriptor tool.
11. Version changes¶
This section lists and describes the changes for each version of this tool.
Version |
Change descriptions |
---|---|
1.0 |
New tool. |
1.1 |
Updated the icons to be standard. Added Notice List. |
2.0 |
Changed the user configuration storage location from the header file to the *.cyusbdev file. Added New, Save As, Reset View commands. Changed the Load command to Open. Updated the icons. Removed the CUSTOM item from HID Report. Removed the functionality to launch the USB Configurator from the Device Configurator. |
2.1 |
Added the Undo/Redo feature. |
2.20 |
Updated versioning to support patches. Added Copy feature to the Notice List. Added the calculation of the Endpoint Address for a new Endpoint Number. |
2.30 |
Removed the command-line generate options: -g and –generate. |
2.40 |
Added Device Descriptor Tree as the root element. Added: Device Qualifier Descriptor with Other_Speed_Configuration Descriptor, Billboard Capability Descriptor, and Billboard Alternate Mode Capability Descriptor. Added an Array Editor dialog for array fields. Updated the GUI by moving to Qt-5.15.2 Removed: the migration of configuration to the current XML format – configuration saved in the comments in generated HEADER files (the old method). |
Revision history
Revision |
Date |
Description |
---|---|---|
** |
11/20/2018 |
New document. |
*A |
02/26/2019 |
Added Notice List. |
*B |
10/16/2019 |
Updated to version 2.0: changed the user configuration storage location from the header file to the *.cyusbdev file. Added New, Save As, Reset View commands. Changed the Load command to Open. Updated the icons. Removed the custom item from HID Report. Removed the functionality to launch the USB configurator from the device configurator. Resubmitted to update the description of how to open from the IDE. Fixed footer issue. |
*C |
03/27/2020 |
Added the Undo/Redo feature. |
*D |
09/01/2020 |
1. Updated versioning to support patches. 2. Added copy feature to the Notice List. 3. Added the calculation of the Endpoint address for a new endpoint number. |
*E |
03/11/2021 |
2.30 removed the command-line generate options: -g and –generate. |
*F |
09/22/2021 |
Updated to version 2.40. |