Library Manager User Guide¶
About this document
Version
1.40
Scope and purpose
This document provides information and instructions for how to use the ModusToolbox™ Library Manager.
Intended audience
Read this document to learn how to manage ModusToolbox™ BSPs and libraries for your application.
Document conventions
Convention |
Explanation |
---|---|
Bold |
Emphasizes heading levels, column headings, menus and sub-menus |
Italics |
Denotes file names and paths. |
Courier New |
Denotes APIs, functions, interrupt handlers, events, data types, error handlers, file/folder names, directories, command line inputs, code snippets |
File > New |
Indicates that a cascading sub-menu opens when you select a menu item |
Reference documents
Refer to the following documents for more information as needed:
1. Overview¶
The Library Manager provides a GUI to select which Board Support Package (BSP) should be used when building a ModusToolbox™ application. The tool collects a list of available and currently selected BSPs and libraries, as well as all the necessary metadata from a webservice. The tool allows you to add and remove BSPs and libraries, as well as change their versions.
In ModusToolbox™ 2.2 and later, we structured applications with the MTB flow and .mtb files. Using this flow, applications can share BSPs and libraries. If needed, different applications can use different versions of the same BSP/library. Sharing resources reduces the number of files on your computer and speeds up subsequent application creation time. Shared BSPs, libraries, and versions are located in a “mtb_shared” directory adjacent to your application directories. You can easily switch a shared BSP or library to become local to a specific application, or back to being shared.
Most example applications use the MTB flow. However, there are still older applications that use the previous flow, now called the LIB flow (.lib files), and these applications generally do not share BSPs and libraries. ModusToolbox™ fully supports both flows, but it only supports one flow or the other for a given application. If an application uses the MTB flow, the system will process .mtb files only and ignore any .lib files.
1.1 Version¶
All BSPs and libraries have a version. Versions apply to both the MTB and LIB flows. See also BSP and library versions later in this document.
1.1.1 Dynamic¶
If a BSP or library uses a “Latest” tag, then it is dynamic. ModusToolbox™ will download and use the appropriate version specified in the manifest and attempt to resolve any potential conflicts with different library versions. Using a “Latest” tag means the library will update to the latest version whenever you run the make getlibs command, including when you click the Library Manager Update button.
1.1.2 Fixed¶
By selecting a specific version from the pull-down menu in the Library Manager GUI, you assign a fixed version to the BSP or Library that does not change, unless you manually change it.
1.2 Manifests¶
Manifests are XML files that tell the Library Manager how to discover the list of available BSPs, libraries, and library dependencies. Manifests apply to both the MTB and LIB flows. For more information, refer to the Manifest chapter in the ModusToolbox™ user guide.
1.3 MTB flow¶
The MTB flow applies to ModusToolbox™ 2.2 and later releases. This flow uses .mtb files to manage libraries. The Library Manager runs the make getlibs command to process the .mtb files, pull the libraries from the specified git repos, and store them in the specified location. The system also creates a file called mtb.mk in the application’s libs subdirectory. The build system uses that file to find all the libraries required by the application.
The following shows the Library Manager for a typical PSoC 6 BSP and the MTB flow, with BSPs and Libraries tabs. The key items are the Shared column and the lock symbols for libraries that are included because they are dependendies of other libraries. See Working with BSPs/libraries (MTB flow) for more details about using the tool in the MTB flow.
The following concepts are key to understanding the MTB flow:
1.3.1 .mtb file¶
This file provides information about the associated BSP/library. It contains:
A URL to a git repository somewhere that is accessible by your computer such as GitHub.
A git Commit Hash or Tag that tells which version of the library that you want.
A path to where the library should be stored.
A typical .mtb file looks like this:
https://github.com/cypresssemiconductorco/TARGET_CY8CKIT-062S2-43012/#latest-v1.X#$$ASSET_REPO$$/TARGET_CY8CKIT-062S2-43012/latest-v1.X
The variable $$ASSET_REPO$$ points to the root of the shared location. If you want a library to be local to the application instead of shared, use $$LOCAL$$ instead of $$ASSET_REPO$$.
1.3.2 Direct dependency¶
This is a library or BSP that is directly referenced by an application. In many applications, the only direct dependency is a BSP. In other applications, there will be additional direct dependencies such as Wi-Fi or Bluetooth libraries. You may also have changed the location or version of an indirect library, which makes that library a direct dependency.
You manage the .mtb files for direct dependencies, and .mtb files should be checked into source control along with your application source code. A .mtb file for a direct dependency is typically stored in the application’s deps subdirectory by default. You can store it anywhere inside the application except in the application’s libs subdirectory.
1.3.3 Indirect dependency¶
This is a library that was included indirectly as a dependency of a BSP or another library. The system stores the code in the appropriate directory and chooses the appropriate version specified in the manifest, as well as resolves any potential conflicts with different library versions.
The system finds indirect dependencies for each library using information that is stored in a manifest file. For each indirect dependency found, the Library Manager places an .mtb file in the application’s libs subdirectory. The tool also creates a locking_commit.log file in the application’s deps subdirectory to record the locked release version of those libraries.
You do not manage .mtb files for indirect dependencies, and they do not need to be checked into source control. The .mtb file for an indirect dependency is stored in the application’s libs subdirectory and must not be moved.
1.3.5 Local¶
A local BSP/library includes the code for the associated .mtb file, and the BSP/library is used only for a specific application. The local BSP/library is stored in the libs subdirectory of the specific application. These BSPs/libraries do not need to be checked into source control. All the code can be re-downloaded at any time from the information in the .mtb file.
If you change BSPs and libraries to be local to an application (see Share/unshare BSPs and libraries later in this guide), then the source code for these are located in the libs subdirectory inside the application directory.
1.4 LIB flow¶
Some older applications before ModusToolbox™ 2.3 use the LIB flow, where libraries are managed with .lib files.
In the Library Manager, these applications also have the BSPs and Libraries tabs like the MTB flow, but they do not have a Shared column and they do not distinguish between libraries that are included by the application vs. libraries that are included because other libraries depend on them. See Working with BSPs/libraries (LIB flow) for more details.
Some applications also have Shared BSPs and Shared Libraries tabs.
These are the concepts for the LIB flow.
Local lib file – This is a .lib file present in the project whose library is being edited.
Shared lib file – This is a .lib file that is used indirectly via the shared library mechanism.
Target project – This is the project directory whose library is being edited.
Fully editable mode – You can add, remove, and change the version of the library.
Restricted edit mode – You can manage the version of the selected library, but you cannot add or remove the library.
2. Launch the Library Manager¶
There are numerous ways to launch the Library Manager, and that depends on how you use the various tools included with ModusToolbox™ software.
2.1 make command¶
As described in the ModusToolbox™ user guide build system chapter, you can run numerous make commands in the application directory, such as launching the Library Manager. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:
make modlibs
This command opens the Library Manager GUI for the specific application in which you are working.
2.2 Eclipse IDE¶
If you use the Eclipse IDE for ModusToolbox™, you can launch the Library Manager for the selected application.
In the Project Explorer, right-click on the project and select ModusToolbox™ > Library Manager <version>.
You can also click the Library Manager link in the IDE Quick Panel.
Similar to the make command method, launching the Library Manager using the Eclipse IDE opens the tool for the selected application. Refer to the Eclipse IDE for ModusToolbox™ user guide for details about the IDE.
2.3 Stand-alone GUI mode¶
You can also launch the Library Manager in stand-alone mode by running its executable as appropriate for your operating system (for example, double-click it or select it using the Windows Start menu). By default, it is installed here:
<install_dir>/ModusToolbox/tools_<version>/library-manager-<version>
When run in stand-alone mode, the Library Manager opens with the target directory set as <user-home> or as the directory selected from a previous stand-alone session.
If you haven’t opened the Library Manager tool previously, it starts at your home directory and looks for directories with a Makefile, and then it opens the first application it finds in that directory. If the tool does not find an application, it doesn’t display any BSPs or libraries.
Click the Browse… button next to the Directory field and navigate to the directory that contains one or more applications. Then, select from the Project pull-down menu as needed.
Note
The next time you open the Library Manager in stand-alone mode, it will open with the most recently selected application.
2.4 Offline mode¶
If the Library Manager cannot connect to the internet when launching, it displays a message in the console that it cannot access the manifest file. Adjust your internet and/or proxy settings (from the Settings menu), and then click the Retry button to re-read library information.
If you have the ModusToolbox™ Offline Content bundle installed and run the Library Manager without an internet connection, the following dialog displays:
If you click Yes, the Library Manager switches to offline mode and reads library information from the offline content bundle. If you click No, you can adjust internet and/or proxy settings, and then click Retry to re-read library information. Refer to the ModusToolbox™ user guide for more details about the offline content bundle.
2.5 Non-GUI command line interface (CLI)¶
You can also open a non-graphical interface from the command line. However, there are only a few reasons to do this in practice. The primary use case would be part of an overall build script for the entire application. For information about command line options, run the library-manager-cli executable using the -h option.
3. Working with BSPs/libraries (MTB flow)¶
This section covers various ways to update BSPs and libraries for the MTB flow, including:
Update indirect dependency libraries
Add/remove BSPs or libraries
Select Active BSP
Share/unshare BSPs and libraries
Change BSP/library version
When using the MTB flow, the BSPs and Libraries tabs show selection check boxes to the left of each of the listed BSPs and libraries. Selected check boxes represent BSPs/libraries included in the application, while those without selected check boxes are not included. Check boxes under the Shared column indicate if a BSP/library is shared or local, and each BSP/library shows a version under the Version column.
When you make a change to a BSP or library, an asterisk (*) displays next to it indicating a change is pending, but it has not yet been updated. Changes will take effect when you click the Update button.
When a BSP/library has a newer version available than the one currently selected, a “newer version” symbol displays next to the version number, indicating that a newer major or minor version is available.
If you hover the mouse cursor over the symbol, a tooltip displays the type of version.
3.1 Update indirect dependency libraries¶
Several libraries included in your application show a lock symbol by default. This symbol indicates that a library is an indirect dependency, and it is required by the BSP and/or another library.
These libraries cannot be removed using the Library Manager; however, you can change whether it is shared or not, and you can select a different version.
When you make a change to an Indirect Dependency library, the lock symbol changes to regular check box. This indicates that after you click Update, the library is now a direct dependency and it is your responsibility to manage it either as a local library and/or with the selected version.
To change the library back to an Indirect Dependency, click on the check box. The icon reverts back to the lock symbol, and the Shared and Version settings revert back to the defaults. You must click the Update button to process the changes.
3.2 Add/remove BSPs¶
Add BSPs to your application and remove them by selecting and deselecting the check boxes to the left of the BSPs. Click the Update button to process the change(s). The message console displays the progress and indicates when changes are complete.
Note
Use caution when removing all Cypress BSPs from your application. BSPs are responsible for* ensuring key libraries are present, including “psoc6make” for PSoC 6 projects and “baselib” for Bluetooth projects. Before you remove all Cypress BSPs, make sure a custom BSP is present in your application; otherwise, the Library Manager tool may not function correctly. For information on creating and customizing BSPs, refer to the ModusToolbox™ user guide.
3.3 Select Active BSP¶
The Active BSP for the application is shown in bold text with “(Active)” next to it. An application can only have one active BSP for which all settings apply. If your application has more than one BSP included (shown with selected check boxes), you can use the Active BSP pull-down menu to select one of the other BSPs to be active.
When you click the Update button, the system displays progress in the message console and updates your application’s makefile “TARGET=” field to specify the new BSP as active.
3.5 Change BSP/library version¶
Libraries have a specific version, by default. You can change a BSP/library version by selecting the pull-down menu under the Version column and choosing another version. See BSP and library versions for a detailed description.
When you change versions for a shared BSP/library, the tool creates a new subdirectory for the added version to ensure that the existing version is available for other applications. For example:
However, when you change a version for a local BSP/library, the system will not create a new local subdirectory. Instead, the version of the BSP/library will just be updated with the appropriate tag.
4. Working with BSPs/libraries (LIB flow)¶
This section covers various ways to update BSPs and libraries for the LIB flow, including:
Add BSPs/Libraries
Remove BSPs/Libraries
Update Shared BSPs/Libraries
Change BSP/Library Version
When using the LIB flow, the BSP and Libraries tabs show selection check boxes next to each of the listed BSPs and libraries supported in the application. Selected check boxes represent BSPs/libraries already included in the application, while those without selected check boxes are not included. The Active BSP for the application is shown in bold text with “(Active)” next to it.
Note
When you make a change to a BSP or library, an asterisk () displays next to it indicating a change is pending, but it has not yet been updated. Changes will take effect when you click the **Update* button.
4.1 Adding BSPs/libraries¶
To add a BSP/library to your application, select the check box for one or more item on each tab and click Update. The tool starts updating the project and displaying progress in the status box.
When complete, the additional items will display with selected check boxes.
4.2 Remove BSPs/libraries¶
To remove a BSP/library from your application, deselect the check box for one or more item on each tab, and click Update.
Note
Use caution when removing all Cypress BSPs from your application. BSPs are responsible for* ensuring key libraries are present, including “psoc6make” for PSoC 6 projects and “baselib” for Bluetooth projects. Before you remove all Cypress BSPs, make sure a custom BSP is present in your application; otherwise, the Library Manager tool may not function correctly. For information on creating and customizing BSPs, refer to theModusToolbox™ user guide.
Click Update and the tool starts updating the project and displaying progress in the status box.
When complete, the removed items will display in the Library Manager without selected check boxes. On disk, the libraries are removed by creating a special .lib file with a commit set to a sentinel value that indicates the library is removed.
5. GUI description¶
5.2 Fields¶
The Library Manager contains the following fields at the top of the GUI:
Directory – Location of the application’s top-level directory, which contains one or more ModusToolbox™ makefile projects. Use the Browse… button to select a different directory, if needed.
Project – Location of the application’s selected makefile. Use the pull-down menu to select another project, if applicable.
Active BSP – The name of the currently active target BSP. Use the pull-down menu to choose any of the boards with a selected check box in the BSPs tab. You can have multiple sets of BSP code in a project; however, the make project is built only for the selected Active BSP.
Filter text – Field used to show only the BSPs/libraries that match the text entered.
Show/Hide – Toggle to show only the BSPs/libraries with check boxes selected or show all BSPs/libraries. If there is filter text, then only BSPs/libraries with check boxes selected and BSPs/libraries with matching text will be shown instead of all.
Collapse All – Click to collapse all item trees.
Expand All – Click to expand all item trees.
5.3 Tabs¶
The Library Manager may display one or more of the following tabs, depending several variables:
BSPs tab – Shows available BSPs and versions. This tab is hidden if there are no BSPs in the project and the project type is a library project or if the project uses shared BSPs.
Libraries tab – Shows libraries supported by the Active BSP. This tab is hidden if the project type is a library project and if the project contains zero local libraries.
Shared BSPs tab (LIB Flow) – Shows a read-only view of BSPs that are available via the LIB flow shared library mechanism. This tab is hidden if the project is not using any shared BSPs or if the project type is a library project.
Shared Libraries tab (LIB Flow) – Shows a read-only view of LIB flow code libraries that will be used by the project. This tab is hidden if the project is not using any shared libraries or if the project type is a library project.
5.3.2 BSP and library versions¶
The Library Manager contains a Version column for each BSP and library shown in the tool. You can select “Latest X.Y release” or “X.Y.Z release.” These represent tags for versions of BSPs/libraries in Cypress GitHub repos:
The “latest-vX.Y” tag is updated whenever you run make getlibs (such as by clicking the Update button) to point to a newer, backward-compatible version of the library when Cypress releases it.
The “release-vX.Y.Z” tag always points to a specific, official release, and it does not change.
When you create a new application from a Cypress code example, the application converts BSPs and libraries to use the “X.Y.Z release” version, by default. This ensures that they will not be updated automatically, unless you change the version to “Latest X.Y release.”
When you open the Library Manager for that application and make any kind of change, the change summary displays in the console. If a “latest-vX.Y” tag has a newer version, the console displays a warning about the “latest-vX.Y” tag. It includes a hyperlink to open a dialog that explains how the “latest-vX.Y” tag auto-update works.
If you click Update, all items with the “latest-vX.Y” tag will be moved to the newer version, even if you didn’t make changes them.
5.4 Buttons¶
The Library Manager contains the following buttons to perform the described actions:
Update – Use this button to update your project with changes made in the Library Manager. This action runs the make getlibs command, and you can use it at any time even if you made no changes. You might do this for a project that has no libraries yet or to update the libraries specified as “Latest” to get any updates.
Close – Use this button to close the Library Manager.
Retry – This button displays if the message console indicates that the tool cannot access the manifest file. Use the Retry button after adjusting your internet and/or proxy settings to check if the tool can access the manifest file.
5.5 Message console¶
The area below the BSPs and Libraries displays various messages, such as when you select/deselect an item, click the Update or Retry button, or select Offline mode.
5.6 Status indicator¶
At the bottom of the tool, the status indicator displays as faded in offline mode and displays as normal in online mode. If you hover over the indicator, a tooltip displays.
6. Manual library management¶
If a library is not in a manifest file, it will not appear in the Library Manager and will need to be managed manually. Regardless of the library management flow, this is a two-step process:
Acquire the library
Acquire the library’s dependencies
These steps can be done several different ways depending on the construction of the library and the library management flow being used by the application. Note that for (custom) BSPs, the Project Creator tool simplifies this process greatly. You can still use the other methods on BSPs if you want to include a custom BSP into an existing application.
Note
By manually managing libraries, all dependencies will be included directly in the application. Indirect dependencies only occur in the MTB flow when libraries and dependencies are included in manifest files as described in the indirect dependency section.
6.1 Acquiring a library (MTB flow)¶
There are three basic ways to get a library that isn’t in a manifest file using the MTB flow:
Requirements |
Method |
---|---|
Library is hosted in a Git repo |
Create a .mtb file for the library in the application’s deps subdirectory. Run make getlibs from the application’s root directory. The library can be local or shared based on the .mtb file contents. |
Any library Library is local to app |
Use copy, git clone, or use some other revision control system to pull the library into the application. It can be located anywhere except the application’s libs subdirectory. |
Any library Library is in a shared location |
Use copy, git clone, or use some other revision control system to pull the library into a shared location. Edit the SEARCH variable in the application’s Makefile to point to the library. |
Custom BSP |
Use copy, git clone, or use some other revision control system to get the BSP somewhere on disk if it isn’t already. The location is not important. It will be copied into the application folder during project creation. Use the Project Creator Import function to select the BSP. The custom BSP will be copied into the application. See the Project Creator user gui de for details. |
Once you have a library, the next step is to get its dependencies. The methods used depend on whether you are using the MTB flow or the LIB flow.
6.2 Acquiring dependencies (MTB flow)¶
There are several ways to acquire dependencies:
Requirements |
Method |
---|---|
Library contains mtbx files for its dependencies |
Run make import_deps followed by make getlibs from the application’s root directory (see import_deps for details). |
Dependencies can be local |
|
Library does not contain mtbx files but does contain lib files for its dependencies |
Run make lib2mtbx, then make import_deps and finally make getlibs from the application’s root directory (see lib2mtbx and import_deps for details). |
Dependencies will be local |
|
Dependencies are in a manifest |
Use the Library Manager. |
Dependencies are hosted in git repos |
Create a .mtb file for each dependency in the application’s deps subdirectory. Run make getlibs from the application’s root directory. The dependencies can be local or shared based on the .mtb file contents. |
Any Dependency |
Use copy, git clone, or use some other revision control system to pull the library into the application. It can be located anywhere except the application’s libs subdirectory. |
Dependency is local to app |
|
Any dependency Dependency is in a shared location |
Use copy, git clone, or use some other revision control system to pull the library into a shared location. Edit the SEARCH variable in the application’s Makefile to point to the library. |
Custom BSP |
Dependencies are pulled automatically by Project Creator. |
6.2.1 import_deps¶
The make import_deps target is intended specifically to acquire dependencies in MTB flow applications for
libraries that don’t have their dependencies specified manifest files. To use it, you need a .mtbx file in the
library for each dependency. The format of .mtbx files is identical to .mtb files. When you run make
import_deps, it will copy the .mtbx files from the library into the application’s deps folder while also changing
the extension to .mtb. This results in the dependencies being direct to the application which are then pulled in
when make getlibs is run. The libraries can either be local or shared depending on the contents of the .mtbx
files. Usage:
make import_deps IMPORT_PATH=<path_to_library>
6.2.2 lib2mtbx¶
The make lib2mtbx target is mainly intended for libraries (or BSPs) that were created for ModusToolbox™ 2.0 or 2.1 that do not contain .mtbx files but do contain lib files for their dependencies. When you run make lib2mtbx, it will create .mtbx files in the library based on the .lib files in the library. The .mtbx files will be created to place the dependencies local to the application unless the optional argument “shared” is specified.
You can save the .mtbx files to the library’s source control so that you don’t need to do this step the next time the library is included into an application. Usage:
make lib2mtbx CONVERSION_PATH=<path_to_library> [CONVERSION_TYPE=”shared”]
6.3 Acquiring a library (LIB flow)¶
There are two basic ways to get a library that isn’t in a manifest file using the LIB flow.
Requirements |
Method |
---|---|
Library is hosted in a git repo |
Create a .lib file for the library in the application’s deps subdirectory. Run make getlibs from the application’s root directory. |
Any library |
Use copy, git clone, or use some other revision control system to pull the library into the application. It can be located anywhere except the application’s libs subdirectory. |
Custom BSP |
Use copy, git clone, or use some other revision control system to get the BSP somewhere on disk if it isn’t already. The location is not important. It will be copied into the application folder during project creation. Use the Project Creator Import function to select the BSP. The custom BSP will be copied into the application. See the Project Creator user guide for details. |
6.4 Acquiring dependencies (LIB flow)¶
Again, there are several ways to acquire dependencies depending on the library’s structure:
Requirements |
Method |
---|---|
Library contains .lib files for its dependencies |
Run make getlibs (this step is already done if you used make getlibs to acquire the library). |
Dependencies are listed in a manifest |
Use the Library Manager. |
Dependencies are hosted in a git repo |
Create a .lib file for each dependency in the application’s deps subdirectory. Run make getlibs from the application’s root directory. |
Any dependency |
Use copy, git clone, or use some other revision control system to pull the library into the application. It can be located anywhere except the libs directory. |
Custom BSP |
Dependencies are pulled automatically by Project Creator. |
7. Tool change description¶
This section lists and describes the changes for each version of this tool.
Version |
Change descriptions |
---|---|
1.0 |
New tool. |
1.1 |
Added Settings and Help menus. Moved link about version changes to the message console, when it is applicable. Added icon to indicate online/offline status. Removed Summary dialog; summary is shown in the console. |
1.2.0 |
Added Retry button. Changed Apply button to Update. Added Close button. Tool can be launched from the Windows Start menu. Updated versioning to support patch releases. Updated for the MTB flow. Added toolbar commands to show/hide items, as well as collapse and expand the trees. |
1.30 |
Added indications for newer versions of BSPs and libraries. For BSPs and libraries that are not selected, the displayed version was changed from Latest #.X release to the actual most recent X.Y.Z release. |
1.40 |
Updated the handling on .mtbx files. |
Revision history¶
Revision |
Date |
Description |
---|---|---|
** |
10/16/19 |
New document. |
*A |
10/17/19 |
Added a warning about removing all Cypress BSPs/libraries when there is no custom BSP. |
*B |
03/26/20 |
Updated to version 1.1. |
*C |
09/01/20 |
Updated to version 1.2.0. |
*D |
10/07/20 |
Added details for BTSDK 2.8. |
*E |
03/25/21 |
Updated to version 1.30. |
*F |
09/28/21 |
Updated to version 1.40. |