SHA2 with Cryptographic Hardware Block Example¶
This code example shows how to generate a 32-byte hash value or message digest for an arbitrary user input message with the SHA2 algorithm using the Cryptographic hardware block in PSoC ® 6 MCU. The example further shows that any change in the message results in a unique hash value for the message. The hash value generated for the message is displayed on a UART terminal emulator.
Click here to be taken to the project on GitHub.