Provisioning with BLE¶
This example uses the Arm® Cortex ®-M4 (CM4) CPU of PSoC ® 6 MCU to communicate with the CYW43xxx combo devices and control the Wi-Fi and BLE functionality. It uses BLE on the combo device to help connect the Wi-Fi to the AP. It also enables low-power mode on Wi-Fi and BLE.
Click here to be taken to the project on GitHub.