Threads¶
-
group
group_abstraction_rtos_threads
APIs for creating and working with Threads.
Unnamed Group
-
cy_rslt_t
cy_rtos_create_thread
(cy_thread_t *thread, cy_thread_entry_fn_t entry_function, const char *name, void *stack, uint32_t stack_size, cy_thread_priority_t priority, cy_thread_arg_t arg)¶ Create a thread with specific thread argument.
This function is called to startup a new thread. If the thread can exit, it must call cy_rtos_exit_thread() just before doing so. All created threads that can terminate, either by themselves or forcefully by another thread MUST have cy_rtos_join_thread() called on them by another thread in order to cleanup any resources that might have been allocated for them.
- Parameters
thread – [out] Pointer to a variable which will receive the new thread handle
entry_function – [in] Function pointer which points to the main function for the new thread
name – [in] String thread name used for a debugger
stack – [in] The buffer to use for the thread stack. This must be aligned to CY_RTOS_ALIGNMENT_MASK with a size of at least CY_RTOS_MIN_STACK_SIZE. If stack is null, cy_rtos_create_thread will allocate a stack from the heap.
stack_size – [in] The size of the thread stack in bytes
priority – [in] The priority of the thread. Values are operating system specific, but some common priority levels are defined: CY_THREAD_PRIORITY_LOW CY_THREAD_PRIORITY_NORMAL CY_THREAD_PRIORITY_HIGH
arg – [in] The argument to pass to the new thread
- Returns
The status of thread create request. [CY_RSLT_SUCCESS, CY_RTOS_NO_MEMORY, CY_RTOS_GENERAL_ERROR]
-
cy_rslt_t
cy_rtos_exit_thread
()¶ Exit the current thread.
This function is called just before a thread exits. In some cases it is sufficient for a thread to just return to exit, but in other cases, the RTOS must be explicitly signaled. In cases where a return is sufficient, this should be a null funcition. where the RTOS must be signaled, this function should perform that In cases operation. In code using RTOS services, this function should be placed at any at any location where the main thread function will return, exiting the thread. Threads that can exit must still be joined (cy_rtos_join_thread) to ensure their resources are fully cleaned up.
- Returns
The status of thread exit request. [CY_RSLT_SUCCESS, CY_RTOS_GENERAL_ERROR]
-
cy_rslt_t
cy_rtos_terminate_thread
(cy_thread_t *thread)¶ Terminates another thread.
This function is called to terminate another thread and reap the resources claimed by the thread. This should be called both when forcibly terminating another thread as well as any time a thread can exit on its own. For some RTOS implementations this is not required as the thread resources are claimed as soon as it exits. In other cases, this must be called to reclaim resources. Threads that are terminated must still be joined (cy_rtos_join_thread) to ensure their resources are fully cleaned up.
- Parameters
thread – [in] Handle of the thread to terminate
- Returns
The status of the thread terminate. [CY_RSLT_SUCCESS, CY_RTOS_GENERAL_ERROR]
-
cy_rslt_t
cy_rtos_join_thread
(cy_thread_t *thread)¶ Waits for a thread to complete.
This must be called on any thread that can complete to ensure that any resources that were allocated for it are cleaned up.
- Parameters
thread – [in] Handle of the thread to wait for
- Returns
The status of thread join request. [CY_RSLT_SUCCESS, CY_RTOS_GENERAL_ERROR]
-
cy_rslt_t
cy_rtos_is_thread_running
(cy_thread_t *thread, bool *running)¶ Checks if the thread is running.
This function is called to determine if a thread is actively running or not. For information on the thread state, use the cy_rtos_get_thread_state() function.
- Parameters
thread – [in] Handle of the terminated thread to delete
running – [out] Returns true if the thread is running, otherwise false
- Returns
The status of the thread running check. [CY_RSLT_SUCCESS, CY_RTOS_GENERAL_ERROR]
-
cy_rslt_t
cy_rtos_get_thread_state
(cy_thread_t *thread, cy_thread_state_t *state)¶ Gets the state the thread is currently in.
This function is called to determine if a thread is running/blocked/inactive/ready etc.
- Parameters
thread – [in] Handle of the terminated thread to delete
state – [out] Returns the state the thread is currently in
- Returns
The status of the thread state check. [CY_RSLT_SUCCESS, CY_RTOS_GENERAL_ERROR]
-
cy_rslt_t
cy_rtos_get_thread_handle
(cy_thread_t *thread)¶ Get current thread handle.
Returns the unique thread handle of the current running thread.
- Parameters
thread – [out] Handle of the current running thread
- Returns
The status of thread join request. [CY_RSLT_SUCCESS, CY_RTOS_GENERAL_ERROR]
Typedefs
-
typedef void (*
cy_thread_entry_fn_t
)(cy_thread_arg_t arg)¶ The type of a function that is the entry point for a thread.
- Parameters
arg – [in] the argument passed from the thread create call to the entry function
Enums
-
enum
cy_thread_state_t
¶ cy_thread_state_t: The state a thread can be in.
Values:
-
enumerator
CY_THREAD_STATE_INACTIVE
¶ thread has not started or was terminated but not yet joined
-
enumerator
CY_THREAD_STATE_READY
¶ thread can run, but is not currently
-
enumerator
CY_THREAD_STATE_RUNNING
¶ thread is currently running
-
enumerator
CY_THREAD_STATE_BLOCKED
¶ thread is blocked waiting for something
-
enumerator
CY_THREAD_STATE_TERMINATED
¶ thread has terminated but not freed
-
enumerator
CY_THREAD_STATE_UNKNOWN
¶ thread is in an unknown state
-
enumerator
-
cy_rslt_t