Class Support Functions¶
-
group
group_usb_dev_functions_class_support
Functions
-
cy_en_usb_dev_status_t
Cy_USB_Dev_RegisterClass
(cy_stc_usb_dev_class_ll_item_t *classItem, cy_stc_usb_dev_class_t *classObj, void *classContext, cy_stc_usb_dev_context_t *context)¶ Registers device class that will be supported by USB Device.
The USB Device provides a hooks to implement required class support.
- Parameters
classItem – The pointer to class linked list element.
classObj – The pointer to the class structure.
classContext – The pointer to the context class structure allocated by the user. The structure is used during the custom class operation for internal configuration and data retention.
context – The pointer to the context structure cy_stc_usb_dev_context_t allocated by the user. The structure is used during the USB Device operation for internal configuration and data retention. The user must not modify anything in this structure.
- Returns
Status code of the function execution cy_en_usb_dev_status_t.
-
__STATIC_INLINE void Cy_USB_Dev_RegisterClassBusResetCallback (cy_cb_usb_dev_bus_reset_t callback, cy_stc_usb_dev_class_t *classObj)
Registers a callback function to notify a certain class about a Bus Reset event.
To remove the callback function, pass NULL as the function pointer.
- Parameters
callback – The pointer to a callback function.
classObj – The pointer to the class structure.
-
__STATIC_INLINE void Cy_USB_Dev_RegisterClassSetConfigCallback (cy_cb_usb_dev_set_config_t callback, cy_stc_usb_dev_class_t *classObj)
Registers a callback function to notify a certain class that SET_CONFIGURATION request was received from USB Host.
To remove the callback function, pass a NULL as the function pointer.
- Parameters
callback – The pointer to a callback function.
classObj – The pointer to the class structure.
-
__STATIC_INLINE void Cy_USB_Dev_RegisterClassSetInterfaceCallback (cy_cb_usb_dev_set_interface_t callback, cy_stc_usb_dev_class_t *classObj)
Registers a callback function to notify a certain class that SET_INTERFACE request was received from the USB Host.
To remove the callback function, pass a NULL as the function pointer.
- Parameters
callback – The pointer to a callback function.
classObj – The pointer to the class structure.
-
__STATIC_INLINE void Cy_USB_Dev_RegisterClassRequestRcvdCallback (cy_cb_usb_dev_request_received_t callback, cy_stc_usb_dev_class_t *classObj)
Registers a callback function to notify a certain class that setup packet was received from USB Host but was not recognized.
Therefore, this might require manual class processing. To remove the callback function, pass a NULL as the function pointer.
- Parameters
callback – The pointer to a callback function.
classObj – The pointer to the class structure.
-
__STATIC_INLINE void Cy_USB_Dev_RegisterClassRequestCmpltCallback (cy_cb_usb_dev_request_cmplt_t callback, cy_stc_usb_dev_class_t *classObj)
Registers a callback function to notify a certain class that the USB Device received data from the USB Host as part of current request processing.
The class setup packet callback function must enable notification to trigger this event. This makes sense only when class request processing requires a data stage. To remove callback function pass NULL as function pointer.
- Parameters
callback – The pointer to a callback function.
classObj – The pointer to the class structure.
-
cy_en_usb_dev_status_t