ModusToolbox™ QSPI Configurator Guide¶
Overview¶
The Quad Serial Peripheral Interface (QSPI) Configurator is part of a collection of tools included with the ModusToolbox software. Use the QSPI Configurator to open or create configuration files, configure memory slots, and generate code for your application. The QSPI Configurator is a stand-alone tool. Use the top area for configuring memories; the read-only area below it displays information about the selected memory part number.
Launch the QSPI Configurator¶
You can launch the QSPI Configurator various ways: as a stand-alone tool, from the Eclipse IDE for ModusToolbox, from the Device Configurator or from the command line. Then, you can either use the generated source with an Eclipse IDE application, or use it in any software environment you choose.
As a Stand-Alone Tool¶
You can launch the QSPI Configurator as a stand-alone tool without the Eclipse IDE. By default, it is installed here:
<install_dir>/ModusToolbox/tools_<version>/qspi-configurator
On Windows, you can launch the tool from the Start menu.
For other operating systems, the installation directory will vary, based on how the software was installed.
When run independently, the QSPI Configurator opens without any memories configured. You can either open a specific Configuration file or create a new one. See Menus for more information.
If you open a Configuration file from an Eclipse IDE application, it will be the same flow as if you opened it from the Eclipse IDE.
If you open a Configuration file from a non-Eclipse IDE application, the flow will be for your preferred working environment.
If you create a new Configuration file, specify the file name and location to store the file.
From the Device Configurator¶
If your Eclipse IDE application does not include a design.cyqspi file:
Open the Device Configurator. See the Device Configurator User Guide for details.
On the Peripherals tab, enable the QSPI resource.
Optionally, review and resolve the tasks in the Notice List pane. These can be resolved later.
On the Parameters tab, click the Launch QSPI Configurator button.
The QSPI Configurator saves configuration information in a *.cyqspi file, which contains all the required information about the device and the application. When you save changes, the QSPI Configurator generates/updates firmware in the BSP’s “GeneratedSource” folder.
From the Eclipse IDE¶
If your Eclipse IDE application includes a design.cyqspi file in the Board Support Package (BSP), right-click on a project in the IDE Project Explorer, and select ModusToolbox > QSPI Configurator to open the tool.
Note
You can also launch the QSPI Configurator from a link in the Quick Panel.
From the Command Line¶
You can run the qspi-configurator executable from the command line. There is also a qspi-configurator-cli executable, which regenerates source code based on the latest configuration settings from a command-line prompt or from within batch files or shell scripts. The exit code for the qspi-configurator-cli executable is zero if the operation is successful, or non-zero if the operation encounters an error. In order to use the qspi-configurator-cli executable, you must provide at least the –config argument with a path to the configuration file.
For information about the command-line options, run the qspi-configurator or qspi-configurator-cli executable using the -h option.
Quick Start¶
This section provides a simple workflow for how to use the QSPI Configurator.
Select a memory from the Memory Part Number list.
If your memory device supports SFDP, select Auto detect SFDP.
If your memory device does not support SFDP, or for manual configuration, select a memory from the Memory Part Number list, and specify the configuration parameters as required (for example, memory mapped, write enable, etc.). See QSPI Configuration Fields.
Note
If the required memory part number is not present in the list, you can add it. Select <Browse>…, navigate to the memory file location, and select it.
Save the Configuration file to generate source code. See Code Generation.
Use the generated structures as input parameters for QSPI functions in your application.
Code Generation¶
The QSPI Configurator generates code into a “GeneratedSource” directory in your BSP, or in the same location you saved the Configuration file for non-Eclipse IDE applications. That directory contains the necessary source (.c) and header (.h) files for the generated firmware, which uses the relevant driver APIs to configure the hardware.
Files Used by the Configuration Tool¶
The QSPI Configurator uses and provides write access to two types of files: the QSPI configuration file (*.cyqspi), and the memory configuration files: ( .cymem). The QSPI Configurator uses the information from these files to generate cycfg_qspi_memslot.c, cycfg_qspi_memslot.h, and qspi_config.cfg files.
*.cyqspi – This file controls the application-level settings used to provide access to the serial memory device. In the GUI, these settings are at the top of the main window. For the format and contents of the
*.cyqspi file, see *.cyqspi Schema.
*.cymem – These files contain parameters of a specific serial memory device, including command formats, memory access sizes, and memory access timings. Unless you are creating a new *.cymem file, these settings are typically read-only and are shown in the lower part of the main window. For the format and contents of *.cymem files, see *.cymem Schema.
cy_qspi_memslot.c – This file is generated by the QSPI Configurator and contains structures populated with parameters specified by the *.cyqspi file and the *.cymem file or files.
cy_qspi_memslot.h – This file is generated by the QSPI Configurator and contains the declarations of the structures defined in cy_qspi_memslot.c.
qspi_config.cfg – This file contains a SMIF Bank layout for use with OpenOCD. It can be ignored if OpenOCD is not in use.
GUI Description¶
QSPI Configuration Fields¶
The top part of the QSPI Configurator contains the following parameters:
Parameter |
Description |
---|---|
Slave Slot |
Specifies the slave slot being configured. This number corresponds to the slave select line that will be connected to the memory device. |
Memory Part Number |
Device part number represents the memory device that is being interfaced to the corresponding slave slot. You can select a memory device from the list, or select the option to auto detect the device. Based on the memory device selected, the corresponding *.cymem file is linked into the slave slot. |
Configuration |
For certain Memory Part Numbers, there is additional configuration information, such as 3-byte or 4-byte Addressing Mode. |
Data Select |
Allows you to select the data line options for the corresponding memory slot. |
Memory Mapped |
When this option is enabled, the configured memory device is mapped to the PSoC MCU’s memory map. If disabled, access to memory must be done through the QSPI API. |
Pair with Slot |
Determines the paired slot for dual Quad operation. |
Start Address |
Determines the starting address where the memory device is going to be mapped in the PSoC memory map. |
Size |
Determines size in bytes of the memory device to be mapped in the PSoC memory map. |
End Address |
Represents the end address of the memory device as mapped in the PSoC MCU’s memory map. This is a read-only field that is calculated automatically from “Start Address” and “Size” cells values. |
Write Enable |
This lets you enable or disable writes to the external memory in a memory mapped mode of operation. |
Config Data in Flash |
Determines whether a specific memory slot’s config structures are to be placed in Flash or SRAM. When chosen to be placed in SRAM, the support for the programmer is not provided. Refer to AN228740 - PSoC 6 MCU Guide to Using Serial Memory Interface (QSPI). |
Encrypt |
Determines whether to treat the memory device in the corresponding slave slot as an encrypted device. If the memory is mapped, all access to this memory will be decrypted on-the-fly. Setting this field does expect that the right encryption key is loaded as a part of the secure image. |
Merge XIP Transaction s |
Specifies how many cycles can pass between memory accesses while still skipping the overhead of re-sending the read command. For CAT1A (PSoC 6) devices, this field must be Disabled. |
Edit Memory File Fields¶
The Edit Memory dialog contains the following fields. These fields also display as read-only in the lower part of the QSPI Configurator.
Field |
Description |
---|---|
Location |
The path and file name of the current memory file. |
Memory Part Number |
The is the name of the memory chip for which this configuration file is designed. This field will be displayed in the main QSPI Configurator window in the Memory Part Number drop-down menu. |
Configuration |
Some memory parts can be configured in more than one way, and each configuration is contained in a separate memory file. When creating more than one memory file for a part, use this field to describe how this file differs from the others. For example, “3-byte Addressing Mode” or “Hybrid Sectors at Bottom”. |
Configuration Is Default |
For memory parts with more than one configuration, this check box specifies whether this configuration is the one that should be automatically selected when this memory part is chosen in the Memory Part Number drop-down menu. |
Status Register Busy (WIP) Mask |
Mask for the busy bit in the status register. |
Status Register Quad Enable (QE) Mask |
Mask for the quad enable bit in the status register. |
Size of Memory |
Denotes the actual size of the memory device. |
Program Page Size |
Denotes the page size for a program operation. This size provides the granularity with which program operations can be committed in the memory device. |
Erase Block Size (bytes) |
Provides the erase block size. |
Number of Address Bytes for SPI Transactions |
Sets the number of bytes that are expected for the address field in the QSPI transaction. |
Max Erase Time |
Time the device typically takes to erase a Erase Type 1 size. You must poll the device’s busy status to determine whether the operation has completed. This field has no meaning if the corresponding Erase Type size is 00h. |
Max Chip Erase Time |
Typical time to erase one chip (die). You must poll the device’s busy status to determine whether the operation has completed. For a device consisting of multiple dies that are individually accessed, the time is for each die to which a chip erase command is applied. |
Max Program Time (µs) |
Typical time the device takes to write a full page. You must poll the device’s busy status to determine whether the operation has completed. You may scale this by half or a quarter to determine approximate times for half and quarter page program operations. |
Description |
Blank field to type a description for the memory. |
Commands Table (Single SPI,Dual SPI, Quad SPI, Octal SPI) Tabs show the SPI data widths supported by the selected memory. |
|
Description |
|
Number |
Byte command word. |
Command Width |
Width of the command transfer. |
Command Rate |
Determines whether the command byte should be sent in Single Data Rate (SDR) or Double Data Rate (DDR) mode. CAT1A (PSoC 6) devices only support SDR. |
Address Width |
Width of the address transfer. |
Address Rate |
Determines whether the address bytes should be sent in SDR or DDR mode. CAT1A (PSoC 6) devices only support SDR. |
Mode |
Provides the mode word for the command. |
Mode Width |
Provides the width of the mode word transfer. |
Mode Rate |
Determines whether the mode byte should be sent in SDR or DDR mode. CAT1A (PSoC 6) devices only support SDR. |
Dummy Cycles |
Provides the number of dummy cycles in the transfer. |
Data Width |
Provides the width of data bytes in the transfer. |
Data Rate |
Determines whether the data bytes should be sent in SDR or DDR mode. CAT1A (PSoC 6) devices only support SDR. |
Hybrid Erase Sectors Section |
|
Hybrid Erase Sectors |
This check box specifies whether sectors of different sizes are present in this configuration. The table below contains details about those sectors. If this check box is not enabled, then there are no sectors with different sizes, and none of the other fields are active. |
Row Buttons |
Use these buttons to add and delete rows, as well as move rows up and down. |
Region Table |
|
Memory Database¶
The QSPI Configurator memory database is a set of default memory configurations, based on values from each memory’s datasheet. Check that the selected memory configuration is aligned with a particular part number.
Notes:¶
By default, some memory parts are configured with protected regions, which prevents the successful execution of program/erase memory commands.
Dummy cycles may vary based on memory part configuration.
The list of supported commands may vary between memory parts.
Create New Memory File¶
Select New *.cymem File… to open the Edit Memory window from the main QSPI Configurator:
Click [ … ] button next to the Location field to specify the file name and location of the memory configuration file (.cymem). If you prefer, you can ignore the **Location* field for now, and then specify the file name and location when saving the file.
Enter a desired Memory Part Number. When selected, this field will be displayed in the main QSPI Configurator window in the Memory Part Number.
Complete the information for the remaining fields, as appropriate. See Edit Memory File Fields.
Click Save to save the configured memory. If Location was not specified previously, this will open a save dialog to navigate to the appropriate location, type a file name, and click Save.
Clock Close to return to the QSPI Configurator.
Migration of Configuration File Format¶
Versions of the QSPI Configurator prior to 2.0 used a C header file to store its configuration as a comment in XML format. In version 2.0 and beyond, the configuration is stored in a separate .cyqspi file in the XML format. Use the following instructions to migrate to the .cyqspi file as appropriate:
From the Eclipse IDE¶
Launch the QSPI Configurator. If there is no .cyqspi file, and if the .h file contains an XML configuration, it will be loaded automatically.
Click Save to create the .cyqspi file and update the C file.
Without the Eclipse IDE¶
Launch the QSPI Configurator.
Click Open.
Next to the File name, select the Obsolete configurator files (*.h) option and choose a header file.
After the configuration loads, click Save to create the .cyqspi file and update the C file.
Notes¶
The .cyqspi file is located one directory up related to the header file.
The command-line argument –config does not accept obsolete configuration files (*.h).
Patching Flashloaders¶
If you invoke the command line argument qspi-configurator or qspi-configurator-cli using the –flashloader option, the next argument must be the location of the ELF file containing variables with names matching those placed in QSPI Configurator generated code, as well as the string CFGSMIF placed where memory part numbers would normally be found. When the tools generate code for this case, they modify the data stored in these variables to match the data contained in the code being generated.
XML Schemas¶
*.cyqspi Schema¶
<xs:schema xmlns:xs=”http://www.w3.org/2001/XMLSchema” attributeFormDefault=”unqualified” elementFormDefault=”qualified”>
<xs:element name=”Configuration”>
<xs:complexType>
<xs:sequence>
<xs:element type=”xs:string” name=”DevicePath” />
<xs:element name=”SlotConfigs”>
<xs:complexType>
<xs:sequence>
<xs:element name=”SlotConfig” maxOccurs=”4” minOccurs=”0”>
<xs:complexType>
<xs:sequence>
<xs:element type=”xs:byte” name=”SlaveSlot” />
<xs:element type=”xs:string” name=”PartNumber” />
<xs:element type=”xs:boolean” name=”MemoryMapped” />
<xs:element type=”xs:string” name=”DualQuad” />
<xs:element type=”xs:string” name=”StartAddress” />
<xs:element type=”xs:string” name=”Size” />
<xs:element type=”xs:string” name=”EndAddress” />
<xs:element type=”xs:boolean” name=”WriteEnable” />
<xs:element type=”xs:boolean” name=”Encrypt” />
<xs:element type=”xs:string” name=”DataSelect” />
<xs:element type=”xs:string” name=”MemoryConfigsPath” />
<xs:element type=”xs:boolean” name=”ConfigDataInFlash” />
<xs:element type=”xs:string” name=”MergeTimeout” />
</xs:sequence>
</xs:complexType>
</xs:element>
</xs:sequence>
</xs:complexType>
</xs:element>
</xs:sequence>
<xs:attribute type=”xs:string” name=”app” fixed=”QSPI” />
<xs:attribute type=”xs:int” name=”major” />
<xs:attribute type=”xs:int” name=”minor” />
</xs:complexType>
</xs:element>
</xs:schema>
*.cymem Schema¶
<xs:schema xmlns:xs=”http://www.w3.org/2001/XMLSchema” attributeFormDefault=”unqualified” elementFormDefault=”qualified”>
<xs:element name=”CyMemoryConfiguration”>
<xs:complexType>
<xs:sequence>
<xs:element type=”xs:string” name=”PartNumber” />
<xs:element type=”xs:string” name=”Configuration” minOccurs=”0” />
<xs:element type=”xs:string” name=”DisplayName” minOccurs=”0” />
<xs:element type=”xs:string” name=”Description” />
<xs:element type=”xs:string” name=”NumberOfAddress” />
<xs:element type=”xs:string” name=”SizeOfMemory” />
<xs:element type=”xs:string” name=”EraseBlockSize” />
<xs:element type=”xs:string” name=”ProgramPageSize” />
<xs:element type=”xs:string” name=”StatusRegisterBusyMask” />
<xs:element type=”xs:string” name=”StatusRegisterQuadEnableMask” />
<xs:element type=”xs:int” name=”EraseTime” />
<xs:element type=”xs:int” name=”ChipEraseTime” />
<xs:element type=”xs:int” name=”ProgramTime” />
<xs:element name=”HybridInfo” minOccurs=”0” maxOccurs=”1”>
<xs:complexType>
<xs:sequence>
<xs:element maxOccurs=”unbounded” name=”Region”>
<xs:complexType>
<xs:sequence>
<xs:element name=”RegionIndex” type=”xs:int” />
<xs:element name=”SectorCount” type=”xs:int” />
<xs:element name=”SectorSize” type=”xs:string” />
<xs:element name=”EraseCommand” type=”xs:string” />
<xs:element name=”EraseTime” type=”xs:int” />
</xs:sequence>
</xs:complexType>
</xs:element>
</xs:sequence>
</xs:complexType>
</xs:element>
<xs:element name=”Commands” maxOccurs=”4” minOccurs=”1”>
<xs:complexType>
<xs:sequence>
<xs:element name=”Command” maxOccurs=”unbounded” minOccurs=”0”>
<xs:complexType>
<xs:sequence>
<xs:element type=”xs:string” name=”CommandDescription” />
<xs:element type=”xs:string” name=”CommandName” />
<xs:element type=”xs:string” name=”CommandNumber” />
<xs:element type=”xs:string” name=”CmdWidth” />
<xs:element type=”xs:string” name=”CmdRate” />
<xs:element type=”xs:string” name=”AddrWidth” />
<xs:element type=”xs:string” name=”AddrRate” />
<xs:element type=”xs:string” name=”Mode” />
<xs:element type=”xs:string” name=”ModeWidth” />
<xs:element type=”xs:string” name=”ModeRate” />
<xs:element type=”xs:byte” name=”DummyCycles” />
<xs:element type=”xs:string” name=”DataWidth” />
<xs:element type=”xs:string” name=”DataRate” />
</xs:sequence>
</xs:complexType>
</xs:element>
</xs:sequence>
<xs:attribute type=”xs:string” name=”mode” use=”optional” default=”Quad” />
</xs:complexType>
</xs:element>
</xs:sequence>
<xs:attribute type=”xs:string” name=”version” use=”optional” default=”1” />
</xs:complexType>
</xs:element>
</xs:schema>
References¶
Refer to the following documents for more information, as needed:
Device Datasheets
Device Technical Reference Manuals
Version Changes¶
This section lists and describes the changes for each version of this tool.
Version |
Change Descriptions |
---|---|
1.0 |
New tool. |
1.1 |
Added Notice List and toolbar. Updated to accommodate back end changes. |
2.0 |
Added Import/Export functionality. Moved configuration data from being embedded in the .h file to a new .cyqspi file. Set EraseTime, ChipEraseTime and ProgramTime to max. Allowed memory mapping for any Data Select selections. Added warning when “Config Data in Flash” check box isn’t selected, and the device part number is not in “auto detect mode.” Disabled the “Config Data in Flash” check box when the “Memory Part Number” is set to “Auto detect SFDP.” Added handling of invalid command line arguments. Made it impossible for paired slots to have different memory part numbers. Fixed the Pair with Slot Memory Overlap Error. |
2.1 |
Separated the Memory Part Number combo box into Memory Part Number and Configuration. Added support for hybrid erase sectors. |
2.20 |
Added Undo/Redo commands. Added Copy feature to the Notice List. |
2.30 |
Removed the command-line generate options: -g and –generate. |
Removed version 1.1 personality support. |