ModusToolbox™ Device Firmware Update Host tool guide

Version

1.50

Scope and purpose

The Device Firmware Update (DFU) Host tool is a stand-alone program included with the ModusToolbox™ software. This tool is used to communicate with a PSoC™ 6 or PSoC™ 4 MCU that has already been programmed with an application that includes the DFU capability.

Intended audience

This document helps application developers understand how to use the DFU Host tool as part of creating a ModusToolbox™ application.

Document conventions

Convention

Explanation

Bold

Emphasizes heading levels, column headings, menus and sub-menus

Italics

Denotes file names and paths.

Courier New

Denotes APIs, functions, interrupt handlers, events, data types, error handlers, file/folder names, directories, command line inputs, code snippets

File > New

Indicates that a cascading sub-menu opens when you select a menu item

Reference documents

Refer to the following documents for more information as needed:

Overview

The DFU Host tool is provided as a graphical user interface (GUI) and a command-line interface (CLI).

image0

This tool allows you to:

  • Program new application data onto a PSoC™ 6 or PSoC™ 4 MCU

  • Verify the program data that is already contained on the device

  • Erase the application from the device

  • Select a *.cyacd2 file output from a ModusToolbox™ application for programming

  • Abort an operation.

Note

This operation leaves the device in whatever state it is in when the abort message is acted upon.

The DFU Host tool supports communicating via I2C, SPI, and UART. They are displayed to configure their settings and view the programming status. For I2C and SPI, PSoC™ 6 and PSoC™ 4 kits include the KitProg3 firmware module, which implements USB-UART, USB-I2C, and USB-SPI bridges. For UART, communication can be done directly from the PC simply by connecting an appropriate cable.

Note

The process of initializing the device, two CPUs therein, and executing code in the SROM and supervisory flash, is referred to as “bootloading.” The process of installing and updating applications in the field is referred to as “device firmware update”. This process uses standard communication channels (UART, I2C, USB, etc.) to download new applications from a host.

Example code

We provide source code for the DFU Host tool in the installation directory, as follows:

  • Windows/Linux: ~/ModusToolbox/tools_2.3/dfuh-tool/sample_code/

  • Linux: ~/ModusToolbox/tools_2.3/dfuh-tool/share/dfuh-tool/sample_code/

  • macOS: /Applications/ModusToolbox/tools_2.3/dfuh-tool/dfuh-tool.app/Contents/sample_code/

Use this source code as a reference to build your own tool for your needs. Refer to the CMakeLists.txt file for instructions on how to build the example.

Note

This example requires CMake 3.12 or later.

Walkthrough

This section contains a basic walkthrough using the DFU Host tool.

  1. First, make sure you have a PSoC™ MCU that has been programmed with an application that includes the DFU capability.

  2. Launch the DFU Host tool GUI.

  3. In the graphical DFU Host tool, click File > Open to browse to the location of your application file (.*cyacd).

  4. Connect a hardware port that supports the communication selected in your bootloader project.

  5. Wire the hardware port pins to the corresponding pins on the target device.

  6. Update the port configuration. These values are set from the communication component used by the bootloader component.

After updating configuration information, click Program to load the new application.

Launch the DFU Host tool

There are several ways to launch the DFU Host tool, and those ways depend on how you use the various tools in ModusToolbox™ software.

make command

As described in the ModusToolbox™ user guide”Build System” chapter, you can run numerous make commands in the application directory, such as launching the DFU Host tool. After you have created a ModusToolbox™ application, navigate to the application directory and type the following command in the appropriate bash terminal window:

make open CY_OPEN_TYPE=dfuh-tool

This command opens the DFU Host tool GUI for the specific application in which you are working.

Eclipse IDE

If the selected Eclipse IDE application is suitable to use the DFU Host tool, right-click on the appropriate project and select ModusToolbox™ > Device Firmware Update Tool. You can also click the DFU Host tool link in the IDE Quick Panel.

image1

Executable (GUI)

You can launch the DFU Host tool as a stand-alone tool without the Eclipse IDE. By default, it is installed here:

<install_dir>/ModusToolbox_<version>/tools_<version>/dfuh-tool

On Windows, you can launch the tool from the Start menu. For other operating systems, the installation directory will vary, based on how the software was installed.

Executable (CLI)

Refer to CLI Description to run the dfuh-cli tool. You can also run the DFU Host tool GUI executable using the following command line arguments:

-?, -h, –help

Displays information about all valid command-line arguments and exits.

-v, –version

Displays version information and exits.

–debug <filename>

Appends detailed debugging information to the specified file.

GUI description

Main window

image2

  1. File selection

    Use this section to select the cyacd2 file that contains the DFU image.

  2. Ports

    This is a list of all the ports attached to the computer that can be used to communicate with the bootloader. Based on which item is selected, different options are available for the Port Configuration.

  3. Filters

    The Filters button allows for restricting which ports are displayed in the ports list.

image3

Port configuration

This section allows for configuring the interface-specific options for communicating with the DFU system. This is necessary to ensure both the DFU and host computer are configured the same.

Refer to the appropriate probe documentation for a list of supported modes.

Note

Not all SPI and UART communication properties combinations are supported.

I2C

For I2C communication, there are two pieces of required information:

image4

  • The address of the I2C-based target DFU system with which the host is communicating. The range for valid addresses is from 8 - 120.

  • The I2C SCK signal frequency.

SPI

For SPI communication, there are three pieces of required information:

image5

  • The SPI SCLK signal frequency.

  • The bit ordering of transferred data.

  • The SPI operating mode.

UART

For UART communication, there are four pieces of required information:

image6

  • The baud (bit) rate at which data is transferred.

  • The number of data bits per byte.

  • The number of stop bits indicating the termination of a byte.

  • The parity bit that is added to a byte.

Log

The log displays:

  • history of what happened while the Host was open

  • information about user-initiated operations

  • when items started/completed

  • the error messages during an operation if any.

Errors

Any errors for various fields display as a red X in the field containing the error, and it contains a tooltip when you hover the mouse cursor on it.

CLI description

In addition to the dfuh-tool GUI executable, there is also a dfuh-cli executable. The CLI allows programming, verifying, and erasing of devices from a command-line prompt or from within batch files or shell scripts. The exit code for the dfuh-cli executable is zero if the operation is successful, or non-zero if the operation encounters an error.

In order to use the dfuh-cli executable, you must provide exactly one of the following flags:

–program-device <cyacd2_file>

Program the device with the specified file and exit.

–verify-device <cyacd2_file>

Verify the programming of the device with the specified file and exit.

–erase-device <cyacd2_file>

Erase the specified program from the device and exit.

If there is more than one device connected to the host, use the following flag to specify which device to use:

–hwid <string>

Specifies the ID of the hardware to program/verify/erase. If this option is skipped, the first appropriate device found will be used.

In addition, you must provide the appropriate configuration values for exactly one of the following protocols:

The I2C flags are:

–I2C-address <int>

Sets the address for the I2C protocol. Valid values are between 8 (0x08) and 120 (0x78).

–I2C-speed <int>

Sets the speed for the I2C protocol in kHz. Common values are 50, 100, 400 and 1000.

The SPI flags are:

–spi-clockspeed <float>

Sets the clock speed for the SPI protocol in MHz.

–spi-mode <int>

Sets the mode for the SPI protocol in binary. Valid values are 00, 01, 10 and 11.

–spi-lsb-first

Specifies that the least-significant bit should be sent first for the SPI protocol. Otherwise, the most-significant bit will be sent first.

The UART flags are:

–uart-baudrate <int>

Sets the baud rate for the UART protocol.

–uart-databits <int>

Sets the number of data bits for the UART protocol.

–uart-paritytype <string>

Sets the parity type for the UART protocol. Valid strings are “None”, “Odd” and “Even”.

–uart-stopbits <float>

Sets the stop bits for the UART protocol. Valid values are 1, 1.5 and 2.

Command-line flags

The following flags change the overall functioning of the tool:

-?, -h, –help

Displays information about all valid command-line arguments and exits.

-v, –version

Displays version information and exits.

–debug

Outputs debugging information to the terminal running the CLI tool during programming, verifying or erasing.

–display-hw

Outputs all compatible hardware attached to the computer and exits.

CLI example

The following shows a simple example for using the dfu-cli executable

dfuh-cli –program-device test_app.cyacd2 –i2c-address 8 –i2c-speed 100

Troubleshooting

Problem

Workaround

On common Linux distributions, the serial UART ports (usually /dev/ttySx or /dev/ttyUSBx devices) belong to the root user and to the dialout group. Standard users are not allowed to access these devices.

An easy way to allow the current user access to the Linux machine’s serial ports is by adding the user to the dialout group. This can be done using the following command:

$sudo usermod -a -G dialout $USER

Note

For this command to take effect, you must log out and then log back in.

On Linux, attempts to set up or start DFU Host tool communication causes the tool to close without any messages.

To enable DFU Host tool communication under Linux, install the udev rules for KitProg3:

Disconnect the KitProg device.

Execute in the terminal (root access required):

sh $CYSDK/tools/fw-loader/ude v_rules/install_rules.sh

Reconnect the KitProg device.

On common Linux distributions, the DFU Host tool forbids communication protocol selection after re-plugging KitProg during communication.

Refer to the “Installation Procedure on Ubuntu Linux (x64)” section in the CYPRESS™ Programmer 2.1 CLI User Guide.

KitProg3 UART is accessible but not able to read data on Linux kernel 4.15 and above or Mac OS X 10.13 and above.

Use a third-party UART to USB bridge.

Update the KitProg3 firmware to version 1.11.243 or above.

After updating firmware and middleware for your application, SPI transfer speed is not as fast as expected.

You may be able to improve performance by modifying the src/backend/cychannelspi.cpp file. Remove the calls to QThread::msleep(1) when building your bootloader host tool.

Version changes

This section lists and describes the changes for each version of this tool.

Version

Change Descriptions

1.0

New tool.

1.1

Added Notice List.

Added command-line interface (CLI) and handling of invalid command line arguments. Added logging for firmware update process.

1.2

Removed Notice List.

1.30

Updated versioning to support patches.

1.40

Fixed minor defects.

1.50

Added PSoC™ 4 device support.

Revision history

Revision

Date

Description

**

11/09/2018

New document.

*A

10/16/2019

Updated to version 1.1.

*B

03/27/2020

Updated to version 1.2.

*C

09/01/2020

Updated to version 1.30.

*D

10/16/2020

Added information about code example.

*E

03/11/2021

Updated to version 1.40.

*F

09/20/2021

Updated to version 1.50.