BLE Common API¶
-
group
group_ble_common_api
The common API act as a general interface between the BLE application and the BLE Stack module.
The application may use these API to control the underlying hardware such as radio power, data encryption and device bonding via the stack. It may also access the GAP, GATT and L2CAP layers of the stack. These are divided into the following categories:
These API also use API specific definitions and data structures. These are classified in the following subset: