SAR_Type Struct Reference

struct SAR_Type

The struct type definition for the hardware register set contained in the block.

The address of a variable of this type can be used as the base hardware address for register access. A device may support more than one instance of a peripheral block.

Refer to a device-specific header file, e.g. <PDL_DIR>/COMPONENT_CAT1A/include/cy8c637bzi_bld74.h

for the list of block instances available on that device.

Refer to the device TRM for the block register descriptions.