Enumerated Types¶
-
group
group_sysint_enums
Enums
-
enum
cy_en_intr_t
¶ cy_en_intr_t: The enumerated type representing interrupt numbers that can be routed to the CM0+ Nested Vector Interrupt Controller (NVIC). Interrupt numbers are device-dependent. Refer to a device-specific header file, e.g. <PDL_DIR>/devices/include/cy8c637bzi_bld74.h for the specific enumerations for each interrupt number for that device.
Values:
-
enum
IRQn_Type
¶ IRQn_Type: The enumerated type representing interrupt numbers. Interrupt numbers are device-dependent. Refer to a device-specific header file, e.g. <PDL_DIR>/devices/include/cy8c637bzi_bld74.h for the specific enumerations for each interrupt number for that device.
Values:
-
enum
cy_en_sysint_status_t
cy_en_sysint_status_t: SysInt Driver error codes.
Values:
-
enumerator
CY_SYSINT_SUCCESS
Returned successful.
-
enumerator
CY_SYSINT_BAD_PARAM
Bad parameter was passed.
-
enumerator
-
enum
cy_en_sysint_nmi_t
cy_en_sysint_nmi_t: NMI connection input.
Values:
-
enumerator
CY_SYSINT_NMI1
NMI source input 1.
-
enumerator
CY_SYSINT_NMI2
NMI source input 2.
-
enumerator
CY_SYSINT_NMI3
NMI source input 3.
-
enumerator
CY_SYSINT_NMI4
NMI source input 4.
-
enumerator
-
enum