Functions¶
-
group
group_sysclk_clk_timer_funcs
Functions
-
void
Cy_SysClk_ClkTimerSetSource
(cy_en_clktimer_in_sources_t source) Sets the source for the timer clock (clk_timer).
The timer clock can be used as a source for SYSTICK as an alternate clock and one or more of the energy profiler counters.
- Function Usage
/* Scenario: The timer clock source needs to be updated to HFCLK0. */ if(CY_SYSCLK_CLKTIMER_IN_HF0_NODIV != Cy_SysClk_ClkTimerGetSource()) { Cy_SysClk_ClkTimerSetSource(CY_SYSCLK_CLKTIMER_IN_HF0_NODIV); }
- Parameters
source – cy_en_clktimer_in_sources_t
-
cy_en_clktimer_in_sources_t
Cy_SysClk_ClkTimerGetSource
(void) Reports the source for the timer clock (clk_timer).
- Function Usage
/* Scenario: The timer clock source needs to be updated to HFCLK0. */ if(CY_SYSCLK_CLKTIMER_IN_HF0_NODIV != Cy_SysClk_ClkTimerGetSource()) { Cy_SysClk_ClkTimerSetSource(CY_SYSCLK_CLKTIMER_IN_HF0_NODIV); }
- Returns
-
void
Cy_SysClk_ClkTimerSetDivider
(uint8_t divider) Sets the divider for the timer clock (clk_timer).
note
Do not change the divider value while the timer clock is enabled.
- Function Usage
/* Scenario: The timer divider needs to be updated to 64. */ if(63u != Cy_SysClk_ClkTimerGetDivider()) { Cy_SysClk_ClkTimerSetDivider(63u); /* divider = value + 1 */ }
- Parameters
divider – Divider value; valid range is 0 to 255. Divides the selected source (Cy_SysClk_ClkTimerSetSource) by the (value + 1).
-
uint8_t
Cy_SysClk_ClkTimerGetDivider
(void) Reports the divider value for the timer clock (clk_timer).
- Function Usage
/* Scenario: The timer divider needs to be updated to 64. */ if(63u != Cy_SysClk_ClkTimerGetDivider()) { Cy_SysClk_ClkTimerSetDivider(63u); /* divider = value + 1 */ }
- Returns
The divider value
-
void
Cy_SysClk_ClkTimerEnable
(void) Enables the timer clock (clk_timer).
The timer clock can be used as a source for SYSTICK and one or more of the energy profiler counters.
- Function Usage
/* Scenario: Timer clock needs to operate at HFCLK/32. */ Cy_SysClk_ClkTimerSetSource(CY_SYSCLK_CLKTIMER_IN_HF0_DIV8); Cy_SysClk_ClkTimerSetDivider(3u); /* divider = value + 1 */ Cy_SysClk_ClkTimerEnable(); /* Use the Timer clock as a source for the alternative ARM SysTick clock or for an Energy Profile counter clock. */ /* In case if there is a need to get the timer clock frequency */ uint32_t timerClkFreq = Cy_SysClk_ClkTimerGetFrequency();
-
bool
Cy_SysClk_ClkTimerIsEnabled
(void) Reports the Enabled/Disabled status of the Timer.
note
This API is available for CAT1A devices.
- Function Usage
/* Scenario: Timer clock is no longer required and needs to be disabled. All peripherals clocked using this source are disabled. */ if (Cy_SysClk_ClkTimerIsEnabled()) { Cy_SysClk_ClkTimerDisable(); }
- Returns
Boolean status of Timer: true - Enabled, false - Disabled.
-
void
Cy_SysClk_ClkTimerDisable
(void) Disables the timer clock (clk_timer).
- Function Usage
/* Scenario: Timer clock is no longer required and needs to be disabled. All peripherals clocked using this source are disabled. */ if (Cy_SysClk_ClkTimerIsEnabled()) { Cy_SysClk_ClkTimerDisable(); }
-
uint32_t
Cy_SysClk_ClkTimerGetFrequency
(void) Reports the frequency of the timer clock (clk_timer).
note
If the the timer clock is not enabled - a zero frequency is reported.
note
This API is available for CAT1A devices.
- Function Usage
/* Scenario: Timer clock needs to operate at HFCLK/32. */ Cy_SysClk_ClkTimerSetSource(CY_SYSCLK_CLKTIMER_IN_HF0_DIV8); Cy_SysClk_ClkTimerSetDivider(3u); /* divider = value + 1 */ Cy_SysClk_ClkTimerEnable(); /* Use the Timer clock as a source for the alternative ARM SysTick clock or for an Energy Profile counter clock. */ /* In case if there is a need to get the timer clock frequency */ uint32_t timerClkFreq = Cy_SysClk_ClkTimerGetFrequency();
-
void