SysAnalog (System Analog Reference Block)¶
-
group
group_sysanalog
This driver provides an interface for configuring the Analog Reference (AREF), Low Power Oscillator (LpOsc), Deep Sleep Clock and Timer blocks and querying the INTR_CAUSE register of the Programmable Analog SubSystem (PASS) hardware block.
The functions and other declarations used in this driver are in cy_sysanalog.h. You can include cy_pdl.h to get access to all functions and declarations in the PDL.
PASS block structure
The Programmable Analog SubSystem (PASS) hardware block contains a set of analog subblocks such as AREF, CTB, SAR, analog routing switches and others. In order to provide a firmware interface to PASS, subblocks are united into groups, which have their own drivers: SysAnalog, CTB and SAR.
SysAnalog Features Description
SysAnalog driver includes the following features:
AREF
Low Power Oscillator (Available only for PASS_ver2.)
Deep Sleep Clock (Available only for PASS_ver2.)
Timer (Available only for PASS_ver2.)
The following sections describe how to initialize driver features:
AREF Configuration
Low Power Oscillator, Deep Sleep Clock and Timer Configuration
AREF
The AREF block has the following features:
Generates a voltage reference (VREF) from one of three sources:
Local 1.2 V reference (low noise, optimized for analog performance)
Reference from the SRSS (high noise, not recommended for analog performance)
An external pin
Generates a 1 uA “zero dependency to absolute temperature” (IZTAT) current reference that is independent of temperature variations. It can come from one of two sources:
Local reference (low noise, optimized for analog performance)
Reference from the SRSS (high noise, not recommended for analog performance)
Generates a “proportional to absolute temperature” (IPTAT) current reference
Option to enable local references in Deep Sleep mode
The locally generated references are the recommended sources for blocks in the PASS because they have tighter accuracy, temperature stability, and lower noise than the SRSS references. The SRSS references can be used to save power if the low accuracy and higher noise can be tolerated.
The outputs of the AREF are consumed by multiple blocks in the PASS and by the CapSense (CSDv2) block. In some cases, these blocks have the option of using the references from the AREF. This selection would be in the respective drivers for these blocks. In some cases, these blocks require the references from the AREF to function.
AREF Output
CSDv2
VREF
optional
optional
optional
IZTAT
required
optional
optional
IPTAT
required
This driver provides a function to query the INTR_CAUSE register of the PASS. There are two interrupts in the PASS:
one global interrupt for all CTBs (up to 4)
one global interrupt for all CTDACs (up to 4)
Because the interrupts are global, the INTR_CAUSE register is needed to query which hardware instance triggered the interrupt.
AREF Configuration
To configure the AREF, call Cy_SysAnalog_Init and provide a pointer to the configuration structure, cy_stc_sysanalog_config_t. Three predefined structures are provided in this driver to cover a majority of use cases:
Cy_SysAnalog_Fast_Local (recommended for analog performance)
After initialization, call Cy_SysAnalog_Enable to enable the hardware.
Deep Sleep Operation
The AREF current and voltage references can be enabled to operate in Deep Sleep mode with Cy_SysAnalog_SetDeepSleepMode. There are four options for Deep Sleep operation:
CY_SYSANALOG_DEEPSLEEP_DISABLE : Disable AREF IP block
CY_SYSANALOG_DEEPSLEEP_IPTAT_1 : Enable IPTAT generator for fast wakeup from Deep Sleep mode. IPTAT outputs for CTBs are disabled.
CY_SYSANALOG_DEEPSLEEP_IPTAT_2 : Enable IPTAT generator and IPTAT outputs for CTB
CY_SYSANALOG_DEEPSLEEP_IPTAT_IZTAT_VREF : Enable all generators and outputs: IPTAT, IZTAT, and VREF
Recall that the CTB requires the IPTAT reference. For the CTB to operate at the 1 uA current mode in Deep Sleep mode, the AREF must be enabled for CY_SYSANALOG_DEEPSLEEP_IPTAT_IZTAT_VREF. For the CTB to operate at the 100 nA current mode in Deep Sleep mode, the AREF must be enabled for CY_SYSANALOG_DEEPSLEEP_IPTAT_2 minimum. In this lower current mode, the AREF IPTAT must be redirected to the CTB IZTAT. See the high level function Cy_CTB_SetCurrentMode in the CTB PDL driver.
If the CTDAC is configured to use the VREF in Deep Sleep mode, the AREF must be enabled for CY_SYSANALOG_DEEPSLEEP_IPTAT_IZTAT_VREF.
note
The SRSS references are not available to the AREF in Deep Sleep mode. When operating in Deep Sleep mode, the local or external references must be selected.
Low Power Oscillator
Features:
Internal PASS_ver2 8MHz oscillator which does not require any external components.
Can work in Deep Sleep power mode.
Can be used as a clock source for the Deep Sleep Clock.
Low Power Oscillator clocking mode is configured by cy_stc_sysanalog_deep_sleep_config_t::lpOscDsMode configuration structure item, which should be passed as a parameter to Cy_SysAnalog_DeepSleepInit function. See Low Power Oscillator Functions for other Low Power Oscillator control functions.
Deep Sleep Clock
Features:
Internal PASS_ver2 deep sleep capable clock selector/divider
Can be used as clock source for CTB pump, SAR ADC and Timer
Deep Sleep clock is configurable by cy_stc_sysanalog_deep_sleep_config_t::dsClkSource and cy_stc_sysanalog_deep_sleep_config_t::dsClkdivider configuration structure items, which should be passed as a parameter to Cy_SysAnalog_DeepSleepInit function.
Timer
Features:
Internal PASS_ver2 16-bit down counting timer
Can be used to trigger one or few SAR ADCs
Can be clocked from
Peripheral Clock (CLK_PERI),
Low Frequency Clock (CLK_LF)
Deep Sleep Clock
If clocked from Deep Sleep Clock, timer can be used to trigger SAR ADC scans in Deep Sleep power mode.
Timer is configurable by cy_stc_sysanalog_deep_sleep_config_t::timerClock and cy_stc_sysanalog_deep_sleep_config_t::timerPeriod configuration structure items, which should be passed as a parameter to Cy_SysAnalog_DeepSleepInit function. Also see Timer Functions for other Timer configuration and control functions.
Low Power Oscillator, Deep Sleep Clock and Timer Configuration
To configure Low Power Oscillator, Deep Sleep Clock and Timer blocks, call Cy_SysAnalog_DeepSleepInit function and provide pointer to PASS block and pointer to the cy_stc_sysanalog_deep_sleep_config_t configuration structure. In order to start Low Power Oscillator and Timer, call corresponding enable functions:
/* Initializes Deep Sleep features */ const cy_stc_sysanalog_deep_sleep_config_t dsConfig = { /*.lpOscDsMode */ CY_SYSANALOG_LPOSC_ALWAYS_ON, /*.dsClkSource */ CY_SYSANALOG_DEEPSLEEP_SRC_LPOSC, /*.dsClkdivider */ CY_SYSANALOG_DEEPSLEEP_CLK_DIV_BY_4, /*.timerClock */ CY_SYSANALOG_TIMER_CLK_DEEPSLEEP, /*.timerPeriod */ 4000UL }; if (CY_SYSANALOG_SUCCESS == Cy_SysAnalog_DeepSleepInit(PASS, &dsConfig)) { /* Enable LpOsc and Timer blocks. */ Cy_SysAnalog_LpOscEnable(PASS); Cy_SysAnalog_TimerEnable(PASS); }
More Information
For more information on the AREF, Deep Sleep Clock and Timer, refer to the technical reference manual (TRM).
Changelog
Version
Changes
Reason for Change
2.0
Added new features: LPOSC, DSCLK, TIMER.
New silicon family support.
1.10.1
Minor documentation updates.
Documentation enhancement.
1.10
Flattened the organization of the driver source code into the single source directory and the single include directory.
Driver library directory-structure simplification.
Added register access layer. Use register access macros instead of direct register access using dereferenced pointers.
Makes register access device-independent, so that the PDL does not need to be recompiled for each supported part number.
1.0
Initial version