General Functions

group group_smartio_functions_general

Functions

__STATIC_INLINE uint8_t Cy_SmartIO_GetChBypass (SMARTIO_PRT_Type *base)

Gets the bypass/route state of all 8 channels in the Smart I/O.

Bypass bit

Channel

0

io0<->chip0

1

io1<->chip1

2

io2<->chip2

3

io3<->chip3

4

io4<->chip4

5

io5<->chip5

6

io6<->chip6

7

io7<->chip7

Function Usage


    /* Refer to the Cy_SmartIO_SetChBypass() function usage example */

Parameters

base – Pointer to the Smart I/O base address

Returns

Bypass/Route state of 8 io<->chip channels (bits [7:0]): 1=bypass, 0=routed.

cy_en_smartio_status_t Cy_SmartIO_SetChBypass(SMARTIO_PRT_Type *base, uint8_t bypassMask)

Sets the bypass/route state of all 8 channels in the Smart I/O.

Bypass bit

Channel

0

io0<->chip0

1

io1<->chip1

2

io2<->chip2

3

io3<->chip3

4

io4<->chip4

5

io5<->chip5

6

io6<->chip6

7

io7<->chip7

note

The Smart I/O block must be disabled before calling this function.

Function Usage


    #define ioss_0_port_8_smartio_0_HW SMARTIO_PRT8
    
    /* Scenario: Smart I/O block 8 needs to bypass channels 2 and 3 */
    
    uint8_t bypassMask;
    
    bypassMask = Cy_SmartIO_GetChBypass(SMARTIO_PRT8);
    Cy_SmartIO_Disable(SMARTIO_PRT8);
    Cy_SmartIO_SetChBypass(SMARTIO_PRT8, (uint8_t)(bypassMask|CY_SMARTIO_CHANNEL2|CY_SMARTIO_CHANNEL3));
    Cy_SmartIO_Enable(SMARTIO_PRT8);

Parameters
  • base – Pointer to the Smart I/O base address

  • bypassMask – Bypass/Route state of 8 io<->chip channels (bits [7:0]): 1=bypass, 0=routed.

Returns

Status of the operation

__STATIC_INLINE cy_en_smartio_clksrc_t Cy_SmartIO_GetClock (SMARTIO_PRT_Type *base)

Gets the clock source of the Smart I/O.

Function Usage


    /* Refer to the Cy_SmartIO_SetClock() function usage example */

Parameters

base – Pointer to the Smart I/O base address

Returns

Clock source

cy_en_smartio_status_t Cy_SmartIO_SetClock(SMARTIO_PRT_Type *base, cy_en_smartio_clksrc_t clkSrc)

Sets the clock source of the Smart I/O.

note

The Smart I/O block must be disabled before calling this function.

Function Usage


    #define ioss_0_port_8_smartio_0_HW SMARTIO_PRT8
    
    /* Scenario: Smart I/O block 8 needs to change the clock source to low-frequency clock */
    
    cy_en_smartio_clksrc_t clkSrc;
    clkSrc = Cy_SmartIO_GetClock(SMARTIO_PRT8);
    
    if(clkSrc != CY_SMARTIO_CLK_LFCLK )
    {
        Cy_SmartIO_Disable(SMARTIO_PRT8);
        Cy_SmartIO_SetClock(SMARTIO_PRT8, CY_SMARTIO_CLK_LFCLK);
        Cy_SmartIO_Enable(SMARTIO_PRT8);
    }
    

Parameters
  • base – Pointer to the Smart I/O base address

  • clkSrc – Pointer to the Smart I/O base address

Returns

Status of the operation

__STATIC_INLINE uint8_t Cy_SmartIO_GetIoSync (SMARTIO_PRT_Type *base)

Gets the synchronization mode of the 8 I/O terminals.

Sync bit

I/O terminal

0

io0

1

io1

2

io2

3

io3

4

io4

5

io5

6

io6

7

io7

Function Usage


    /* Refer to the Cy_SmartIO_SetIoSync() function usage example */

Parameters

base – Pointer to the Smart I/O base address

Returns

Sync mode of 8 I/O terminals (bits [7:0]): 1=sync, 0=no sync.

cy_en_smartio_status_t Cy_SmartIO_SetIoSync(SMARTIO_PRT_Type *base, uint8_t ioSyncEn)

Sets the synchronization mode of the 8 I/O terminals.

Sync bit

I/O terminal

0

io0

1

io1

2

io2

3

io3

4

io4

5

io5

6

io6

7

io7

note

The Smart I/O block must be disabled before calling this function.

Function Usage


    #define ioss_0_port_8_smartio_0_HW SMARTIO_PRT8
    
    /* Scenario: Smart I/O block 8 needs to change the synchronization option
       on I/O 7 to synchronous mode */
    
    uint8_t syncIo;
    syncIo = Cy_SmartIO_GetClock(SMARTIO_PRT8);
    
    Cy_SmartIO_Disable(SMARTIO_PRT8);
    Cy_SmartIO_SetChBypass(SMARTIO_PRT8, (uint8_t)(syncIo|CY_SMARTIO_CHANNEL7));
    Cy_SmartIO_Enable(SMARTIO_PRT8);
    

Parameters
  • base – Pointer to the Smart I/O base address

  • ioSyncEn – Sync mode of 8 I/O terminals (bits [7:0]): 1=sync, 0=no sync.

Returns

Status of the operation

__STATIC_INLINE uint8_t Cy_SmartIO_GetChipSync (SMARTIO_PRT_Type *base)

Gets the synchronization mode of the 8 chip-side terminals.

Sync bit

chip terminal

0

chip0

1

chip1

2

chip2

3

chip3

4

chip4

5

chip5

6

chip6

7

chip7

Function Usage


    /* Refer to the Cy_SmartIO_SetChipSync() function usage example */

Parameters

base – Pointer to the Smart I/O base address

Returns

Sync mode of 8 chip-side terminals (bits [7:0]): 1=sync, 0=no sync.

cy_en_smartio_status_t Cy_SmartIO_SetChipSync(SMARTIO_PRT_Type *base, uint8_t chipSyncEn)

Sets the synchronization mode of the 8 chip-side terminals.

Sync bit

chip terminal

0

chip0

1

chip1

2

chip2

3

chip3

4

chip4

5

chip5

6

chip6

7

chip7

note

The Smart I/O block must be disabled before calling this function.

Function Usage


    #define ioss_0_port_8_smartio_0_HW SMARTIO_PRT8
    
    /* Scenario: Smart I/O block 8 needs to change the synchronization option
       on chip 7 to synchronous mode */
    
    uint8_t syncChip;
    syncChip = Cy_SmartIO_GetChipSync(SMARTIO_PRT8);
    
    Cy_SmartIO_Disable(SMARTIO_PRT8);
    Cy_SmartIO_SetChipSync(SMARTIO_PRT8, (uint8_t)(syncChip|CY_SMARTIO_CHANNEL7));
    Cy_SmartIO_Enable(SMARTIO_PRT8);
    

Parameters
  • base – Pointer to the Smart I/O base address

  • chipSyncEn – Sync mode of 8 chip-side terminals (bits [7:0]): 1=sync, 0=no sync.

Returns

Status of the operation

cy_en_smartio_status_t Cy_SmartIO_HoldOverride(SMARTIO_PRT_Type *base, bool hldOvr)

Configures the hold override mode.

In Deep-Sleep power mode, the HSIOM holds the GPIO output and output enable signals for all signals that operate in chip active domain. Enabling the hold override allows the Smart I/O to deliver Deep-Sleep output functionality on these GPIO terminals. If the Smart I/O should not drive any of the GPIO outputs, the hold override should be disabled.

note

The Smart I/O block must be disabled before calling this function.

Function Usage


    #define ioss_0_port_8_smartio_0_HW SMARTIO_PRT8
    
    /* Scenario: Smart I/O block 8 needs to enable the hold-override so that 
       it is operational during deep-sleep */

    Cy_SmartIO_Disable(SMARTIO_PRT8);
    Cy_SmartIO_HoldOverride(SMARTIO_PRT8, true);
    Cy_SmartIO_Enable(SMARTIO_PRT8);
    

Parameters
  • base – Pointer to the Smart I/O base address

  • hldOvr – true = Enabled: Smart I/O controls the port I/Os false = Disabled: HSIOM controls the port I/Os

Returns

Status of the operation