Interrupt

group group_scb_spi_interrupt_functions

Functions

void Cy_SCB_SPI_Interrupt(CySCB_Type *base, cy_stc_scb_spi_context_t *context)

This is the interrupt function for the SCB configured in the SPI mode.

This function must be called inside the user-defined interrupt service routine for Cy_SCB_SPI_Transfer to work.

Parameters
  • base – The pointer to the SPI SCB instance.

  • context – The pointer to the context structure cy_stc_scb_spi_context_t allocated by the user. The structure is used during the SPI operation for internal configuration and data retention. The user must not modify anything in this structure.

__STATIC_INLINE void Cy_SCB_SPI_RegisterCallback (CySCB_Type const *base, cy_cb_scb_spi_handle_events_t callback, cy_stc_scb_spi_context_t *context)

Registers a callback function, which notifies that SPI Callback Events occurred in the Cy_SCB_SPI_Interrupt.

note

To remove the callback, pass NULL as the pointer to the callback function.

Parameters
  • base – The pointer to the SPI SCB instance.

  • callback – The pointer to the callback function. See cy_cb_scb_spi_handle_events_t for the function prototype.

  • context – The pointer to the context structure cy_stc_scb_spi_context_t allocated by the user. The structure is used during the SPI operation for internal configuration and data retention. The user should not modify anything in this structure.