Data Structures¶
-
group
group_scb_i2c_data_structures
Typedefs
-
typedef void (*
cy_cb_scb_i2c_handle_events_t
)(uint32_t event) Provides the typedef for the callback function called in the Cy_SCB_I2C_Interrupt to notify the user about occurrences of I2C Callback Events.
-
typedef cy_en_scb_i2c_command_t (*
cy_cb_scb_i2c_handle_addr_t
)(uint32_t event) Provides the typedef for the callback function called in the Cy_SCB_I2C_Interrupt to notify the user about occurrences of I2C Address Callback Events.
This callback must return a decision to ACK (continue transaction) or NAK (end transaction) the received address. Note if the slave is configured to accept an address in RX FIFO, it must read from it using the Cy_SCB_ReadRxFifo function.
-
struct
cy_stc_scb_i2c_config_t
- #include <>
I2C configuration structure.
Public Members
-
cy_en_scb_i2c_mode_t
i2cMode
Specifies the mode of operation.
-
bool
useRxFifo
The SCB provides an RX FIFO in hardware (consult the selected device datasheet to get the actual FIFO size).
The useRxFifo field defines how the driver firmware reads data from the RX FIFO:
If this option is enabled, the hardware is configured to automatically ACK incoming data, and interrupt is enabled to take data out of the RX FIFO when it has some number of bytes (typically, when it is half full).
If this option is disabled, the interrupt is enabled to take data out of the RX FIFO when a byte is available. Also, hardware does not automatically ACK the data. Firmware must tell the hardware to ACK the byte (so each byte requires interrupt processing). Typically, this option should be enabled to configure hardware to automatically ACK incoming data. Otherwise hardware might not get the command to ACK or NACK a byte fast enough, and clock stretching is applied (the transaction is delayed) until the command is set. When this option is enabled, the number of interrupts required to process the transaction is significantly reduced because several bytes are handled at once. However, there is a side effect:
For master mode, the drawback is that the master may receive more data than desired due to the interrupt latency. An interrupt fires when the second-to-last byte has been received. This interrupt tells the hardware to stop receiving data. If the latency of this interrupt is longer than one transaction of the byte on the I2C bus, then the hardware automatically ACKs the following bytes until the interrupt is serviced or the RX FIFO becomes full.
For slave mode, the drawback is that the slave only NACKs the master when the RX FIFO becomes full, NOT when the slave write firmware buffer becomes full.
In either master or slave mode, all received extra bytes are dropped.
note
The useRxFifo option is not available if acceptAddrInFifo is true.
-
bool
useTxFifo
The SCB provides a TX FIFO in hardware (consult the selected device datasheet to get the actual FIFO size).
The useTxFifo option defines how the driver firmware loads data into the TX FIFO:
If this option is enabled, the TX FIFO is fully loaded with data and the interrupt is enabled to keep the TX FIFO loaded until the end of the transaction.
If this option is disabled, a single byte is loaded into the TX FIFO and the interrupt enabled to load the next byte when the TX FIFO becomes empty (so each byte requires interrupt processing). Typically, this option should be enabled to keep the TX FIFO loaded with data and reduce the probability of clock stretching. When there is no data to transfer, clock stretching is applied (the transaction is delayed) until the data is loaded. When this option is enabled, the number of interrupts required to process the transaction is significantly reduced because several bytes are handled at once. The drawback of enabling useTxFifo is that the abort operation clears the TX FIFO. The TX FIFO clear operation also clears the shift register. As a result the shifter may be cleared in the middle of a byte transaction, corrupting it. The remaining bits to transaction within the corrupted byte are complemented with 1s. If this is an issue, then do not enable this option.
-
uint8_t
slaveAddress
The 7-bit right justified slave address, used only for the slave mode.
-
uint8_t
slaveAddressMask
The slave address mask is used to mask bits of the slave address during the address match procedure (it is used only for the slave mode).
Bit 0 of the address mask corresponds to the read/write direction bit and is always a do not care in the address match therefore must be set 0. Bit value 0 - excludes bit from address comparison. Bit value 1 - the bit needs to match with the corresponding bit of the I2C slave address.
-
bool
acceptAddrInFifo
True - the slave address is accepted in the RX FIFO, false - the slave addresses are not accepted in the RX FIFO.
-
bool
ackGeneralAddr
True - accept the general call address; false - ignore the general call address.
-
bool
enableWakeFromSleep
When set, the slave will wake the device from Deep Sleep on an address match (the device datasheet must be consulted to determine which SCBs support this mode)
-
bool
enableDigitalFilter
Enables a digital 3-tap median filter to be applied to the inputs of filter glitches on the lines.
-
uint32_t
lowPhaseDutyCycle
The number of SCB clock cycles in the low phase of SCL.
Only applicable in master modes. The valid range is 7 to 16.
-
uint32_t
highPhaseDutyCycle
The number of SCB clock cycles in the high phase of SCL.
Only applicable in master modes. The valid range is 5 to 16.
-
cy_en_scb_i2c_mode_t
-
struct
cy_stc_scb_i2c_context_t
- #include <>
I2C context structure.
All fields for the context structure are internal. Firmware never reads or writes these values. Firmware allocates the structure and provides the address of the structure to the driver in function calls. Firmware must ensure that the defined instance of this structure remains in scope while the drive is in use.
-
struct
cy_stc_scb_i2c_master_xfer_config_t
- #include <>
The I2C Master transfer structure.
Public Members
-
uint8_t
slaveAddress
The 7-bit right justified slave address to communicate with.
-
uint8_t *
buffer
The pointer to the buffer for data to read from the slave or data to write into the slave.
-
uint32_t
bufferSize
The size of the buffer.
-
bool
xferPending
The transfer operation is pending - the stop condition will not be generated.
A new transfer starts from start condition and ends with or without stop condition. The stop condition releases I2C bus from master control. When stop is not generated master keeps bus control (transfer is pending) and can issue the next transfer using restart condition instead of start. The I2C driver automatically generates start or restart condition depends on current state. Note if master lost arbitration during transfer it stops control the bus and does not send/receive data or generate stop condition - the transfer ends.
-
uint8_t
-
typedef void (*