I2C (SCB)¶
-
group
group_scb_i2c
Driver API for I2C Bus Peripheral.
I2C - The Inter-Integrated Circuit (I2C) bus is an industry-standard.
The functions and other declarations used in this part of the driver are in cy_scb_i2c.h. You can also include cy_pdl.h to get access to all functions and declarations in the PDL.
The I2C peripheral driver provides an API to implement I2C slave, master, or master-slave devices based on the SCB hardware block. I2C devices based on SCB hardware are compatible with I2C Standard-mode, Fast-mode, and Fast-mode Plus specifications as defined in the I2C-bus specification.
Features:
An industry-standard I2C bus interface
Supports slave, master, and master-slave operation
Supports standard data rates of 100/400/1000 kbps
Hardware Address Match, multiple addresses
Wake from Deep Sleep on Address Match
note
I2C supports clock stretching. This occurs when a slave device is not capable of processing data, it holds the SCL line by driving a '0'. The master device monitors the SCL line and detects it when it cannot generate a positive clock pulse ('1') on the SCL line. It then reacts by delaying the generation of a positive edge on the SCL line, effectively synchronizing with the slave device that is stretching the clock. Clock stretching can occur in the case of externally clocked address matching until the internally clocked logic takes over. The largest reason for clock stretching is when the master tries to write to the slave and the slave's RX FIFO is full, the slave will then clock stretch until the FIFO is no longer full. For more information on FIFO size and clock stretching see the architecture TRM.
Configuration Considerations
The I2C driver configuration can be divided to number of sequential steps listed below:
Configure I2C
Assign and Configure Pins
Assign Clock Divider
Configure Data Rate
Configure Interrupt
Enable I2C
note
I2C driver is built on top of the SCB hardware block. The SCB3 instance is used as an example for all code snippets. Modify the code to match your design.
Configure I2C
To set up the I2C driver, provide the configuration parameters in the cy_stc_scb_i2c_config_t structure. Provide i2cMode to the select operation mode slave, master or master-slave. The useRxFifo and useTxFifo parameters specify if RX and TX FIFO is used during operation. Typically, both FIFOs should be enabled to reduce possibility of clock stretching. However, using RX FIFO has side effects that needs to be taken into account (see useRxFifo field description in cy_stc_scb_i2c_config_t structure). For master modes, parameters lowPhaseDutyCycle, highPhaseDutyCycle and enableDigitalFilter can be used to define output data rate (refer to section Configure Data Rate
for more information). For slave mode, provide the slaveAddress and slaveAddressMask. The other parameters are optional for operation.
To initialize the driver, call
Cy_SCB_I2C_Init function providing a pointer to the populated cy_stc_scb_i2c_config_t structure and the allocated cy_stc_scb_i2c_context_t structure.Set up I2C slave read and write buffer before enabling its operation using Cy_SCB_I2C_SlaveConfigReadBuf and Cy_SCB_I2C_SlaveConfigWriteBuf appropriately. Note that the master reads data from the slave read buffer and writes data into the slave write buffer./* Allocate context for I2C operation */ cy_stc_scb_i2c_context_t i2cContext; /* Populate configuration structure */ #if (USE_I2C_SLAVE) /* Slave configuration */ const cy_stc_scb_i2c_config_t i2cConfig = { .i2cMode = CY_SCB_I2C_SLAVE, .useRxFifo = false, .useTxFifo = true, .slaveAddress = 0x08U, .slaveAddressMask = 0xFEU, .acceptAddrInFifo = false, .ackGeneralAddr = false, .enableWakeFromSleep = false, .enableDigitalFilter = false, .lowPhaseDutyCycle = 0U, .highPhaseDutyCycle = 0U, }; #else /* USE_I2C_MASTER */ /* Master configuration */ const cy_stc_scb_i2c_config_t i2cConfig = { .i2cMode = CY_SCB_I2C_MASTER, .useRxFifo = false, .useTxFifo = true, .slaveAddress = 0U, .slaveAddressMask = 0U, .acceptAddrInFifo = false, .ackGeneralAddr = false, .enableWakeFromSleep = false, .enableDigitalFilter = false, .lowPhaseDutyCycle = 8U, .highPhaseDutyCycle = 8U, }; #endif /* Configure I2C to operate */ (void) Cy_SCB_I2C_Init(SCB3, &i2cConfig, &i2cContext);
/* Allocate buffers for I2C slave operation */ #define BUFFER_SIZE (128UL) uint8_t i2cReadBuffer[BUFFER_SIZE]; uint8_t i2cWriteBuffer[BUFFER_SIZE]; /* Configure write and read buffers for communication with master */ Cy_SCB_I2C_SlaveConfigReadBuf (SCB3, i2cReadBuffer, BUFFER_SIZE, &i2cContext); Cy_SCB_I2C_SlaveConfigWriteBuf(SCB3, i2cWriteBuffer, BUFFER_SIZE, &i2cContext);
Assign and Configure Pins
Only dedicated SCB pins can be used for I2C operation. The HSIOM register must be configured to connect dedicated SCB I2C pins to the SCB block. Also the I2C pins must be configured in Open-Drain, Drives Low mode (this pins configuration implies usage of external pull-up resistors):
/* Assign pins for I2C on SCB3: P6[0] and P6[1] */ #define I2C_PORT (P6_0_PORT) #define I2C_SCL_NUM (P6_0_NUM) #define I2C_SDA_NUM (P6_1_NUM) /* Connect SCB3 I2C function to pins */ Cy_GPIO_SetHSIOM(I2C_PORT, I2C_SCL_NUM, P6_0_SCB3_I2C_SCL); Cy_GPIO_SetHSIOM(I2C_PORT, I2C_SDA_NUM, P6_1_SCB3_I2C_SDA); /* Configure pins for I2C operation */ Cy_GPIO_SetDrivemode(I2C_PORT, I2C_SCL_NUM, CY_GPIO_DM_OD_DRIVESLOW); Cy_GPIO_SetDrivemode(I2C_PORT, I2C_SDA_NUM, CY_GPIO_DM_OD_DRIVESLOW);
note
The alternative pins configuration is Resistive Pull-ups which implies usage internal pull-up resistors. This configuration is not recommended because resistor value is fixed and cannot be used for all supported data rates. Refer to the device datasheet parameter RPULLUP for resistor value specifications.
Assign Clock Divider
A clock source must be connected to the SCB block to oversample input and output signals, in this document this clock will be referred as clk_scb. You must use one of the 8-bit or 16-bit dividers. Use the SysClk (System Clock) driver API to do this.
/* Assign divider type and number for I2C */ #define I2C_CLK_DIV_TYPE (CY_SYSCLK_DIV_8_BIT) #define I2C_CLK_DIV_NUM (0U) /* Connect assigned divider to be a clock source for I2C */ Cy_SysClk_PeriphAssignDivider(PCLK_SCB3_CLOCK, I2C_CLK_DIV_TYPE, I2C_CLK_DIV_NUM);
Configure Data Rate
To get I2C slave operation with the desired data rate, the clk_scb must be fast enough to provide sufficient oversampling. Use the SysClk (System Clock) driver API to do this.
To get I2C master operation with the desired data rate, the source clock frequency and SCL low and high phase duration must be configured. Use the SysClk (System Clock) driver API to configure source clock frequency. Then call Cy_SCB_I2C_SetDataRate to set the SCL low, high phase duration and digital filter. This function sets SCL low and high phase settings based on source clock frequency./* I2C slave desired data rate is 400 kbps. * To support this data rate the clk_scb frequency must be in range 7.82 – 15.38 MHz. * Find clk_scb valid ranges in TRM section I2C sub-section Oversampling and Bit Rate. * For clk_peri = 50 MHz, select divider value 4 and get clk_scb = (50 MHz / 4) = 12.5 MHz. * This clock frequency meets requirements above. */ Cy_SysClk_PeriphSetDivider (I2C_CLK_DIV_TYPE, I2C_CLK_DIV_NUMBER, 3u); Cy_SysClk_PeriphEnableDivider(I2C_CLK_DIV_TYPE, I2C_CLK_DIV_NUMBER);
Alternatively, the low, high phase and digital filter can be set directly using configuration structure cy_stc_scb_i2c_config_t fields lowPhaseDutyCycle, highPhaseDutyCycle and enableDigitalFilter appropriately.Refer to the technical reference manual (TRM) section I2C sub-section Oversampling and Bit Rate to get information how to configure I2C to run with the desired data rate.uint32_t dataRate; /* I2C master desired data rate in Hz */ #define I2C_DESIRED_DATA_RATE_HZ (100000U) /* I2C master desired data rate is 100 kbps. * To support this data rate the clk_scb frequency must be in range 1.55 – 3.2 MHz. * Find clk_scb valid ranges in TRM section I2C sub-section Oversampling and Bit Rate. * For clk_peri = 50 MHz, select divider value 32 and get clk_scb = (50 MHz / 32) = 1.563 MHz. * This clock frequency meets requirements above. */ Cy_SysClk_PeriphSetDivider (I2C_CLK_DIV_TYPE, I2C_CLK_DIV_NUMBER, 31u); Cy_SysClk_PeriphEnableDivider(I2C_CLK_DIV_TYPE, I2C_CLK_DIV_NUMBER); /* Configure master to operate with desired data rate */ dataRate = Cy_SCB_I2C_SetDataRate(SCB3, I2C_DESIRED_DATA_RATE_HZ, Cy_SysClk_PeriphGetFrequency(I2C_CLK_DIV_TYPE, I2C_CLK_DIV_NUMBER)); if ((dataRate > I2C_DESIRED_DATA_RATE_HZ) || (dataRate == 0U)) { /* Can not reach desired data rate */ CY_ASSERT(0U); }
note
For I2C slave, the analog filter is used for all supported data rates.
For I2C master, the analog filter is used for Standard and Fast modes and the digital filter for Fast Plus mode.Configure Interrupt
The interrupt is mandatory for I2C operation. The exception is the when only the Master Low-Level functions are used. The driver provides three interrupt functions: Cy_SCB_I2C_Interrupt, Cy_SCB_I2C_SlaveInterrupt, and Cy_SCB_I2C_MasterInterrupt. One of these functions must be called in the interrupt handler for the selected SCB instance. Call Cy_SCB_I2C_SlaveInterrupt when I2C is configured to operate as a slave, Cy_SCB_I2C_MasterInterrupt when I2C is configured to operate as a master and Cy_SCB_I2C_Interrupt when I2C is configured to operate as master and slave. Using the slave- or master-specific interrupt function allows reducing the flash consumed by the I2C driver. Also this interrupt must be enabled in the NVIC otherwise it will not work.
note
The I2C driver documentation refers to the Cy_SCB_I2C_Interrupt function when interrupt processing is mandatory for the operation. This is done to simplify the readability of the driver's documentation. The application should call the slave- or master-specific interrupt functions Cy_SCB_I2C_SlaveInterrupt or Cy_SCB_I2C_MasterInterrupt, when appropriate.
void I2C_Isr(void) { Cy_SCB_I2C_Interrupt(SCB3, &i2cContext); }
/* Assign I2C interrupt number and priority */ #define I2C_INTR_NUM scb_3_interrupt_IRQn #define I2C_INTR_PRIORITY (7UL) /* Populate configuration structure (code specific for CM4) */ const cy_stc_sysint_t i2cIntrConfig = { .intrSrc = I2C_INTR_NUM, .intrPriority = I2C_INTR_PRIORITY, }; /* Hook interrupt service routine and enable interrupt */ (void) Cy_SysInt_Init(&i2cIntrConfig, &I2C_Isr); NVIC_EnableIRQ(I2C_INTR_NUM);
Enable I2C
Finally, enable the I2C operation by calling Cy_SCB_I2C_Enable. Then I2C slave starts respond to the assigned address and I2C master ready to execute transfers.
/* Enable I2C to operate */ Cy_SCB_I2C_Enable(SCB3); /* Enable global interrupts */ __enable_irq();
Common Use Cases
Master Operation
The master API is divided into two categories: Master High-Level and Master Low-Level. Therefore, there are two methods for initiating I2C master transactions using either Low-Level or High-Level API. These two methods are described below. Only one method should be used at a time. They should not be mixed.
Use High-Level Functions
Call Cy_SCB_I2C_MasterRead or Cy_SCB_I2C_MasterWrite to communicate with the slave. These functions do not block and only start a transaction. After a transaction starts, the Cy_SCB_I2C_Interrupt handles further data transaction until its completion (successfully or with error occurring). To monitor the transaction, use Cy_SCB_I2C_MasterGetStatus or register callback function using Cy_SCB_I2C_RegisterEventCallback to be notified about I2C Callback Events.
cy_stc_scb_i2c_master_xfer_config_t transfer; uint8_t readBuffer [5UL]; uint8_t writeBuffer[2UL] = {0U, 5U}; /* Configure write transaction */ transfer.slaveAddress = 0x08U; transfer.buffer = writeBuffer; transfer.bufferSize = sizeof(writeBuffer); transfer.xferPending = true; /* Do not generate Stop condition at the end of transaction */ /* Initiate write transaction. * The Start condition is generated to begin this transaction. */ (void) Cy_SCB_I2C_MasterWrite(SCB3, &transfer, &i2cContext); /* Wait for transaction completion */ while (0UL != (CY_SCB_I2C_MASTER_BUSY & Cy_SCB_I2C_MasterGetStatus(SCB3, &i2cContext))) { } /* Configure read transaction */ transfer.buffer = readBuffer; transfer.bufferSize = sizeof(readBuffer); transfer.xferPending = false; /* Generate Stop condition the end of transaction */ /* Initiate read transaction. * The ReStart condition is generated to begin this transaction because * previous transaction was completed without Stop. */ (void) Cy_SCB_I2C_MasterRead(SCB3, &transfer, &i2cContext); /* Wait for transaction completion */ while (0UL != (CY_SCB_I2C_MASTER_BUSY & Cy_SCB_I2C_MasterGetStatus(SCB3, &i2cContext))) { } /* Process received data */
Use Low-Level Functions
Call Cy_SCB_I2C_MasterSendStart to generate a start, send an address with the Read/Write direction bit, and receive acknowledgment. After the address is ACKed by the slave, the transaction can be continued by calling Cy_SCB_I2C_MasterReadByte or Cy_SCB_I2C_MasterWriteByte depending on its direction. These functions handle one byte per call. Therefore, they should be called for each byte in the transaction. Note that for the Read transaction, the last byte must be NAKed. To complete the current transaction, call Cy_SCB_I2C_MasterSendStop or call Cy_SCB_I2C_MasterSendReStart to complete the current transaction and start a new one. Typically, do a restart to change the transaction direction without releasing the bus from the master control. The Low-Level functions are blocking and do not require calling Cy_SCB_I2C_Interrupt inside the interrupt handler. Using these functions requires extensive knowledge of the I2C protocol to execute transactions correctly.
Master Write Operation
Master Read Operationcy_en_scb_i2c_status_t status; /* Buffer to write to the slave */ uint8_t buffer[] = {0x55, 0x44, 0x33}; /* Wait 100 ms until operation completion */ uint32_t timeout = 100UL; /* Send Start condition, address and receive ACK/NACK response from slave */ status = Cy_SCB_I2C_MasterSendStart(SCB3, 0x08U, CY_SCB_I2C_WRITE_XFER, timeout, &i2cContext); if (CY_SCB_I2C_SUCCESS == status) { uint32_t cnt = 0UL; /* Write data into the slave from the buffer */ do { /* Write byte and receive ACK/NACK response */ status = Cy_SCB_I2C_MasterWriteByte(SCB3, buffer[cnt], timeout, &i2cContext); ++cnt; } while((status == CY_SCB_I2C_SUCCESS) && (cnt < sizeof(buffer))); } /* Check status of transaction */ if ((status == CY_SCB_I2C_SUCCESS) || (status == CY_SCB_I2C_MASTER_MANUAL_NAK) || (status == CY_SCB_I2C_MASTER_MANUAL_ADDR_NAK)) { /* Send Stop condition on the bus */ status = Cy_SCB_I2C_MasterSendStop(SCB3, timeout, &i2cContext); if (status == CY_SCB_I2C_SUCCESS) { /* Data has been written into the slave */ } } else { /* Other statuses do not require any actions */ }
cy_en_scb_i2c_status_t status; /* Buffer to write to the slave */ uint8_t buffer[5U]; /* Wait 100 ms until operation completion */ uint32_t timeout = 100UL; /* Send Start condition, address and receive ACK/NACK response from slave */ status = Cy_SCB_I2C_MasterSendStart(SCB3, 0x08U, CY_SCB_I2C_WRITE_XFER, timeout, &i2cContext); if (CY_SCB_I2C_SUCCESS == status) { uint32_t cnt = 0UL; cy_en_scb_i2c_command_t cmd = CY_SCB_I2C_ACK; /* Read data from the slave into the buffer */ do { if (cnt == (sizeof(buffer) - 1UL)) { /* The last byte must be NACKed */ cmd = CY_SCB_I2C_NAK; } /* Read byte and generate ACK / or prepare for NACK */ status = Cy_SCB_I2C_MasterReadByte(SCB3, cmd, &buffer[cnt], timeout, &i2cContext); ++cnt; } while((status == CY_SCB_I2C_SUCCESS) && (cnt < sizeof(buffer))); } /* Check status of transaction */ if ((status == CY_SCB_I2C_SUCCESS) || (status == CY_SCB_I2C_MASTER_MANUAL_NAK) || (status == CY_SCB_I2C_MASTER_MANUAL_ADDR_NAK)) { /* Send Stop condition on the bus */ status = Cy_SCB_I2C_MasterSendStop(SCB3, timeout, &i2cContext); if (status == CY_SCB_I2C_SUCCESS) { /* Process received data */ } } else { /* Other statuses do not require any actions. * The received data should dropped. */ }
Slave Operation
Slave operation requires the Cy_SCB_I2C_Interrupt be called inside the interrupt handler. The read and write buffers must be provided for the slave to enable communication with the master. Use Cy_SCB_I2C_SlaveConfigReadBuf and Cy_SCB_I2C_SlaveConfigWriteBuf for this purpose. Note that after transaction completion the buffer must be configured again. Otherwise, the same buffer is used starting from the point where the master stopped a previous transaction. For example: The read buffer is configured to be 10 bytes and the master reads 8 bytes. If the read buffer is not configured again, the next master read will start from the 9th byte. To monitor the transaction status, use Cy_SCB_I2C_SlaveGetStatus or use Cy_SCB_I2C_RegisterEventCallback to register a callback function to be notified about I2C Callback Events.
Get Slave Events Notification
/* Register callback for event notification. * It is better to do this during initialization before I2C is enabled. */ Cy_SCB_I2C_RegisterEventCallback(SCB3, I2C_SlaveEventHandler, &i2cContext);
Polling Slave Completion Events/* Callback implementation */ void I2C_SlaveEventHandler(uint32_t events) { /* Slave sent data to master */ if (0UL != (events & CY_SCB_I2C_SLAVE_RD_CMPLT_EVENT)) { if (0UL == (events & CY_SCB_I2C_SLAVE_ERR_EVENT)) { /* Read complete without errors: update buffer content */ } /* Setup read buffer for the next read transaction */ Cy_SCB_I2C_SlaveConfigReadBuf(SCB3, i2cReadBuffer, BUFFER_SIZE, &i2cContext); } /* Slave received data from master */ if (0UL != (events & CY_SCB_I2C_SLAVE_WR_CMPLT_EVENT)) { if (0UL == (events & CY_SCB_I2C_SLAVE_ERR_EVENT)) { /* Write complete without errors: process received data */ } /* Setup buffer for the next write transaction */ Cy_SCB_I2C_SlaveConfigWriteBuf(SCB3, i2cWriteBuffer, BUFFER_SIZE, &i2cContext); } /* Ignore all other events */ }
/* Disable I2C Interrupt: protect code from interruption */ NVIC_DisableIRQ(I2C_INTR_NUM); /* Check if write transaction completed */ if (0UL != (CY_SCB_I2C_SLAVE_WR_CMPLT & Cy_SCB_I2C_SlaveGetStatus(SCB3, &i2cContext))) { /* Process received data */ /* Configure buffer for the next write */ Cy_SCB_I2C_SlaveConfigWriteBuf(SCB3, i2cWriteBuffer, BUFFER_SIZE, &i2cContext); /* Clear slave write status to capture following updates */ Cy_SCB_I2C_SlaveClearWriteStatus(SCB3, &i2cContext); } /* Enable I2C interrupt */ NVIC_EnableIRQ(I2C_INTR_NUM);
note
All slave API (except Cy_SCB_I2C_SlaveAbortRead and Cy_SCB_I2C_SlaveAbortWrite) are not interrupt-protected and to prevent a race condition, they should be protected from the I2C interruption in the place where they are called. The code snippet Polling Slave Completion Events above shows how to prevent a race condition when detect transfer completion and update I2C slave write buffer. The simple example of race condition is: application updates slave read buffer the I2C master starts read transfer. The I2C interrupts read buffer update and I2C interrupt loads current read buffer content in the TX FIFO . After I2C interrupt returns the application updates remaining part of the read buffer. As a result the mater read partly updated buffer.
Low Power Support
The I2C driver provides callback functions to handle power mode transition. The callback Cy_SCB_I2C_DeepSleepCallback must be called during execution of Cy_SysPm_CpuEnterDeepSleep Cy_SCB_I2C_HibernateCallback must be called during execution of Cy_SysPm_SystemEnterHibernate. To trigger the callback execution, the callback must be registered before calling the power mode transition function. Refer to SysPm (System Power Management) driver for more information about power mode transitions and callback registration.
note
Only applicable for rev-08 of the CY8CKIT-062-BLE. For proper operation, when the I2C slave is configured to be a wakeup source from Deep Sleep mode, the Cy_SCB_I2C_DeepSleepCallback must be copied and modified. Refer to the function description to get the details.