Functions¶
- Initialization and Basic Functions
- Low Power Callback
- Run-time Configuration Functions
- Counts Conversion Functions
- Interrupt Functions
- SARMUX Switch Control Functions
- Useful Configuration Query Functions
- Low Power features control Functions
- FIFO buffer contlol Functions
- Common triggering Functions for multiple SAR instances
-
group
group_sar_functions
Defines
-
Cy_SAR_Sleep
This macro is for backward compatibility macro for driver v1.10 and before, the preferred API is Cy_SAR_DeepSleep.
Functions
-
__STATIC_INLINE void Cy_SAR_SimultStart (PASS_Type *base, uint32_t sarMask, cy_en_sar_start_convert_sel_t mode)
Simultaneously starts two or more SARs.
- Function Usage
/* Scenario: Simultaneously start continuous SAR0 and SAR1 scan */ Cy_SAR_SimultStart(PASS, CY_SAR_SAR0 | CY_SAR_SAR1, CY_SAR_START_CONVERT_CONTINUOUS); /* Scenario: Stop SAR0 and SAR1 continuous scan */ Cy_SAR_SimultStop(PASS, CY_SAR_SAR0 | CY_SAR_SAR1);
- Parameters
base – Pointer to structure describing PASS registers.
sarMask – specifies which SAR instances will be started. Mask should contain at least two SAR instances for operation.
mode – specifies mode of SARs operation.
- Returns
None
-
__STATIC_INLINE void Cy_SAR_SimultStop (PASS_Type *base, uint32_t sarMask)
Stops the selected SARs.
- Function Usage
/* Scenario: Simultaneously start continuous SAR0 and SAR1 scan */ Cy_SAR_SimultStart(PASS, CY_SAR_SAR0 | CY_SAR_SAR1, CY_SAR_START_CONVERT_CONTINUOUS); /* Scenario: Stop SAR0 and SAR1 continuous scan */ Cy_SAR_SimultStop(PASS, CY_SAR_SAR0 | CY_SAR_SAR1);
- Parameters
base – Pointer to structure describing PASS registers.
sarMask – specifies which SAR instances should be stopped.
- Returns
None
-