Data Structures

group group_mcwdt_data_structures
struct MCWDT_STRUCT_Type
#include <>

struct cy_stc_mcwdt_config_t
#include <>

The MCWDT component configuration structure.

Public Members

uint16_t c0Match

The sub-counter#0 match comparison value, for interrupt or watchdog timeout.

Range: 0 - 65535 for c0ClearOnMatch = 0 and 1 - 65535 for c0ClearOnMatch = 1.

uint16_t c1Match

The sub-counter#1 match comparison value, for interrupt or watchdog timeout.

Range: 0 - 65535 for c1ClearOnMatch = 0 and 1 - 65535 for c1ClearOnMatch = 1.

uint8_t c0Mode

The sub-counter#0 mode.

It can have the following values: CY_MCWDT_MODE_NONE, CY_MCWDT_MODE_INT, CY_MCWDT_MODE_RESET and CY_MCWDT_MODE_INT_RESET.

uint8_t c1Mode

The sub-counter#1 mode.

It can have the following values: CY_MCWDT_MODE_NONE, CY_MCWDT_MODE_INT, CY_MCWDT_MODE_RESET and CY_MCWDT_MODE_INT_RESET.

uint8_t c2ToggleBit

The sub-counter#2 Period / Toggle Bit value.

Range: 0 - 31.

uint8_t c2Mode

The sub-counter#2 mode.

It can have the following values: CY_MCWDT_MODE_NONE and CY_MCWDT_MODE_INT.

bool c0ClearOnMatch

The sub-counter#0 Clear On Match parameter enabled/disabled.

note

This parameter is available for devices having MXS40SSRSS IP.

bool c1ClearOnMatch

The sub-counter#1 Clear On Match parameter enabled/disabled.

bool c0c1Cascade

The sub-counter#1 is clocked by LFCLK or from sub-counter#0 cascade.

bool c1c2Cascade

The sub-counter#2 is clocked by LFCLK or from sub-counter#1 cascade.