Functions¶
API Reference
-
group
group_lpcomp_functions
Functions
-
cy_en_lpcomp_status_t
Cy_LPComp_Init
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel, const cy_stc_lpcomp_config_t *config) Initializes LPCOMP and returns the LPCOMP register address.
- Parameters
*base – LPCOMP registers structure pointer.
*config – The pointer to the configuration structure for PDL.
channel – The LPCOMP channel index.
- Returns
cy_en_lpcomp_status_t *base checking result. If the pointer is NULL, returns error.
-
void
Cy_LPComp_Enable
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel) Enables the LPCOMP and sets the LPCOMP interrupt mode.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
- Returns
None
-
void
Cy_LPComp_Disable
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel) Disables the LPCOMP power and sets the interrupt mode to disabled.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
- Returns
None
-
__STATIC_INLINE void Cy_LPComp_GlobalEnable (LPCOMP_Type *base)
Activates the IP of the LPCOMP hardware block.
This API should be enabled before operating any channel of comparators. Note: Interrupts can be enabled after the block is enabled and the appropriate start-up time has elapsed: 3 us for the normal power mode; 6 us for the LP mode; 50 us for the ULP mode.
- Parameters
*base – The structure of the channel pointer.
- Returns
None
-
__STATIC_INLINE void Cy_LPComp_GlobalDisable (LPCOMP_Type *base)
Deactivates the IP of the LPCOMP hardware block.
(Analog in power down, open all switches, all clocks off).
- Parameters
*base – The structure of the channel pointer.
- Returns
None
-
__STATIC_INLINE void Cy_LPComp_UlpReferenceEnable (LPCOMP_Type *base)
Enables the local reference-generator circuit.
- Parameters
*base – The structure of the channel pointer.
- Returns
None
-
__STATIC_INLINE void Cy_LPComp_UlpReferenceDisable (LPCOMP_Type *base)
Disables the local reference-generator circuit.
- Parameters
*base – The structure of the channel pointer.
- Returns
None
-
__STATIC_INLINE uint32_t Cy_LPComp_GetCompare (LPCOMP_Type const *base, cy_en_lpcomp_channel_t channel)
This function returns a nonzero value when the voltage connected to the positive input is greater than the negative input voltage.
- Parameters
*base – The LPComp register structure pointer.
channel – The LPComp channel index.
- Returns
LPComp compare result. The value is a nonzero value when the voltage connected to the positive input is greater than the negative input voltage.
-
void
Cy_LPComp_SetPower
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel, cy_en_lpcomp_pwr_t power) Sets the drive power and speeds to one of the four settings.
note
Interrupts can be enabled after the block is enabled and the appropriate start-up time has elapsed: 3 us for the normal power mode; 6 us for the LP mode; 50 us for the ULP mode. Otherwise, unexpected interrupts events can occur.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
power – The power setting sets an operation mode of the component: CY_LPCOMP_OFF_POWER (=0) - Off power CY_LPCOMP_MODE_ULP (=1) - Slow/ultra low power CY_LPCOMP_MODE_LP (=2) - Medium/low power CY_LPCOMP_MODE_NORMAL(=3) - Fast/normal power
- Returns
None
-
void
Cy_LPComp_SetHysteresis
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel, cy_en_lpcomp_hyst_t hysteresis) Adds the 30mV hysteresis to the comparator.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
hysteresis – Sets an operation mode of the component CY_LPCOMP_HYST_ENABLE (=1) - Enables HYST CY_LPCOMP_HYST_DISABLE(=0) - Disable HYST.
- Returns
None
-
void
Cy_LPComp_SetInputs
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel, cy_en_lpcomp_inputs_t inputP, cy_en_lpcomp_inputs_t inputN) Sets the comparator input sources.
The comparator inputs can be connected to the dedicated GPIO pins or AMUXBUSA/AMUXBUSB. Additionally, the negative comparator input can be connected to the local VREF. At least one unconnected input causes a comparator undefined output.
note
Connection to AMUXBUSA/AMUXBUSB requires closing the additional switches which are a part of the IO system. These switches can be configured using the HSIOM->AMUX_SPLIT_CTL[3] register. Refer to the appropriate Technical Reference Manual (TRM) of a device for a detailed description.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
inputP – Positive input selection CY_LPCOMP_SW_GPIO (0x01u) CY_LPCOMP_SW_AMUXBUSA (0x02u) - Hi-Z in hibernate mode CY_LPCOMP_SW_AMUXBUSB (0x04u) - Hi-Z in the hibernate mode.
inputN – Negative input selection CY_LPCOMP_SW_GPIO (0x01u) CY_LPCOMP_SW_AMUXBUSA (0x02u) - Hi-Z in hibernate mode CY_LPCOMP_SW_AMUXBUSB (0x04u) - Hi-Z in hibernate mode CY_LPCOMP_SW_LOCAL_VREF (0x08u) - the negative input only for a crude REF.
- Returns
None
-
void
Cy_LPComp_SetOutputMode
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel, cy_en_lpcomp_out_t outType) Sets the type of the comparator DSI output.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
outType – Interrupt edge trigger selection CY_LPCOMP_OUT_PULSE (=0) - the DSI output with the pulse option, no bypass CY_LPCOMP_OUT_DIRECT (=1) - the bypass mode, the direct output of the comparator CY_LPCOMP_OUT_SYNC (=2) - DSI output with the level option, it is similar to the bypass mode but it is 1 cycle slow than the bypass. [DSI_LEVELx : DSI_BYPASSx] = [Bit11 : Bit10] 0 : 0 = 0x00 -> Pulse (PULSE) 1 : 0 = 0x02 -> Level (SYNC) x : 1 = 0x01 -> Bypass (Direct).
- Returns
None
-
void
Cy_LPComp_SetInterruptTriggerMode
(LPCOMP_Type *base, cy_en_lpcomp_channel_t channel, cy_en_lpcomp_int_t intType) Sets the interrupt edge-detect mode.
This also controls the value provided on the output.
note
Interrupts can be enabled after the block is enabled and the appropriate start-up time has elapsed: 3 us for the normal power mode; 6 us for the LP mode; 50 us for the ULP mode.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
intType – Interrupt edge trigger selection CY_LPCOMP_INTR_DISABLE (=0) - Disabled, no interrupt will be detected CY_LPCOMP_INTR_RISING (=1) - Rising edge CY_LPCOMP_INTR_FALLING (=2) - Falling edge CY_LPCOMP_INTR_BOTH (=3) - Both rising and falling edges.
- Returns
None
-
__STATIC_INLINE uint32_t Cy_LPComp_GetInterruptStatus (LPCOMP_Type const *base)
Returns the status of 2 different LPCOMP interrupt requests.
- Parameters
*base – The LPCOMP register structure pointer.
- Returns
bit mapping information Bit 0: COMP0 Interrupt status Bit 1: COMP1 Interrupt status
-
__STATIC_INLINE void Cy_LPComp_ClearInterrupt (LPCOMP_Type *base, uint32_t interrupt)
Clears LPCOMP interrupts by setting each bit.
- Parameters
*base – The LPCOMP register structure pointer.
interrupt – Bit 0: COMP0 Interrupt status Bit 1: COMP1 Interrupt status
- Returns
None
-
__STATIC_INLINE void Cy_LPComp_SetInterrupt (LPCOMP_Type *base, uint32_t interrupt)
Sets a software interrupt request.
This function is used in the case of combined interrupt signal from the global signal reference. This function from either component instance can be used to trigger either or both software interrupts. It sets the INTR_SET interrupt mask.
- Parameters
*base – The LPCOMP register structure pointer.
interrupt – Bit 0: COMP0 Interrupt status Bit 1: COMP1 Interrupt status
- Returns
None
-
__STATIC_INLINE uint32_t Cy_LPComp_GetInterruptMask (LPCOMP_Type const *base)
Returns an interrupt mask.
- Parameters
*base – The LPCOMP register structure pointer.
- Returns
bit mapping information Bit 0: COMP0 Interrupt Mask Bit 1: COMP1 Interrupt Mask
-
__STATIC_INLINE void Cy_LPComp_SetInterruptMask (LPCOMP_Type *base, uint32_t interrupt)
Configures which bits of the interrupt request register will trigger an interrupt event.
- Parameters
*base – The LPCOMP register structure pointer.
interrupt – uint32_t interruptMask: Bit Mask of interrupts to set. Bit 0: COMP0 Interrupt Mask Bit 1: COMP1 Interrupt Mask
- Returns
None
-
__STATIC_INLINE uint32_t Cy_LPComp_GetInterruptStatusMasked (LPCOMP_Type const *base)
Returns an interrupt request register masked by an interrupt mask.
Returns the result of the bitwise AND operation between the corresponding interrupt request and mask bits.
- Parameters
*base – The LPCOMP register structure pointer.
- Returns
bit mapping information Bit 0: COMP0 Interrupt Masked Bit 1: COMP1 Interrupt Masked
-
__STATIC_INLINE void Cy_LPComp_ConnectULPReference (LPCOMP_Type *base, cy_en_lpcomp_channel_t channel)
Connects the local reference generator output to the comparator negative input.
- Parameters
*base – The LPCOMP register structure pointer.
channel – The LPCOMP channel index.
- Returns
None
-
cy_en_lpcomp_status_t