Functions¶
-
group
group_ipc_sema_functions
Functions are used in the driver.
Functions
-
cy_en_ipcsema_status_t
Cy_IPC_Sema_Init
(uint32_t ipcChannel, uint32_t count, uint32_t memPtr[]) This function initializes the semaphores subsystem.
The user must create an array of unsigned 32-bit words to hold the semaphore bits. The number of semaphores will be the size of the array * 32. The total semaphores count will always be a multiple of 32.
note
In a multi-CPU system this init function should be called with all initialized parameters on one CPU only to provide a pointer to SRAM that can be shared between all the CPUs in the system that will use semaphores. On other CPUs user must specify the IPC semaphores channel and pass 0 / NULL to count and memPtr parameters correspondingly.
- Function Usage
/* Scenario: set up a single semaphore channel for use in communicating between two cores */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #if (CY_CPU_CORTEX_M0P) /* The semaphore data is usually allocated in CM0+ memory space */ uint32_t mySemaData; /* So there are 32 semaphores */ if (CY_IPC_SEMA_SUCCESS != Cy_IPC_Sema_Init(MY_IPC_CHAN_INDEX, 32UL, &mySemaData)) { /* Handle possible errors */ } #else /* Therefore, enother core (usually CM4) initializes semaphore subsystem without data pointer */ if (CY_IPC_SEMA_SUCCESS != Cy_IPC_Sema_Init(MY_IPC_CHAN_INDEX, 0UL, NULL)) { /* Handle possible errors */ } #endif /* (CY_CPU_CORTEX_M0P) */
- Parameters
ipcChannel – The IPC channel number used for semaphores
count – The maximum number of semaphores to be supported (multiple of 32).
memPtr – This points to the array of (count/32) words that contain the semaphore data.
- Returns
Status of the operation
- Returns
CY_IPC_SEMA_SUCCESS – Successfully initialized
CY_IPC_SEMA_BAD_PARAM – Memory pointer is NULL and count is not zero, or count not multiple of 32
CY_IPC_SEMA_ERROR_LOCKED – Could not acquire semaphores IPC channel
-
cy_en_ipcsema_status_t
Cy_IPC_Sema_InitExt
(uint32_t ipcChannel, cy_stc_ipc_sema_t *ipcSema) This function initializes the semaphores subsystem.
The user must create an array of unsigned 32-bit words to hold the semaphore bits. The number of semaphores will be the size of the array * 32. The total semaphores count will always be a multiple of 32.
note
In a multi-CPU system this init function should be called with all initialized parameters on one CPU only to provide a pointer to SRAM that can be shared between all the CPUs in the system that will use semaphores. On other CPUs user must specify the IPC semaphores channel and pass 0 / NULL to count and memPtr parameters correspondingly.
- Parameters
ipcChannel – The IPC channel number used for semaphores
ipcSema – This is configuration structure of the IPC semaphore. See cy_stc_ipc_sema_t.
- Returns
Status of the operation
- Returns
CY_IPC_SEMA_SUCCESS – Successfully initialized
CY_IPC_SEMA_BAD_PARAM – Memory pointer is NULL and count is not zero, or count not multiple of 32
CY_IPC_SEMA_ERROR_LOCKED – Could not acquire semaphores IPC channel
-
cy_en_ipcsema_status_t
Cy_IPC_Sema_Set
(uint32_t semaNumber, bool preemptable) This function tries to acquire a semaphore.
If the semaphore is not available, this function returns immediately with CY_IPC_SEMA_LOCKED.
It first acquires the IPC channel that is used for all the semaphores, sets the semaphore if it is cleared, then releases the IPC channel used for the semaphore.
note
If preemptable is enabled (true), the user must ensure that there are no deadlocks in the system, which can be caused by an interrupt that occurs after the IPC channel is locked. Unless the user is ready to handle IPC channel locks correctly at the application level, set preemptable to false.
- Function Usage
/* Scenario: set semaphore #MY_SEMA_NUM to inform the other core * of the intention to perform some action. */ #define MY_SEMA_NUM (3UL) switch (Cy_IPC_Sema_Set(MY_SEMA_NUM, false)) { case CY_IPC_SEMA_SUCCESS: /* The semaphore is set successfully */ break; case CY_IPC_SEMA_LOCKED: /* The semaphore channel is busy or locked by another process */ break; case CY_IPC_SEMA_NOT_ACQUIRED: /* Semaphore is already set */ break; case CY_IPC_SEMA_OUT_OF_RANGE: /* The semaphore number is not valid */ break; default: break; }
- Parameters
semaNumber – The semaphore number to acquire.
preemptable – When this parameter is enabled the function can be preempted by another task or other forms of context switching in an RTOS environment.
- Returns
Status of the operation
- Returns
CY_IPC_SEMA_SUCCESS – The semaphore was set successfully
CY_IPC_SEMA_LOCKED – The semaphore channel is busy or locked by another process
CY_IPC_SEMA_NOT_ACQUIRED – Semaphore was already set
CY_IPC_SEMA_OUT_OF_RANGE – The semaphore number is not valid
-
cy_en_ipcsema_status_t
Cy_IPC_Sema_Clear
(uint32_t semaNumber, bool preemptable) This functions tries to releases a semaphore.
It first acquires the IPC channel that is used for all the semaphores, clears the semaphore if it is set, then releases the IPC channel used for the semaphores.
note
If preemptable is enabled (true), the user must ensure that there are no deadlocks in the system, which can be caused by an interrupt that occurs after the IPC channel is locked. Unless the user is ready to handle IPC channel locks correctly at the application level, set preemptable to false.
- Function Usage
/* Scenario: action is completed. Clear the semaphore #MY_SEMA_NUM to inform * the other core that the action is already completed. */ #define MY_SEMA_NUM (3UL) switch (Cy_IPC_Sema_Clear(MY_SEMA_NUM, false)) { case CY_IPC_SEMA_SUCCESS: /* The semaphore is cleared successfully */ break; case CY_IPC_SEMA_LOCKED: /* The semaphore channel is busy or locked by another process */ break; case CY_IPC_SEMA_NOT_ACQUIRED: /*Semaphore is already cleared */ break; case CY_IPC_SEMA_OUT_OF_RANGE: /* The semaphore number is not valid */ break; default: break; }
- Parameters
semaNumber – The index of the semaphore to release.
preemptable – When this parameter is enabled the function can be preempted by another task or other forms of context switching in an RTOS environment.
- Returns
Status of the operation
- Returns
CY_IPC_SEMA_SUCCESS – The semaphore was cleared successfully
CY_IPC_SEMA_NOT_ACQUIRED – The semaphore was already cleared
CY_IPC_SEMA_LOCKED – The semaphore channel was semaphored or busy
CY_IPC_SEMA_OUT_OF_RANGE – The semaphore number is not valid
-
cy_en_ipcsema_status_t
Cy_IPC_Sema_Status
(uint32_t semaNumber) This function returns the status of the semaphore.
- Function Usage
/* Scenario: check the state of semaphore #3. */ #define MY_SEMA_NUM (3UL) switch (Cy_IPC_Sema_Status(MY_SEMA_NUM)) { case CY_IPC_SEMA_STATUS_LOCKED: /* The semaphore is in the set state */ break; case CY_IPC_SEMA_STATUS_UNLOCKED: /* The semaphore is in the cleared state */ break; case CY_IPC_SEMA_OUT_OF_RANGE: /* The semaphore number is not valid */ break; default: break; }
- Parameters
semaNumber – The index of the semaphore to return status.
- Returns
Status of the operation
- Returns
CY_IPC_SEMA_STATUS_LOCKED – The semaphore is in the set state.
CY_IPC_SEMA_STATUS_UNLOCKED – The semaphore is in the cleared state.
CY_IPC_SEMA_OUT_OF_RANGE – The semaphore number is not valid
-
uint32_t
Cy_IPC_Sema_GetMaxSems
(void) This function returns the number of semaphores in the semaphores subsystem.
- Function Usage
/* Scenario: get the maximum number of configured semaphores * and check if the MY_SEMA_NUM is valid. */ #define MY_SEMA_NUM (3UL) if (MY_SEMA_NUM < Cy_IPC_Sema_GetMaxSems()) { /* The MY_SEMA_NUM is valid */ }
- Returns
Returns the semaphores quantity.
-
cy_en_ipcsema_status_t