Functions¶
-
group
group_ipc_functions
Functions are used in the driver.
Functions
-
__STATIC_INLINE IPC_STRUCT_Type * Cy_IPC_Drv_GetIpcBaseAddress (uint32_t ipcIndex)
This function takes an IPC channel index as a parameter and returns the base address the IPC registers corresponding to the IPC channel.
note
The user is responsible for ensuring that ipcIndex does not exceed the limits.
- Function Usage
/* Scenario: there is a need to send a "one word" (32-bit) message, * which can be also used as any command/flag/etc. */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg = 0x12345678UL; /* Example message */ if (CY_IPC_DRV_SUCCESS != Cy_IPC_Drv_SendMsgWord(myIpc, MY_IPC_INTR_MASK, myMsg)) { /* Insert error handling */ }
- Parameters
ipcIndex – Represents the number of IPC structure. This is converted to the base address of the IPC channel registers.
- Returns
Returns a pointer to the base of the IPC registers.
-
__STATIC_INLINE IPC_INTR_STRUCT_Type * Cy_IPC_Drv_GetIntrBaseAddr (uint32_t ipcIntrIndex)
This function takes an IPC interrupt structure index and returns the base address of the IPC interrupt registers corresponding to the IPC Interrupt.
note
The user is responsible for ensuring that ipcIntrIndex does not exceed the limits.
- Function Usage
/* Scenario: there is a need to check the IPC pending interrupts */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ IPC_INTR_STRUCT_Type * myIpcIntr = Cy_IPC_Drv_GetIntrBaseAddr(MY_IPC_INTR_INDEX); uint32_t intrStatus = Cy_IPC_Drv_GetInterruptStatus(myIpcIntr);
- Parameters
ipcIntrIndex – Represents the number of IPC interrupt structure. This is converted to the base address of the IPC interrupt registers.
- Returns
Returns a pointer to the base of the IPC interrupt registers.
-
__STATIC_INLINE void Cy_IPC_Drv_AcquireNotify (IPC_STRUCT_Type *base, uint32_t notifyEventIntr)
The function generates a acquire notification event by IPC interrupt structure.
- Function Usage
/* Scenario: there is a need to acquire the IPC channel so that other CPU * cores are blocked to use it. Prior to acquiring, check if it is not already * acquired by another CPU core. */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ if (!Cy_IPC_Drv_IsLockAcquired(myIpc)) { if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_LockAcquire(myIpc)) { /* Scenario: there is a need to manually trigger the IPC notification * interrupt without specifying the data to be passed. * It can essentially be used as a 1-bit semaphore. */ Cy_IPC_Drv_AcquireNotify(myIpc, MY_IPC_INTR_MASK); /* Another core is expected to own the interrupt generated in the * IPC interrupt channel #MY_IPC_INTR_INDEX */ } else { /* Insert error handling */ } }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
notifyEventIntr – Bit encoded list of IPC interrupt structures that are triggered by a notification. Bit number correspond to number of the IPC interrupt structure.
-
__STATIC_INLINE void Cy_IPC_Drv_ReleaseNotify (IPC_STRUCT_Type *base, uint32_t notifyEventIntr)
The function generates a release notification event by IPC interrupt structure.
- Function Usage
/* Scenario: a notification interrupt has just occurred so * there is a need to receive a "one word" (32-bit) message */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg; /* Example message */ if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_ReadMsgWord(myIpc, &myMsg)) { /* Now myMsg contains the received message word */ /* The IPC data is received and processed. * Free up the channel for the next transaction. */ Cy_IPC_Drv_ReleaseNotify(myIpc, MY_IPC_INTR_MASK); } else { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
notifyEventIntr – Bit encoded list of IPC interrupt lines that are triggered by a notification.
-
__STATIC_INLINE cy_en_ipcdrv_status_t Cy_IPC_Drv_LockAcquire (IPC_STRUCT_Type const *base)
This function is used to acquire the IPC channel.
- Function Usage
/* Scenario: there is a need to acquire the IPC channel so that other CPU * cores are blocked to use it. Prior to acquiring, check if it is not already * acquired by another CPU core. */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ if (!Cy_IPC_Drv_IsLockAcquired(myIpc)) { if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_LockAcquire(myIpc)) { /* Scenario: there is a need to manually trigger the IPC notification * interrupt without specifying the data to be passed. * It can essentially be used as a 1-bit semaphore. */ Cy_IPC_Drv_AcquireNotify(myIpc, MY_IPC_INTR_MASK); /* Another core is expected to own the interrupt generated in the * IPC interrupt channel #MY_IPC_INTR_INDEX */ } else { /* Insert error handling */ } }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress
- Returns
Status of the operation
- Returns
CY_IPC_DRV_SUCCESS – The IPC was successfully acquired
CY_IPC_DRV_ERROR – The IPC was not acquired because it was already acquired by another master
-
cy_en_ipcdrv_status_t
Cy_IPC_Drv_LockRelease
(IPC_STRUCT_Type *base, uint32_t releaseEventIntr) The function is used to release an IPC channel from the locked state.
The function also has a way to specify through a parameter which IPC interrupts must be notified during the release event.
- Function Usage
/* Scenario: an acquire notification interrupt has just occurred * so now is a time to read a message pointer and then whole the * message content */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC interrupt mask */ #define MY_IPC_MSG_SIZE (7UL) /* Example message size */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg[MY_IPC_MSG_SIZE]; /* Example message container */ void * myMsgPtr; /* Example message pointer */ if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_ReadMsgPtr(myIpc, &myMsgPtr)) { uint32_t i; for(i = 0; i < MY_IPC_MSG_SIZE; i++) { myMsg[i] = *((uint32_t*)((uint32_t)myMsgPtr + i)); /* Copying the message content */ } } else { /* Insert error handling */ } /* The IPC data was received and processed. * Free up the channel for the next transaction. */ if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_LockRelease(myIpc, MY_IPC_INTR_MASK)) { /* Now the IPC channel is successfully released */ } else { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
releaseEventIntr – Bit encoded list of IPC interrupt lines that are triggered by a release event.
- Returns
Status of the operation
- Returns
CY_IPC_DRV_SUCCESS – The function executed successfully and the IPC channel was released.
CY_IPC_DRV_ERROR – The IPC channel was not acquired before the function call.
-
__STATIC_INLINE bool Cy_IPC_Drv_IsLockAcquired (IPC_STRUCT_Type const *base)
The function is used to test the status of an IPC channel.
The function tells the reader if the IPC channel was in the locked or released state.
- Function Usage
/* Scenario: there is a need to acquire the IPC channel so that other CPU * cores are blocked to use it. Prior to acquiring, check if it is not already * acquired by another CPU core. */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ if (!Cy_IPC_Drv_IsLockAcquired(myIpc)) { if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_LockAcquire(myIpc)) { /* Scenario: there is a need to manually trigger the IPC notification * interrupt without specifying the data to be passed. * It can essentially be used as a 1-bit semaphore. */ Cy_IPC_Drv_AcquireNotify(myIpc, MY_IPC_INTR_MASK); /* Another core is expected to own the interrupt generated in the * IPC interrupt channel #MY_IPC_INTR_INDEX */ } else { /* Insert error handling */ } }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
- Returns
Status for the function: true: The IPC channel is in the Locked state. false: The IPC channel is in the Released state.
-
__STATIC_INLINE uint32_t Cy_IPC_Drv_GetLockStatus (IPC_STRUCT_Type const *base)
The function is used to get the status of an IPC channel.
- Function Usage
/* Scenario: there is a need to check the IPC channel status */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t ipcStatus = Cy_IPC_Drv_GetLockStatus(myIpc); /* Now the ipcStatus contains all the LOCK_STATUS register content, * such a user/privileged, secure/non-secure access modes, * protection context, bus master, etc. */
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
- Returns
Value from LOCK_STATUS register.
-
cy_en_ipcdrv_status_t
Cy_IPC_Drv_SendMsgWord
(IPC_STRUCT_Type *base, uint32_t notifyEventIntr, uint32_t message) This function is used to send a 32-bit word message through an IPC channel.
The function also has an associated notification field that will let the message notify one or multiple IPC interrupts. The IPC channel is locked and remains locked after the function returns. The receiver of the message should release the channel.
- Function Usage
/* Scenario: there is a need to send a "one word" (32-bit) message, * which can be also used as any command/flag/etc. */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg = 0x12345678UL; /* Example message */ if (CY_IPC_DRV_SUCCESS != Cy_IPC_Drv_SendMsgWord(myIpc, MY_IPC_INTR_MASK, myMsg)) { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
notifyEventIntr – Bit encoded list of IPC interrupt lines that are triggered by a notification.
message – The message word that is the data placed in the IPC data register.
- Returns
Status of the operation:
- Returns
CY_IPC_DRV_SUCCESS – The send operation was successful.
CY_IPC_DRV_ERROR – The IPC channel is unavailable because it is already locked.
-
cy_en_ipcdrv_status_t
Cy_IPC_Drv_ReadMsgWord
(IPC_STRUCT_Type const *base, uint32_t *message) This function is used to read a 32-bit word message through an IPC channel.
This function assumes that the channel is locked (for a valid message). If the channel is not locked, the message is invalid. The user must call Cy_IPC_Drv_Release() function after reading the message to release the IPC channel.
- Function Usage
/* Scenario: a notification interrupt has just occurred so * there is a need to receive a "one word" (32-bit) message */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg; /* Example message */ if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_ReadMsgWord(myIpc, &myMsg)) { /* Now myMsg contains the received message word */ /* The IPC data is received and processed. * Free up the channel for the next transaction. */ Cy_IPC_Drv_ReleaseNotify(myIpc, MY_IPC_INTR_MASK); } else { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
message – A variable where the read data is copied.
- Returns
Status of the operation
- Returns
CY_IPC_DRV_SUCCESS – The function executed successfully and the IPC was acquired.
CY_IPC_DRV_ERROR – The function encountered an error because the IPC channel was already in a released state, meaning the data may be invalid.
-
cy_en_ipcdrv_status_t
Cy_IPC_Drv_SendMsgDWord
(IPC_STRUCT_Type *base, uint32_t notifyEventIntr, uint32_t *message) This function is used to send two 32-bit word message through an IPC channel.
The function also has an associated notification field that will let the message notify one or multiple IPC interrupts. The IPC channel is locked and remains locked after the function returns. The receiver of the message should release the channel.
- Function Usage
/* Scenario: there is a need to send a "one word" (32-bit) message, * which can be also used as any command/flag/etc. */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg = 0x12345678UL; /* Example message */ if (CY_IPC_DRV_SUCCESS != Cy_IPC_Drv_SendMsgWord(myIpc, MY_IPC_INTR_MASK, myMsg)) { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
notifyEventIntr – Bit encoded list of IPC interrupt lines that are triggered by a notification.
message – The message word that is the data placed in the IPC data register.
- Returns
Status of the operation:
- Returns
CY_IPC_DRV_SUCCESS – The send operation was successful.
CY_IPC_DRV_ERROR – The IPC channel is unavailable because it is already locked.
-
cy_en_ipcdrv_status_t
Cy_IPC_Drv_ReadMsgDWord
(IPC_STRUCT_Type const *base, uint32_t *message) This function is used to read two 32-bit word message through an IPC channel.
This function assumes that the channel is locked (for a valid message). If the channel is not locked, the message is invalid. The user must call Cy_IPC_Drv_Release() function after reading the message to release the IPC channel.
- Function Usage
/* Scenario: a notification interrupt has just occurred so * there is a need to receive a "one word" (32-bit) message */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC release interrupt mask */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg; /* Example message */ if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_ReadMsgWord(myIpc, &myMsg)) { /* Now myMsg contains the received message word */ /* The IPC data is received and processed. * Free up the channel for the next transaction. */ Cy_IPC_Drv_ReleaseNotify(myIpc, MY_IPC_INTR_MASK); } else { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
message – A variable where the read data is copied.
- Returns
Status of the operation
- Returns
CY_IPC_DRV_SUCCESS – The function executed successfully and the IPC was acquired.
CY_IPC_DRV_ERROR – The function encountered an error because the IPC channel was already in a released state, meaning the data may be invalid.
-
__STATIC_INLINE cy_en_ipcdrv_status_t Cy_IPC_Drv_SendMsgPtr (IPC_STRUCT_Type *base, uint32_t notifyEventIntr, void const *msgPtr)
This function is used to send a message pointer through an IPC channel.
The message structure may hold a generic pointer that may contain the address of any user data type or structure. This parameter could be a pointer to a 32-bit integer, an array, or even a data structure defined in the user code. This function acts as a transfer engine for sending the pointer. Any memory management of the pointer allocation and deallocation is up to the application code. The function also has an associated notification field that will let the message notify one or multiple interrupts.
- Function Usage
/* Scenario: there is a need to send a pointer of the message mailbox */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC interrupt mask */ #define MY_IPC_MSG_SIZE (7UL) /* Example message size */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg[MY_IPC_MSG_SIZE] = {1,2,3,4,5,6,7}; /* Example message, the content is fully user-defined */ if (CY_IPC_DRV_SUCCESS != Cy_IPC_Drv_SendMsgPtr(myIpc, MY_IPC_INTR_MASK, (void *) myMsg)) { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
notifyEventIntr – Bit encoded list of IPC interrupt lines that are triggered during the release action.
msgPtr – The message pointer that is being sent over the IPC channel.
- Returns
Status of the operation:
- Returns
CY_IPC_DRV_SUCCESS – The send operation was successful.
CY_IPC_DRV_ERROR – The IPC channel is unavailable because it is already locked.
-
__STATIC_INLINE cy_en_ipcdrv_status_t Cy_IPC_Drv_ReadMsgPtr (IPC_STRUCT_Type const *base, void **msgPtr)
This function is used to read a 32-bit pointer message through an IPC channel.
- Function Usage
/* Scenario: an acquire notification interrupt has just occurred * so now is a time to read a message pointer and then whole the * message content */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_INTR_MASK (1UL << MY_IPC_INTR_INDEX) /* IPC interrupt mask */ #define MY_IPC_MSG_SIZE (7UL) /* Example message size */ IPC_STRUCT_Type * myIpc = Cy_IPC_Drv_GetIpcBaseAddress(MY_IPC_CHAN_INDEX); /* Get IPC base register address */ uint32_t myMsg[MY_IPC_MSG_SIZE]; /* Example message container */ void * myMsgPtr; /* Example message pointer */ if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_ReadMsgPtr(myIpc, &myMsgPtr)) { uint32_t i; for(i = 0; i < MY_IPC_MSG_SIZE; i++) { myMsg[i] = *((uint32_t*)((uint32_t)myMsgPtr + i)); /* Copying the message content */ } } else { /* Insert error handling */ } /* The IPC data was received and processed. * Free up the channel for the next transaction. */ if (CY_IPC_DRV_SUCCESS == Cy_IPC_Drv_LockRelease(myIpc, MY_IPC_INTR_MASK)) { /* Now the IPC channel is successfully released */ } else { /* Insert error handling */ }
- Parameters
base – This parameter is a handle that represents the base address of the registers of the IPC channel. The parameter is generally returned from a call to the Cy_IPC_Drv_GetIpcBaseAddress.
msgPtr – Pointer variable to hold the data pointer that is being read from the IPC channel.
- Returns
Status of the operation
- Returns
CY_IPC_DRV_SUCCESS – The function executed successfully and the IPC was acquired.
CY_IPC_DRV_ERROR – The function encountered an error because the IPC channel was already in a released state meaning the data in it is invalid.
-
__STATIC_INLINE void Cy_IPC_Drv_SetInterruptMask (IPC_INTR_STRUCT_Type *base, uint32_t ipcReleaseMask, uint32_t ipcAcquireMask)
This function is used to set the interrupt mask for an IPC Interrupt.
The mask sets release or acquire notification events for all IPC channels.
- Function Usage
/* Scenario: enable IPC interrupts in IPC interrupt channel #MY_IPC_INTR_INDEX * for both acquire and release events from the IPC channel #MY_IPC_CHAN_INDEX */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_RELEASE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC release interrupt mask */ #define MY_IPC_ACQUIRE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC acquire interrupt mask */ IPC_INTR_STRUCT_Type * myIpcIntr = Cy_IPC_Drv_GetIntrBaseAddr(MY_IPC_INTR_INDEX); uint32_t intr = Cy_IPC_Drv_GetInterruptMask(myIpcIntr); uint32_t releaseIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr) | MY_IPC_RELEASE_INTR_MASK; uint32_t acqiureIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr) | MY_IPC_ACQUIRE_INTR_MASK; Cy_IPC_Drv_SetInterruptMask(myIpcIntr, releaseIntr, acqiureIntr); /* Scenario: the next block is inside the IPC interrupt handler */ { /* Get all the enabled pending interrupts */ uint32_t intr = Cy_IPC_Drv_GetInterruptStatusMasked(myIpcIntr); if (0UL != (MY_IPC_RELEASE_INTR_MASK & intr)) { /* Handle the RELEASE event of the IPC channel MY_IPC_CHAN_INDEX */ } if (0UL != (MY_IPC_ACQUIRE_INTR_MASK & intr)) { /* Handle the ACQUIRE interrupt */ } /* Clear the interrupt */ Cy_IPC_Drv_ClearInterrupt(myIpcIntr, _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr), _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr)); } /* Scenario: disable ALL the IPC interrupts (not from the IPC channel * #MY_IPC_CHAN_INDEX only) in the IPC interrupt channel * #MY_IPC_INTR_INDEX when they are not needed anymore */ Cy_IPC_Drv_SetInterruptMask(myIpcIntr, CY_IPC_NO_NOTIFICATION, CY_IPC_NO_NOTIFICATION);
- Parameters
base – This is a handle to the IPC interrupt. This handle can be calculated from the IPC interrupt number using Cy_IPC_Drv_GetIntrBaseAddr.
ipcReleaseMask – An encoded list of all IPC channels that can trigger the interrupt on a release event.
ipcAcquireMask – An encoded list of all IPC channels that can trigger the interrupt on a notify event.
-
__STATIC_INLINE uint32_t Cy_IPC_Drv_GetInterruptMask (IPC_INTR_STRUCT_Type const *base)
This function is used to read the interrupt mask.
- Function Usage
/* Scenario: enable IPC interrupts in IPC interrupt channel #MY_IPC_INTR_INDEX * for both acquire and release events from the IPC channel #MY_IPC_CHAN_INDEX */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_RELEASE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC release interrupt mask */ #define MY_IPC_ACQUIRE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC acquire interrupt mask */ IPC_INTR_STRUCT_Type * myIpcIntr = Cy_IPC_Drv_GetIntrBaseAddr(MY_IPC_INTR_INDEX); uint32_t intr = Cy_IPC_Drv_GetInterruptMask(myIpcIntr); uint32_t releaseIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr) | MY_IPC_RELEASE_INTR_MASK; uint32_t acqiureIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr) | MY_IPC_ACQUIRE_INTR_MASK; Cy_IPC_Drv_SetInterruptMask(myIpcIntr, releaseIntr, acqiureIntr); /* Scenario: the next block is inside the IPC interrupt handler */ { /* Get all the enabled pending interrupts */ uint32_t intr = Cy_IPC_Drv_GetInterruptStatusMasked(myIpcIntr); if (0UL != (MY_IPC_RELEASE_INTR_MASK & intr)) { /* Handle the RELEASE event of the IPC channel MY_IPC_CHAN_INDEX */ } if (0UL != (MY_IPC_ACQUIRE_INTR_MASK & intr)) { /* Handle the ACQUIRE interrupt */ } /* Clear the interrupt */ Cy_IPC_Drv_ClearInterrupt(myIpcIntr, _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr), _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr)); } /* Scenario: disable ALL the IPC interrupts (not from the IPC channel * #MY_IPC_CHAN_INDEX only) in the IPC interrupt channel * #MY_IPC_INTR_INDEX when they are not needed anymore */ Cy_IPC_Drv_SetInterruptMask(myIpcIntr, CY_IPC_NO_NOTIFICATION, CY_IPC_NO_NOTIFICATION);
- Parameters
base – This is a handle to the IPC interrupt. This handle can be calculated from the IPC interrupt number using Cy_IPC_Drv_GetIntrBaseAddr.
- Returns
The return value is encoded as follows
Interrupt sources
Value
Ipc_PORTX_RELEASE
Xth bit set
Ipc_PORTX_NOTIFY
X+16th bit set
-
__STATIC_INLINE uint32_t Cy_IPC_Drv_GetInterruptStatusMasked (IPC_INTR_STRUCT_Type const *base)
This function is used to read the active unmasked interrupt.
This function can be used in the interrupt service routine to find which source triggered the interrupt.
- Function Usage
/* Scenario: enable IPC interrupts in IPC interrupt channel #MY_IPC_INTR_INDEX * for both acquire and release events from the IPC channel #MY_IPC_CHAN_INDEX */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_RELEASE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC release interrupt mask */ #define MY_IPC_ACQUIRE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC acquire interrupt mask */ IPC_INTR_STRUCT_Type * myIpcIntr = Cy_IPC_Drv_GetIntrBaseAddr(MY_IPC_INTR_INDEX); uint32_t intr = Cy_IPC_Drv_GetInterruptMask(myIpcIntr); uint32_t releaseIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr) | MY_IPC_RELEASE_INTR_MASK; uint32_t acqiureIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr) | MY_IPC_ACQUIRE_INTR_MASK; Cy_IPC_Drv_SetInterruptMask(myIpcIntr, releaseIntr, acqiureIntr); /* Scenario: the next block is inside the IPC interrupt handler */ { /* Get all the enabled pending interrupts */ uint32_t intr = Cy_IPC_Drv_GetInterruptStatusMasked(myIpcIntr); if (0UL != (MY_IPC_RELEASE_INTR_MASK & intr)) { /* Handle the RELEASE event of the IPC channel MY_IPC_CHAN_INDEX */ } if (0UL != (MY_IPC_ACQUIRE_INTR_MASK & intr)) { /* Handle the ACQUIRE interrupt */ } /* Clear the interrupt */ Cy_IPC_Drv_ClearInterrupt(myIpcIntr, _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr), _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr)); } /* Scenario: disable ALL the IPC interrupts (not from the IPC channel * #MY_IPC_CHAN_INDEX only) in the IPC interrupt channel * #MY_IPC_INTR_INDEX when they are not needed anymore */ Cy_IPC_Drv_SetInterruptMask(myIpcIntr, CY_IPC_NO_NOTIFICATION, CY_IPC_NO_NOTIFICATION);
- Parameters
base – This is a handle to the IPC interrupt. This handle can be calculated from the IPC interrupt number using Cy_IPC_Drv_GetIntrBaseAddr.
- Returns
The return value is encoded as follows
Interrupt sources
Value
Ipc_PORTX_RELEASE
Xth bit set
Ipc_PORTX_NOTIFY
X+16th bit set
-
__STATIC_INLINE uint32_t Cy_IPC_Drv_GetInterruptStatus (IPC_INTR_STRUCT_Type const *base)
This function is used to read the pending interrupts.
Note that this read is an unmasked read of the interrupt status. Interrupt sources read as active by this function would generate interrupts only if they were not masked.
- Function Usage
/* Scenario: there is a need to check the IPC pending interrupts */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ IPC_INTR_STRUCT_Type * myIpcIntr = Cy_IPC_Drv_GetIntrBaseAddr(MY_IPC_INTR_INDEX); uint32_t intrStatus = Cy_IPC_Drv_GetInterruptStatus(myIpcIntr);
- Parameters
base – This is a handle to the IPC interrupt. This handle can be calculated from the IPC interrupt number using Cy_IPC_Drv_GetIntrBaseAddr.
- Returns
The return value is encoded as follows
Interrupt sources
Value
Ipc_PORTX_RELEASE
Xth bit set
Ipc_PORTX_NOTIFY
X+16th bit set
-
__STATIC_INLINE void Cy_IPC_Drv_SetInterrupt (IPC_INTR_STRUCT_Type *base, uint32_t ipcReleaseMask, uint32_t ipcAcquireMask)
This function is used to set the interrupt source.
This function can be used to activate interrupts through software.
note
That interrupt sources set using this interrupt would generate interrupts only if they are not masked.
- Function Usage
/* Scenario: there is a need to set the acquire of the IPC channel * #MY_IPC_CHAN_INDEX interrupt for the IPC interrupt channel * #MY_IPC_INTR_INDEX by software. * Prior to trigging the interrupt, ensure that the correspondent interrupt * mask is set in the IPC interrupt channel #MY_IPC_INTR_INDEX */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_ACQUIRE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC acquire interrupt mask example */ IPC_INTR_STRUCT_Type * myIpcIntr = Cy_IPC_Drv_GetIntrBaseAddr(MY_IPC_INTR_INDEX); if (0UL != (MY_IPC_ACQUIRE_INTR_MASK & _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, Cy_IPC_Drv_GetInterruptMask(myIpcIntr)))) { Cy_IPC_Drv_SetInterrupt(myIpcIntr, CY_IPC_NO_NOTIFICATION, MY_IPC_ACQUIRE_INTR_MASK); } else { /* See the \ref Cy_IPC_Drv_SetInterruptMask function usage */ }
- Parameters
base – This is a handle to the IPC interrupt. This handle can be calculated from the IPC interrupt number using Cy_IPC_Drv_GetIntrBaseAddr.
ipcReleaseMask – An encoded list of all IPC channels that can trigger the interrupt on a release event.
ipcAcquireMask – An encoded list of all IPC channels that can trigger the interrupt on a notify event.
-
__STATIC_INLINE void Cy_IPC_Drv_ClearInterrupt (IPC_INTR_STRUCT_Type *base, uint32_t ipcReleaseMask, uint32_t ipcAcquireMask)
This function is used to clear the interrupt source.
Use this function to clear a pending interrupt source in the interrupt status.
- Function Usage
/* Scenario: enable IPC interrupts in IPC interrupt channel #MY_IPC_INTR_INDEX * for both acquire and release events from the IPC channel #MY_IPC_CHAN_INDEX */ #define MY_IPC_CHAN_INDEX (8UL) /* Example of IPC channel index */ #define MY_IPC_INTR_INDEX (8UL) /* Example of IPC interrupt channel index */ #define MY_IPC_RELEASE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC release interrupt mask */ #define MY_IPC_ACQUIRE_INTR_MASK (1UL << MY_IPC_CHAN_INDEX) /* IPC acquire interrupt mask */ IPC_INTR_STRUCT_Type * myIpcIntr = Cy_IPC_Drv_GetIntrBaseAddr(MY_IPC_INTR_INDEX); uint32_t intr = Cy_IPC_Drv_GetInterruptMask(myIpcIntr); uint32_t releaseIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr) | MY_IPC_RELEASE_INTR_MASK; uint32_t acqiureIntr = _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr) | MY_IPC_ACQUIRE_INTR_MASK; Cy_IPC_Drv_SetInterruptMask(myIpcIntr, releaseIntr, acqiureIntr); /* Scenario: the next block is inside the IPC interrupt handler */ { /* Get all the enabled pending interrupts */ uint32_t intr = Cy_IPC_Drv_GetInterruptStatusMasked(myIpcIntr); if (0UL != (MY_IPC_RELEASE_INTR_MASK & intr)) { /* Handle the RELEASE event of the IPC channel MY_IPC_CHAN_INDEX */ } if (0UL != (MY_IPC_ACQUIRE_INTR_MASK & intr)) { /* Handle the ACQUIRE interrupt */ } /* Clear the interrupt */ Cy_IPC_Drv_ClearInterrupt(myIpcIntr, _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_RELEASE, intr), _FLD2VAL(IPC_INTR_STRUCT_INTR_MASK_NOTIFY, intr)); } /* Scenario: disable ALL the IPC interrupts (not from the IPC channel * #MY_IPC_CHAN_INDEX only) in the IPC interrupt channel * #MY_IPC_INTR_INDEX when they are not needed anymore */ Cy_IPC_Drv_SetInterruptMask(myIpcIntr, CY_IPC_NO_NOTIFICATION, CY_IPC_NO_NOTIFICATION);
- Parameters
base – This is a handle to the IPC interrupt. This handle can be calculated from the IPC interrupt number using Cy_IPC_Drv_GetIntrBaseAddr.
ipcReleaseMask – An encoded list of all IPC channels that can trigger the interrupt on a release event.
ipcAcquireMask – An encoded list of all IPC channels that can trigger the interrupt on a notify event.
-