SIO Functions

group group_gpio_functions_sio

Functions

void Cy_GPIO_SetVregEn(GPIO_PRT_Type *base, uint32_t pinNum, uint32_t value)

Configures the SIO pin pair output buffer regulation mode.

Note that this function has no effect on non-SIO pins.

note

This function modifies a port register in a read-modify-write operation. It is not thread safe as the resource is shared among multiple pins on a port.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2. 
                 Both pins are configured as output pins. The output (driven)
                 signals on P0.2 and P0.3 need to be at a regulated voltage 
                 based on Voh and VRef selection. */
            
    /* Get the output buffer regulation mode of P0.2/P0.3 pair */
    if(CY_SIO_VREG_UNREGULATED == Cy_GPIO_GetVregEn(P0_3_PORT, P0_3_NUM))
    {
        /* Set the output buffer to be regulated on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetVregEn(P0_3_PORT, P0_3_NUM, CY_SIO_VREG_REGULATED);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

  • value – SIO pair output buffer regulator mode. Options are detailed in SIO output buffer mode macros

uint32_t Cy_GPIO_GetVregEn(GPIO_PRT_Type *base, uint32_t pinNum)

Returns the SIO pin pair output buffer regulation mode.

Note that this function has no effect on non-SIO pins.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2. 
                 Both pins are configured as output pins. The output (driven)
                 signals on P0.2 and P0.3 need to be at a regulated voltage 
                 based on Voh and VRef selection. */
            
    /* Get the output buffer regulation mode of P0.2/P0.3 pair */
    if(CY_SIO_VREG_UNREGULATED == Cy_GPIO_GetVregEn(P0_3_PORT, P0_3_NUM))
    {
        /* Set the output buffer to be regulated on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetVregEn(P0_3_PORT, P0_3_NUM, CY_SIO_VREG_REGULATED);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

Returns

SIO pair output buffer regulator mode. Options are detailed in SIO output buffer mode macros

void Cy_GPIO_SetIbufMode(GPIO_PRT_Type *base, uint32_t pinNum, uint32_t value)

Configures the SIO pin pair input buffer mode.

Note that this function has no effect on non-SIO pins.

note

This function modifies a port register in a read-modify-write operation. It is not thread safe as the resource is shared among multiple pins on a port.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as input pins. The input signals 
                 on P0.2 and P0.3 need to be interpreted as logic 0 or 1 
                 depending on the chosen SIO vtrip point. */
    
    /* Get the input buffer mode of P0.2/P0.3 pair */
    if(CY_SIO_IBUF_SINGLEENDED == Cy_GPIO_GetIbufMode(P0_3_PORT, P0_3_NUM))
    {
        /* Set the input buffer to be differential on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetIbufMode(P0_3_PORT, P0_3_NUM, CY_SIO_IBUF_DIFFERENTIAL);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

  • value – SIO pair input buffer mode. Options are detailed in SIO input buffer mode macros

uint32_t Cy_GPIO_GetIbufMode(GPIO_PRT_Type *base, uint32_t pinNum)

Returns the SIO pin pair input buffer mode.

Note that this function has no effect on non-SIO pins.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as input pins. The input signals 
                 on P0.2 and P0.3 need to be interpreted as logic 0 or 1 
                 depending on the chosen SIO vtrip point. */
    
    /* Get the input buffer mode of P0.2/P0.3 pair */
    if(CY_SIO_IBUF_SINGLEENDED == Cy_GPIO_GetIbufMode(P0_3_PORT, P0_3_NUM))
    {
        /* Set the input buffer to be differential on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetIbufMode(P0_3_PORT, P0_3_NUM, CY_SIO_IBUF_DIFFERENTIAL);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

Returns

SIO pair input buffer mode. Options are detailed in SIO input buffer mode macros

void Cy_GPIO_SetVtripSel(GPIO_PRT_Type *base, uint32_t pinNum, uint32_t value)

Configures the SIO pin pair input buffer trip point.

Note that this function has no effect on non-SIO pins.

note

This function modifies a port register in a read-modify-write operation. It is not thread safe as the resource is shared among multiple pins on a port.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as input pins. The input signals
                 on P0.2 and P0.3 need to be interpreted as logic 0 or 1 at 
                 0.5 x VDDIO threshold. */
    
    /* Set the input buffer to be differential on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetIbufMode(P0_3_PORT, P0_3_NUM, CY_SIO_IBUF_DIFFERENTIAL);
    
    /* Choose VREF to be sourced from VDDIO (pin ref) */
    Cy_GPIO_SetVrefSel(P0_3_PORT, P0_3_NUM, CY_SIO_VREF_PINREF);
    
    /* Get the input buffer trip-point of P0.2/P0.3 pair */
    if(CY_SIO_VTRIP_CMOS == Cy_GPIO_GetVtripSel(P0_3_PORT, P0_3_NUM))
    {
        /* Set the input buffer trip-point to 0.5 x VDDIO on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetVtripSel(P0_3_PORT, P0_3_NUM, CY_SIO_VTRIP_0_5VDDIO_0_5VOH);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

  • value – SIO pair input buffer trip point. Options are detailed in SIO input buffer trip-point macros

uint32_t Cy_GPIO_GetVtripSel(GPIO_PRT_Type *base, uint32_t pinNum)

Returns the SIO pin pair input buffer trip point.

Note that this function has no effect on non-SIO pins.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as input pins. The input signals
                 on P0.2 and P0.3 need to be interpreted as logic 0 or 1 at 
                 0.5 x VDDIO threshold. */
    
    /* Set the input buffer to be differential on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetIbufMode(P0_3_PORT, P0_3_NUM, CY_SIO_IBUF_DIFFERENTIAL);
    
    /* Choose VREF to be sourced from VDDIO (pin ref) */
    Cy_GPIO_SetVrefSel(P0_3_PORT, P0_3_NUM, CY_SIO_VREF_PINREF);
    
    /* Get the input buffer trip-point of P0.2/P0.3 pair */
    if(CY_SIO_VTRIP_CMOS == Cy_GPIO_GetVtripSel(P0_3_PORT, P0_3_NUM))
    {
        /* Set the input buffer trip-point to 0.5 x VDDIO on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetVtripSel(P0_3_PORT, P0_3_NUM, CY_SIO_VTRIP_0_5VDDIO_0_5VOH);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

Returns

SIO pair input buffer trip point. Options are detailed in SIO input buffer trip-point macros

void Cy_GPIO_SetVrefSel(GPIO_PRT_Type *base, uint32_t pinNum, uint32_t value)

Configures the SIO reference voltage for the input buffer trip point.

Note that this function has no effect on non-SIO pins.

note

This function modifies a port register in a read-modify-write operation. It is not thread safe as the resource is shared among multiple pins on a port.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as input pins. The input signals
                 on P0.2 and P0.3 need to be interpreted as logic 0 or 1 at
                 1.25 x 1.2V threshold. */
    
    /* Set the input buffer to be differential on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetIbufMode(P0_3_PORT, P0_3_NUM, CY_SIO_IBUF_DIFFERENTIAL);
    
    /* Set the input buffer trip-point to 0.5 x VOH on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetVtripSel(P0_3_PORT, P0_3_NUM, CY_SIO_VTRIP_0_5VDDIO_0_5VOH);
    
    /* Set the regulated input buffer trip point multiplier to 1.25 x VRef */
    Cy_GPIO_SetVohSel(P0_3_PORT, P0_3_NUM, CY_SIO_VOH_1_25);
    
    /* Get the reference voltage of P0.2/P0.3 pair */
    if(CY_SIO_VREF_PINREF == Cy_GPIO_GetVrefSel(P0_3_PORT, P0_3_NUM))
    {
        /* Set the reference voltage to 1.2V SRSS internal reference on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetVrefSel(P0_3_PORT, P0_3_NUM, CY_SIO_VREF_1_2V);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

  • value – SIO pair reference voltage. Options are detailed in SIO reference voltage for input buffer trip-point macros

uint32_t Cy_GPIO_GetVrefSel(GPIO_PRT_Type *base, uint32_t pinNum)

Returns the SIO reference voltage for the input buffer trip point.

Note that this function has no effect on non-SIO pins.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as input pins. The input signals
                 on P0.2 and P0.3 need to be interpreted as logic 0 or 1 at
                 1.25 x 1.2V threshold. */
    
    /* Set the input buffer to be differential on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetIbufMode(P0_3_PORT, P0_3_NUM, CY_SIO_IBUF_DIFFERENTIAL);
    
    /* Set the input buffer trip-point to 0.5 x VOH on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetVtripSel(P0_3_PORT, P0_3_NUM, CY_SIO_VTRIP_0_5VDDIO_0_5VOH);
    
    /* Set the regulated input buffer trip point multiplier to 1.25 x VRef */
    Cy_GPIO_SetVohSel(P0_3_PORT, P0_3_NUM, CY_SIO_VOH_1_25);
    
    /* Get the reference voltage of P0.2/P0.3 pair */
    if(CY_SIO_VREF_PINREF == Cy_GPIO_GetVrefSel(P0_3_PORT, P0_3_NUM))
    {
        /* Set the reference voltage to 1.2V SRSS internal reference on the P0.2/P0.3 SIO pair */
        Cy_GPIO_SetVrefSel(P0_3_PORT, P0_3_NUM, CY_SIO_VREF_1_2V);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

Returns

SIO pair reference voltage. Options are detailed in SIO reference voltage for input buffer trip-point macros

void Cy_GPIO_SetVohSel(GPIO_PRT_Type *base, uint32_t pinNum, uint32_t value)

Configures the regulated output reference multiplier for the SIO pin pair.

The regulated output reference controls both the output level of digital output pin and the input trip point of digital input pin in the SIO pair.

Note that this function has no effect on non-SIO pins.

note

This function modifies a port register in a read-modify-write operation. It is not thread safe as the resource is shared among multiple pins on a port.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as output pins. The output (driven)
                 signals on P0.2 and P0.3 need to be at 
                 2.5 x AMuxBusA voltage x 2 for logic high. */
    
    /* Set the output buffer to be regulated on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetVregEn(P0_3_PORT, P0_3_NUM, CY_SIO_VREG_REGULATED);
    
    /* Set the reference voltage to be sourced from AMUXBUS A */
    Cy_GPIO_SetVrefSel(P0_3_PORT, P0_3_NUM, CY_SIO_VREF_AMUX_A);
    
    /* Get the regulated voltage multiplier value of P0.2/P0.3 pair */
    if(CY_SIO_VOH_1_00 == Cy_GPIO_GetVohSel(P0_3_PORT, P0_3_NUM))
    {
        /* Set the regulated voltage multiplier to 2.5 x VRef */
        Cy_GPIO_SetVohSel(P0_3_PORT, P0_3_NUM, CY_SIO_VOH_2_50);
    }

Parameters
uint32_t Cy_GPIO_GetVohSel(GPIO_PRT_Type *base, uint32_t pinNum)

Returns the regulated output reference multiplier for the SIO pin pair.

Note that this function has no effect on non-SIO pins.

Function Usage


    /* Scenario: Assume P0.3 is an SIO pin and that it is paired with P0.2.
                 Both pins are configured as output pins. The output (driven)
                 signals on P0.2 and P0.3 need to be at 
                 2.5 x AMuxBusA voltage x 2 for logic high. */
    
    /* Set the output buffer to be regulated on the P0.2/P0.3 SIO pair */
    Cy_GPIO_SetVregEn(P0_3_PORT, P0_3_NUM, CY_SIO_VREG_REGULATED);
    
    /* Set the reference voltage to be sourced from AMUXBUS A */
    Cy_GPIO_SetVrefSel(P0_3_PORT, P0_3_NUM, CY_SIO_VREF_AMUX_A);
    
    /* Get the regulated voltage multiplier value of P0.2/P0.3 pair */
    if(CY_SIO_VOH_1_00 == Cy_GPIO_GetVohSel(P0_3_PORT, P0_3_NUM))
    {
        /* Set the regulated voltage multiplier to 2.5 x VRef */
        Cy_GPIO_SetVohSel(P0_3_PORT, P0_3_NUM, CY_SIO_VOH_2_50);
    }

Parameters
  • base – Pointer to the pin’s port register base address

  • pinNum – Position of the pin bit-field within the port register

Returns

SIO pair reference voltage. Options are detailed in Regulated output voltage level (Voh) and input buffer trip-point of an SIO pair macros