Channel Functions

group group_dma_channel_functions

Functions

cy_en_dma_status_t Cy_DMA_Channel_Init(DW_Type *base, uint32_t channel, cy_stc_dma_channel_config_t const *channelConfig)

Initializes the DMA channel with a descriptor and other parameters.

Function Usage

    
    /* Scenario: Initialize a 1D descriptor */
    #define DATACNT (8UL)
    cy_stc_dma_descriptor_t descriptor;
    cy_stc_dma_descriptor_t nextDescriptor;
    uint32_t src[DATACNT];
    uint32_t dst[DATACNT];
    
    cy_stc_dma_descriptor_config_t descriptor_cfg = 
    {
        .retrigger = CY_DMA_RETRIG_IM,
        .interruptType = CY_DMA_DESCR,
        .triggerOutType = CY_DMA_DESCR,
        .channelState = CY_DMA_CHANNEL_ENABLED,
        .triggerInType = CY_DMA_DESCR,
        .dataSize = CY_DMA_WORD,
        .srcTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .dstTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .descriptorType = CY_DMA_1D_TRANSFER,
        .srcAddress = &src,
        .dstAddress = &dst,
        .srcXincrement = 1U,
        .dstXincrement = 1U,
        .xCount = DATACNT,
        .srcYincrement = 0U,
        .dstYincrement = 0U,
        .yCount = 1UL,
        .nextDescriptor = &nextDescriptor,
    };
    
    if (CY_DMA_SUCCESS != Cy_DMA_Descriptor_Init(&descriptor, &descriptor_cfg))
    {
        /* Insert error handling */
    }
    
    /* Scenario: Setup and enable the DMA channel 0 of block DW0 */
    cy_stc_dma_channel_config_t channelConfig;
    channelConfig.preemptable = false;
    channelConfig.enable = false;
    channelConfig.bufferable = false;
    
    if (CY_DMA_SUCCESS != Cy_DMA_Channel_Init(DW0, 0UL, &channelConfig))
    {
        /* Insert error handling */
    }
    
    Cy_DMA_Channel_SetDescriptor(DW0, 0UL, &descriptor);
    Cy_DMA_Channel_SetPriority(DW0, 0UL, 3UL);
    Cy_DMA_Channel_Enable(DW0, 0UL);
    
    Cy_DMA_Enable(DW0);
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – A channel number.

  • channelConfig – The structure that has the initialization information for the channel.

Returns

The status /ref cy_en_dma_status_t.

void Cy_DMA_Channel_DeInit(DW_Type *base, uint32_t channel)

Clears the content of registers corresponding to the channel.

Function Usage

    
    /* Scenario: Disable the DMA channel 0 of block DW0 if it's priority equals 3 */
    
    if (3UL == Cy_DMA_Channel_GetPriority(DW0, 0UL))
    {    
        if (0UL != Cy_DMA_GetActiveChannel(DW0))
        {
            Cy_DMA_Channel_Disable(DW0, 0UL);
            Cy_DMA_Channel_DeInit(DW0, 0UL);

            /* if needed (if there is only channel used) the whole block can be disabled */
            Cy_DMA_Disable(DW0);
        }
    }
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – A channel number.

__STATIC_INLINE void Cy_DMA_Channel_SetDescriptor (DW_Type *base, uint32_t channel, cy_stc_dma_descriptor_t const *descriptor)

Sets a descriptor as current for the specified DMA channel.

Function Usage

    
    /* Scenario: Initialize a 1D descriptor */
    #define DATACNT (8UL)
    cy_stc_dma_descriptor_t descriptor;
    cy_stc_dma_descriptor_t nextDescriptor;
    uint32_t src[DATACNT];
    uint32_t dst[DATACNT];
    
    cy_stc_dma_descriptor_config_t descriptor_cfg = 
    {
        .retrigger = CY_DMA_RETRIG_IM,
        .interruptType = CY_DMA_DESCR,
        .triggerOutType = CY_DMA_DESCR,
        .channelState = CY_DMA_CHANNEL_ENABLED,
        .triggerInType = CY_DMA_DESCR,
        .dataSize = CY_DMA_WORD,
        .srcTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .dstTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .descriptorType = CY_DMA_1D_TRANSFER,
        .srcAddress = &src,
        .dstAddress = &dst,
        .srcXincrement = 1U,
        .dstXincrement = 1U,
        .xCount = DATACNT,
        .srcYincrement = 0U,
        .dstYincrement = 0U,
        .yCount = 1UL,
        .nextDescriptor = &nextDescriptor,
    };
    
    if (CY_DMA_SUCCESS != Cy_DMA_Descriptor_Init(&descriptor, &descriptor_cfg))
    {
        /* Insert error handling */
    }
    
    /* Scenario: Setup and enable the DMA channel 0 of block DW0 */
    cy_stc_dma_channel_config_t channelConfig;
    channelConfig.preemptable = false;
    channelConfig.enable = false;
    channelConfig.bufferable = false;
    
    if (CY_DMA_SUCCESS != Cy_DMA_Channel_Init(DW0, 0UL, &channelConfig))
    {
        /* Insert error handling */
    }
    
    Cy_DMA_Channel_SetDescriptor(DW0, 0UL, &descriptor);
    Cy_DMA_Channel_SetPriority(DW0, 0UL, 3UL);
    Cy_DMA_Channel_Enable(DW0, 0UL);
    
    Cy_DMA_Enable(DW0);
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

  • descriptor – This is the descriptor to be associated with the channel.

__STATIC_INLINE void Cy_DMA_Channel_Enable (DW_Type *base, uint32_t channel)

The function is used to enable a DMA channel.

Function Usage

    
    /* Scenario: Initialize a 1D descriptor */
    #define DATACNT (8UL)
    cy_stc_dma_descriptor_t descriptor;
    cy_stc_dma_descriptor_t nextDescriptor;
    uint32_t src[DATACNT];
    uint32_t dst[DATACNT];
    
    cy_stc_dma_descriptor_config_t descriptor_cfg = 
    {
        .retrigger = CY_DMA_RETRIG_IM,
        .interruptType = CY_DMA_DESCR,
        .triggerOutType = CY_DMA_DESCR,
        .channelState = CY_DMA_CHANNEL_ENABLED,
        .triggerInType = CY_DMA_DESCR,
        .dataSize = CY_DMA_WORD,
        .srcTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .dstTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .descriptorType = CY_DMA_1D_TRANSFER,
        .srcAddress = &src,
        .dstAddress = &dst,
        .srcXincrement = 1U,
        .dstXincrement = 1U,
        .xCount = DATACNT,
        .srcYincrement = 0U,
        .dstYincrement = 0U,
        .yCount = 1UL,
        .nextDescriptor = &nextDescriptor,
    };
    
    if (CY_DMA_SUCCESS != Cy_DMA_Descriptor_Init(&descriptor, &descriptor_cfg))
    {
        /* Insert error handling */
    }
    
    /* Scenario: Setup and enable the DMA channel 0 of block DW0 */
    cy_stc_dma_channel_config_t channelConfig;
    channelConfig.preemptable = false;
    channelConfig.enable = false;
    channelConfig.bufferable = false;
    
    if (CY_DMA_SUCCESS != Cy_DMA_Channel_Init(DW0, 0UL, &channelConfig))
    {
        /* Insert error handling */
    }
    
    Cy_DMA_Channel_SetDescriptor(DW0, 0UL, &descriptor);
    Cy_DMA_Channel_SetPriority(DW0, 0UL, 3UL);
    Cy_DMA_Channel_Enable(DW0, 0UL);
    
    Cy_DMA_Enable(DW0);
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

__STATIC_INLINE void Cy_DMA_Channel_Disable (DW_Type *base, uint32_t channel)

The function is used to disable a DMA channel.

Function Usage

    
    /* Scenario: Disable the DMA channel 0 of block DW0 if it's priority equals 3 */
    
    if (3UL == Cy_DMA_Channel_GetPriority(DW0, 0UL))
    {    
        if (0UL != Cy_DMA_GetActiveChannel(DW0))
        {
            Cy_DMA_Channel_Disable(DW0, 0UL);
            Cy_DMA_Channel_DeInit(DW0, 0UL);

            /* if needed (if there is only channel used) the whole block can be disabled */
            Cy_DMA_Disable(DW0);
        }
    }
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

__STATIC_INLINE void Cy_DMA_Channel_SetPriority (DW_Type *base, uint32_t channel, uint32_t priority)

The function is used to set a priority for the DMA channel.

Function Usage

    
    /* Scenario: Initialize a 1D descriptor */
    #define DATACNT (8UL)
    cy_stc_dma_descriptor_t descriptor;
    cy_stc_dma_descriptor_t nextDescriptor;
    uint32_t src[DATACNT];
    uint32_t dst[DATACNT];
    
    cy_stc_dma_descriptor_config_t descriptor_cfg = 
    {
        .retrigger = CY_DMA_RETRIG_IM,
        .interruptType = CY_DMA_DESCR,
        .triggerOutType = CY_DMA_DESCR,
        .channelState = CY_DMA_CHANNEL_ENABLED,
        .triggerInType = CY_DMA_DESCR,
        .dataSize = CY_DMA_WORD,
        .srcTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .dstTransferSize = CY_DMA_TRANSFER_SIZE_WORD,
        .descriptorType = CY_DMA_1D_TRANSFER,
        .srcAddress = &src,
        .dstAddress = &dst,
        .srcXincrement = 1U,
        .dstXincrement = 1U,
        .xCount = DATACNT,
        .srcYincrement = 0U,
        .dstYincrement = 0U,
        .yCount = 1UL,
        .nextDescriptor = &nextDescriptor,
    };
    
    if (CY_DMA_SUCCESS != Cy_DMA_Descriptor_Init(&descriptor, &descriptor_cfg))
    {
        /* Insert error handling */
    }
    
    /* Scenario: Setup and enable the DMA channel 0 of block DW0 */
    cy_stc_dma_channel_config_t channelConfig;
    channelConfig.preemptable = false;
    channelConfig.enable = false;
    channelConfig.bufferable = false;
    
    if (CY_DMA_SUCCESS != Cy_DMA_Channel_Init(DW0, 0UL, &channelConfig))
    {
        /* Insert error handling */
    }
    
    Cy_DMA_Channel_SetDescriptor(DW0, 0UL, &descriptor);
    Cy_DMA_Channel_SetPriority(DW0, 0UL, 3UL);
    Cy_DMA_Channel_Enable(DW0, 0UL);
    
    Cy_DMA_Enable(DW0);
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

  • priority – The priority to be set for the DMA channel. The allowed values are 0,1,2,3.

__STATIC_INLINE uint32_t Cy_DMA_Channel_GetPriority (DW_Type const *base, uint32_t channel)

Returns the priority of the DMA channel.

Function Usage

    
    /* Scenario: Disable the DMA channel 0 of block DW0 if it's priority equals 3 */
    
    if (3UL == Cy_DMA_Channel_GetPriority(DW0, 0UL))
    {    
        if (0UL != Cy_DMA_GetActiveChannel(DW0))
        {
            Cy_DMA_Channel_Disable(DW0, 0UL);
            Cy_DMA_Channel_DeInit(DW0, 0UL);

            /* if needed (if there is only channel used) the whole block can be disabled */
            Cy_DMA_Disable(DW0);
        }
    }
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

Returns

The priority of the channel.

__STATIC_INLINE cy_en_dma_intr_cause_t Cy_DMA_Channel_GetStatus (DW_Type const *base, uint32_t channel)

Returns the interrupt reason of the specified channel.

Function Usage

    /* Scenario: Inside the interrupt service routine for block DW0 channel 0: */    
    if (CY_DMA_INTR_MASK == Cy_DMA_Channel_GetInterruptStatusMasked(DW0, 0UL))
    {
        /* Get the interrupt cause */
        cy_en_dma_intr_cause_t cause = Cy_DMA_Channel_GetStatus(DW0, 0UL);

        if (CY_DMA_INTR_CAUSE_COMPLETION != cause)
        {
            /* Insert error handling */
        }

        /* Clear the interrupt */
        Cy_DMA_Channel_ClearInterrupt(DW0, 0UL);
    }

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

Returns

The cause cy_en_dma_intr_cause_t of the interrupt.

__STATIC_INLINE cy_stc_dma_descriptor_t * Cy_DMA_Channel_GetCurrentDescriptor (DW_Type const *base, uint32_t channel)

Returns the descriptor that is active in the channel.

Function Usage

    
    /* Scenario: Disable a descriptor */
    if (&descriptor != Cy_DMA_Channel_GetCurrentDescriptor(DW0, 0UL)) /* Make sure it is not in use */
    {
        Cy_DMA_Descriptor_DeInit(&descriptor);
    }
    

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

Returns

The pointer to the descriptor associated with the channel.

__STATIC_INLINE uint32_t Cy_DMA_Channel_GetInterruptStatus (DW_Type const *base, uint32_t channel)

Returns the interrupt status of the specified channel.

Function Usage

    /* Scenario: Need to check the  interrupt status regardless of whether it is enabled (masked) or not */
    if (CY_DMA_INTR_MASK == Cy_DMA_Channel_GetInterruptStatus (DW0, 0UL))
    {
        /* The DW0 channel 0 interrupt is pending */
    }

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

Returns

The status of an interrupt for the specified channel.

__STATIC_INLINE void Cy_DMA_Channel_ClearInterrupt (DW_Type *base, uint32_t channel)

Clears the interrupt status of the specified channel.

Function Usage

    /* Scenario: Inside the interrupt service routine for block DW0 channel 0: */    
    if (CY_DMA_INTR_MASK == Cy_DMA_Channel_GetInterruptStatusMasked(DW0, 0UL))
    {
        /* Get the interrupt cause */
        cy_en_dma_intr_cause_t cause = Cy_DMA_Channel_GetStatus(DW0, 0UL);

        if (CY_DMA_INTR_CAUSE_COMPLETION != cause)
        {
            /* Insert error handling */
        }

        /* Clear the interrupt */
        Cy_DMA_Channel_ClearInterrupt(DW0, 0UL);
    }

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

__STATIC_INLINE void Cy_DMA_Channel_SetInterrupt (DW_Type *base, uint32_t channel)

Sets the interrupt for the specified channel.

Function Usage

    /* Scenario: Enable interrupts for block DW0 channel 0 */
    Cy_DMA_Channel_SetInterruptMask (DW0, 0UL, CY_DMA_INTR_MASK);
    
    /* Scenario: Test the interrupt for block DW0 channel 0 */
    Cy_DMA_Channel_SetInterrupt(DW0, 0UL);
    /* Now the interrupt should occur (if it is enabled, of course) */

    /* Scenario: Disable interrupts for block DW0 channel 0 if it is enabled */
    if (CY_DMA_INTR_MASK == Cy_DMA_Channel_GetInterruptMask(DW0, 0UL))
    {
        Cy_DMA_Channel_SetInterruptMask (DW0, 0UL, 0UL);
    }

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

__STATIC_INLINE uint32_t Cy_DMA_Channel_GetInterruptMask (DW_Type const *base, uint32_t channel)

Returns the interrupt mask value of the specified channel.

Function Usage

    /* Scenario: Enable interrupts for block DW0 channel 0 */
    Cy_DMA_Channel_SetInterruptMask (DW0, 0UL, CY_DMA_INTR_MASK);
    
    /* Scenario: Test the interrupt for block DW0 channel 0 */
    Cy_DMA_Channel_SetInterrupt(DW0, 0UL);
    /* Now the interrupt should occur (if it is enabled, of course) */

    /* Scenario: Disable interrupts for block DW0 channel 0 if it is enabled */
    if (CY_DMA_INTR_MASK == Cy_DMA_Channel_GetInterruptMask(DW0, 0UL))
    {
        Cy_DMA_Channel_SetInterruptMask (DW0, 0UL, 0UL);
    }

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

Returns

The interrupt mask value.

__STATIC_INLINE void Cy_DMA_Channel_SetInterruptMask (DW_Type *base, uint32_t channel, uint32_t interrupt)

Sets an interrupt mask value for the specified channel.

Function Usage

    /* Scenario: Enable interrupts for block DW0 channel 0 */
    Cy_DMA_Channel_SetInterruptMask (DW0, 0UL, CY_DMA_INTR_MASK);
    
    /* Scenario: Test the interrupt for block DW0 channel 0 */
    Cy_DMA_Channel_SetInterrupt(DW0, 0UL);
    /* Now the interrupt should occur (if it is enabled, of course) */

    /* Scenario: Disable interrupts for block DW0 channel 0 if it is enabled */
    if (CY_DMA_INTR_MASK == Cy_DMA_Channel_GetInterruptMask(DW0, 0UL))
    {
        Cy_DMA_Channel_SetInterruptMask (DW0, 0UL, 0UL);
    }

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.

  • interrupt – The interrupt mask: CY_DMA_INTR_MASK to enable the interrupt or 0UL to disable the interrupt.

__STATIC_INLINE uint32_t Cy_DMA_Channel_GetInterruptStatusMasked (DW_Type const *base, uint32_t channel)

Returns the logical AND of the corresponding INTR and INTR_MASK fields in a single-load operation.

Function Usage

    /* Scenario: Inside the interrupt service routine for block DW0 channel 0: */    
    if (CY_DMA_INTR_MASK == Cy_DMA_Channel_GetInterruptStatusMasked(DW0, 0UL))
    {
        /* Get the interrupt cause */
        cy_en_dma_intr_cause_t cause = Cy_DMA_Channel_GetStatus(DW0, 0UL);

        if (CY_DMA_INTR_CAUSE_COMPLETION != cause)
        {
            /* Insert error handling */
        }

        /* Clear the interrupt */
        Cy_DMA_Channel_ClearInterrupt(DW0, 0UL);
    }

Parameters
  • base – The pointer to the hardware DMA block.

  • channel – The channel number.