Functions¶
-
group
group_crypto_lld_rng_functions
Functions
-
__STATIC_INLINE cy_en_crypto_status_t Cy_Crypto_Core_Prng_Init (CRYPTO_Type *base, uint32_t lfsr32InitState, uint32_t lfsr31InitState, uint32_t lfsr29InitState)
Initializes the PRND parameters.
Invoking this function causes a restart of the pseudo-random sequence.
- Parameters
base – The pointer to the CRYPTO instance.
lfsr32InitState – A non-zero seed value for the first LFSR.
lfsr31InitState – A non-zero seed value for the second LFSR.
lfsr29InitState – A non-zero seed value for the third LFSR.
- Returns
-
__STATIC_INLINE cy_en_crypto_status_t Cy_Crypto_Core_Prng (CRYPTO_Type *base, uint32_t max, uint32_t *randomNum)
Generates a Pseudo Random Number.
- Parameters
base – The pointer to the CRYPTO instance.
max – The maximum value of a random number.
randomNum – The pointer to a variable to store the generated pseudo random number.
- Returns
-
__STATIC_INLINE cy_en_crypto_status_t Cy_Crypto_Core_Trng (CRYPTO_Type *base, uint32_t GAROPol, uint32_t FIROPol, uint32_t max, uint32_t *randomNum)
Generates a True Random Number.
- Parameters
base – The pointer to the CRYPTO instance.
GAROPol – The polynomial for the programmable Galois ring oscillator.
FIROPol – The polynomial for the programmable Fibonacci ring oscillator.
max – The maximum length of a random number, in the range of [0, 32] bits.
randomNum – The pointer to a generated true random number. Must be 4-byte aligned.
- Returns
-