PSoC™ 6 Prebuilt Images

Prebuilt application images are executed on the Cortex M0+ core of the PSoC 6 dual-core MCU. The images are provided as C arrays ready to be compiled as part of the Cortex M4 application. The Cortex M0+ application code is placed to internal flash by the Cortex M4 linker script.

Note: Each application image has a variant based on the hardware die (e.g. psoc6_01, psoc6_02, psoc6_03, …) it is supported on. An #ifdef at the top of each .c file automatically controls which version is used so there is no need to specify a particular image.

Click here to be taken to the GitHub repository for these images.