Typedefs¶
-
group
group_wcm_typedefs
Typedefs
-
typedef uint8_t
cy_wcm_ssid_t
[CY_WCM_MAX_SSID_LEN
+ 1]¶ SSID name (AP name in null-terminated string format).
-
typedef uint8_t
cy_wcm_mac_t
[CY_WCM_MAC_ADDR_LEN
]¶ Unique 6-byte MAC address represented in network byte order.
-
typedef uint8_t
cy_wcm_passphrase_t
[CY_WCM_MAX_PASSPHRASE_LEN
+ 1]¶ Passphrase in null-terminated string format.
-
typedef void (*
cy_wcm_scan_result_callback_t
)(cy_wcm_scan_result_t *result_ptr, void *user_data, cy_wcm_scan_status_t status)¶ Wi-Fi scan result callback function pointer type.
Note: The callback function will be executed in the context of the WCM.
- Parameters
result_ptr – [in] : A pointer to the scan result; the scan result will be freed once the callback function returns from the application. There will not be any scan result when the scan status is CY_WCM_SCAN_COMPLETE.
user_data – [in] : User-provided data.
status – [in] : Status of the scan process.
-
typedef void (*
cy_wcm_event_callback_t
)(cy_wcm_event_t event, cy_wcm_event_data_t *event_data)¶ WCM event callback function pointer type; events are invoked when the WHD posts events to WCM.
Note: The callback function will be executed in the context of the WCM.
- Parameters
event – [in] : WCM events.
event_data – [in] : A pointer to the event data. The event data will be freed once the callback returns from the application.
-
typedef uint8_t